Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi won't boot with noise and PWR lit only
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 708 subscribers
  • Views 7222 views
  • Users 0 members are here
  • problem
  • issue
  • raspberry_pi
  • raspberrypi
  • boot
Related

Pi won't boot with noise and PWR lit only

wcypierre
wcypierre over 10 years ago

Had been running this pi for 24x7 for about a year now and it has been running fine until I realized that it was down just now when I went to do some checking.

Heard some noises too and now I can't seem to get it back up (noise + PWR lit + dim ACT light only).


Model: Raspberry Pi B

OS: Raspbian

Things attached to the pi: LAN cable, SD Card

Video to demonstrate the noise that the pi makes: https://drive.google.com/file/d/0BwiJswXag8O4dkNKbmlmRVBKOW8/view?usp=sharing


Note: I'm using Powerbank to power the pi up just for the sake of taking the video, normally it is attached to a better power supply.


Symptoms:

1. Red PWR light

2. dim ACT light

3. Noise made as per video above


Things that I've tried:

1. Changing the Power Supply(tried from my original source to genuine Pineng Powerbank to Nokia's official charger to Xiaomi's official charger to the charger that was shipped with the pi)

2. SD Card (it was working on the other pi and the other sd card that I've put into from the other pi doesn't work)

3. LAN cable

4. HDMI - No output

5. Composite - No output

6. Heating it up (https://www.youtube.com/watch?v=AwF6v-4NFdg)

7. Holding the sdcard slot to ensure that the issue isn't with the sd card slot

8. R-Pi Troubleshooting - eLinux.org (the "Red power LED is on, green LED does not flash, nothing on display" part)


Things that I know but I couldn't try because of limitations:

1. Serial console


Any other things that I can try of?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    Can someone describe the sound?  I don't have speakers handy.

     

    RasPi doesn't have anything that should be making a sound, so if it is something is broken.  I recommend checking various voltages with a multimeter: 5V, 3.3V, 1.8V, etc.  A stethoscope or even a drinking straw might help localize where the sound is coming from.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    It is a high pitched voice. After some googling, I believe that my situation is somewhat like this(except that my pwr will always lit) https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=124239 I'll get myself a multimeter later as well as to boot the pi up from gpio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to wcypierre

    wcy pierre wrote:

     

    Just an update, got the multimeter and I did the voltage test(RPi Hardware - eLinux.org ) and it seems normal though (5.16v). Did the test for the voltage coming from psu and after passing through the polyfuse(R-Pi Troubleshooting - eLinux.org ) and the difference is only 0.1v (5.16v vs 5.15v), which seems to be normal by referring to the links above. Any other ideas?

    When I commented earlier about L1 and L2 I had assumed you had a RasPi B+.  As Shabaz says, the original B didn't have switching regulators for 3.3V and 1.8V.  However, it does have a switching regulator for the low voltage that powers SoC internal logic.  This regulator is built into the SoC except for external inductor L5, so if L5 is loose you could get a whine.  The other possibility is a crystal.  If one of those is loose its vibration could stimulate an audible harmonic somewhere.  Some very early RasPis had trouble with crystals that weren't soldered on properly, so check the solder joints with a magnifier.

     

    Since you have an original RasPi Model B, you can look at the schematics and check whether all the voltages are OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to johnbeetem

    It is amazing how much confusion the Pi naming has caused over the years when responding to RPI issues. I thought it was common sense that ideally one aims to change model name/numbers in one dimension only, or have a reasonable numbering scheme with (say) series and other key attributes encoded within the numbering. But the Pi starts with nostalgia and 'Model A' and 'Model B' naming, and then hardware revisions encoded in revision number (the 'late' model B as I remember), and then appending an operator (the 'plus' variants) and then a version number (not a revision number) with the Pi 2, and removing the operator!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    I've taken a glimpse at the schematics, and which are the ones that I should look into?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to shabaz

    Exactly. Not to mention that, since Model A and Model B, B+ are referred Pi 1 Model A/B/B+ respectively, then there's also a weird numbering scheme where it goes from 1 to 2 and then back to 0?

     

    Pi 1(A, B with multiple revisions, B+) -> Pi 2 -> Pi 0?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to wcypierre

    Yes, they actually added another two dimensions to the naming scheme with the latest Pi.

    The first dimension they added was the size or functionality aspect, so that the zero implies it is smaller or less functional than the other Pi's.

    It can't be performance related, because the Zero has similar performance to the model A, and B, so it follows that the zero is not the same meaning as the '2' in Pi 2 which is perhaps performance related.

    The other kind-of dimension is the spelling, because the latest one is 'Zero', not '0' image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to wcypierre

    wcy pierre wrote:

     

    I've taken a glimpse at the schematics, and which are the ones that I should look into?

    Here are the released schematics: https://www.raspberrypi.org/documentation/hardware/raspberrypi/schematics/README.md

     

    You want the MODEL A AND B schematics for whichever revision is printed on your PC board.  The original Model A and B used the same PCB.  The B+ and A+ have different size boards and would have different schematics (if the were published image)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to shabaz

    Agreed but when people hear pi 1, pi 2 and pi zero, they tend to think of the 'Zero' as '0' though. Regardless, hopefully they won't have a weird naming scheme in the future causing more and more confusion

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    Like what I've said earlier, I've taken a look at the schematics, but what are the things that I need to check out?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago in reply to johnbeetem

    John Beetem wrote:

    The B+ and A+ have different size boards and would have different schematics (if the were published )

    They probably have different schematics regardless of whether or not they are publishedimage

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to wcypierre

    wcy pierre wrote:

     

    Like what I've said earlier, I've taken a look at the schematics, but what are the things that I need to check out?

    Start by checking the supply voltages.  TP1 to TP2 gives you 5V (which you already checked, IIRC) and then 3.3V, 1.8V (at the regulator and at the USB LAN chip), 2.5V, and VDD_CORE which is probably around 1.2V.  It's the SoC internal voltage and is programmable to allow over-volting.

     

    If a critical supply voltages is bad, nothing else is going to work so no point in checking anything else until you can fix the supply voltage.  If they're all OK, it's something else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 10 years ago in reply to wcypierre

    wcy pierre wrote:

     

    Like what I've said earlier, I've taken a look at the schematics, but what are the things that I need to check out?

    Start by checking the supply voltages.  TP1 to TP2 gives you 5V (which you already checked, IIRC) and then 3.3V, 1.8V (at the regulator and at the USB LAN chip), 2.5V, and VDD_CORE which is probably around 1.2V.  It's the SoC internal voltage and is programmable to allow over-volting.

     

    If a critical supply voltages is bad, nothing else is going to work so no point in checking anything else until you can fix the supply voltage.  If they're all OK, it's something else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    Thanks. I'll check it out over the weekend(or maybe the following weekend, depending on how fast I can understand this thing).