Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi won't boot with noise and PWR lit only
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 708 subscribers
  • Views 7211 views
  • Users 0 members are here
  • problem
  • issue
  • raspberry_pi
  • raspberrypi
  • boot
Related

Pi won't boot with noise and PWR lit only

wcypierre
wcypierre over 10 years ago

Had been running this pi for 24x7 for about a year now and it has been running fine until I realized that it was down just now when I went to do some checking.

Heard some noises too and now I can't seem to get it back up (noise + PWR lit + dim ACT light only).


Model: Raspberry Pi B

OS: Raspbian

Things attached to the pi: LAN cable, SD Card

Video to demonstrate the noise that the pi makes: https://drive.google.com/file/d/0BwiJswXag8O4dkNKbmlmRVBKOW8/view?usp=sharing


Note: I'm using Powerbank to power the pi up just for the sake of taking the video, normally it is attached to a better power supply.


Symptoms:

1. Red PWR light

2. dim ACT light

3. Noise made as per video above


Things that I've tried:

1. Changing the Power Supply(tried from my original source to genuine Pineng Powerbank to Nokia's official charger to Xiaomi's official charger to the charger that was shipped with the pi)

2. SD Card (it was working on the other pi and the other sd card that I've put into from the other pi doesn't work)

3. LAN cable

4. HDMI - No output

5. Composite - No output

6. Heating it up (https://www.youtube.com/watch?v=AwF6v-4NFdg)

7. Holding the sdcard slot to ensure that the issue isn't with the sd card slot

8. R-Pi Troubleshooting - eLinux.org (the "Red power LED is on, green LED does not flash, nothing on display" part)


Things that I know but I couldn't try because of limitations:

1. Serial console


Any other things that I can try of?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    Can someone describe the sound?  I don't have speakers handy.

     

    RasPi doesn't have anything that should be making a sound, so if it is something is broken.  I recommend checking various voltages with a multimeter: 5V, 3.3V, 1.8V, etc.  A stethoscope or even a drinking straw might help localize where the sound is coming from.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    It is a high pitched voice. After some googling, I believe that my situation is somewhat like this(except that my pwr will always lit) https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=124239 I'll get myself a multimeter later as well as to boot the pi up from gpio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to wcypierre

    imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to wcypierre

    wcy pierre wrote:

     

    It is a high pitched voice. After some googling, I believe that my situation is somewhat like this(except that my pwr will always lit) https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=124239 I'll get myself a multimeter later as well as to boot the pi up from gpio

    A high-pitched screech (or whine, depending on how sensitive your ears are) is probably one of the inductors L1 or L2.  As mahjongg suggests at the link, it could be that the switching regulator is overloaded.  This can happen if a chip fails with a short, and may not be repairable.  It could be a spec of conductive debris has shorted out a couple of pins, which might be able to be blown out with air.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    I'll wait for a few days while I wait for my multimeter to arrive, and I get the feel that its dead too. I guess its a sign for me to a Pi2!

     

    And if you don't mind, can you take a look at my other pi at the other thread (http://www.element14.com/community/message/171195/l/pi-pwr-off-but-others-are-on#171195)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    anyway, while waiting for my multimeter to come from China(which should arrive by the end of this week), I've realized that my other rpi can be powered by usb ttl cable while I was testing serial connection to my rpi(despite that I can't ssh into it because of the wifi adapter using too much of power I guess), but is the idea of powering up my "faulty" rpi uses the same concept?

     

    I'm following this link:

    https://learn.adafruit.com/adafruits-raspberry-pi-lesson-5-using-a-console-cable/connect-the-lead

     

    EDIT: ontopic, I've tried it out and it still makes out the high pitched voice, so I guess that's it for my rpi? and to clarify, I'm only powering the pi via 5v gpio, and I'm not powering it up using usb as well.

     

    EDIT: offtopic, but it is because of the wifi adapter using too much of power so I can't ssh into my other rpi, removed the wifi adapter and I can ssh into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to johnbeetem

    Just an update, got the multimeter and I did the voltage test(RPi Hardware - eLinux.org ) and it seems normal though (5.16v). Did the test for the voltage coming from psu and after passing through the polyfuse(R-Pi Troubleshooting - eLinux.org ) and the difference is only 0.1v (5.16v vs 5.15v), which seems to be normal by referring to the links above. Any other ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to wcypierre

    If you've been hearing sounds that sounds like a faulty DC-DC converter. The older Pi's don't have DC-DC converters in-board. So the sound probably came from the thing that was powering your Pi's. It could have damaged them beyond repair. A multimeter alone won't reveal what your supply rail looks like. Replace the supplies, if that doesn't resolve things then replace the Pi's..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago in reply to wcypierre

    If you've been hearing sounds that sounds like a faulty DC-DC converter. The older Pi's don't have DC-DC converters in-board. So the sound probably came from the thing that was powering your Pi's. It could have damaged them beyond repair. A multimeter alone won't reveal what your supply rail looks like. Replace the supplies, if that doesn't resolve things then replace the Pi's..