Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Microsswitch or Breadboard control
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 537 views
  • Users 0 members are here
  • raspberry_pi
Related

Microsswitch or Breadboard control

e14 Contributor
e14 Contributor over 10 years ago

Hello,

 

I am new to Raspberry Pi's however have a Developer background. I am hoping for some assistance creating a BOM to start making a small prototype for fun. What i wish to achieve is capture the response of some push buttons mounted on a board. I wish for the button to be illuminated when on and if button's 1, 6 or 9 are pushed for it to increase brightness momentarily then go back to its normal "on" state. What i was hoping to find out is it best off having a OTS 12v LED microswitch (like attached for testing. I will acquire the mounting caps separately) complete this illuminating actions or control this action using a LED wired into a breadboard to control the event?

 

Either option I was hoping for assistance in building a BOM of compatible components so I can purchase the equipment and start trailing/building on some very basic Python code I've written.

 

Obvious equipment so far Raspberry Pi 2, 8GB MicroSD, 5v Micro USB, Expansions Board & Jumper Wire Kit(recommendations appreciated).

 

Thanks!

Attachments:
image
  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    What is it your trying to do, it would seem on the face of it to be way over complicating it by using a RPI2 to read a few buttons and illuminate indicators

     

    There must be more to it, if not, have you considered something like an Arduino UNO or one of the less expensive clones

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    We are trying to create a physical interactive element of an existing questionnaire platform. I am trailing/trying to make a combination of 1 x 2, 1 x 3, 2 x 2 and 3 x 3 Push Button board an extension the existing questionnaire. The questionnaire consists of basic close ended question web form's(LAMP) with pre-recorded vocals of the question being output to a display/speakers. The purpose of what we am trying to trial is to incorporate a large board with push button functionality with the web form to capture feedback from the user, the reason behind the physical element of the questionnaires are specific to people with a disabilities. The end goal will be to see if the physical push button element engages the user more then the web-form with mouse-click alone.

     

    Questionnaire can be as simple as:

         2 x Buttons Yes/No question set may be be "Are you happy?"

         3 x 3 Buttons 1-9 question set "How many cat's can you see?"

     

    Using large illuminated push buttons with clear plastic caps will allow for a simple printed words, colours, numbers, icons or a combination to be interchangeable on the buttons depending on the questionnaire.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    I'm with Peter on this.

    An Arduino will easily do the button detection/illumination.

     

    You can use analog input and wire the switches so that pressing one results in a voltage change.

    It is much easier than trying to detect rows and columns.

     

    Mark