Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Not Open Source Hardware.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 708 subscribers
  • Views 3874 views
  • Users 0 members are here
  • raspberry_pi
Related

Not Open Source Hardware.

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

Firstly, I would like to make clear that I am a huge fan of the Raspberry Pi and I cannot wait to pick one (or three!) up for myself. However, can we just set the record straight: it is not open source hardware — the schematics and/or Gerber files etc. are not provided and made available under a suitably liberal licence, i.e. as per:

 

http://www.opensource.org/osd.html

 

It runs open source software, but then so can an Apple laptop and an IBM mainframe. Please cease referring to this as open source hardware, which is something quite different. For further clarity, see:

 

http://freedomdefined.org/OSHW#Open_Source_Hardware_.28OSHW.29_Definition_1.0

 

and:

 

http://wiki.openhardware.org/Project:Certified_Open_Hardware_License_Approval_Process

 

This is not to downplay the RP which is an incredible achievement, and having met David and Liz last year and discussed this with them I have a little insight into perhaps why it is, for now at least, a proprietary (closed) hardware design.

 

Regards,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Cabe,

     

    You've completely missed the point of open source. It's not about what you or I think anyone might want to do, or about our notions of what is and isn't economically viable. The fact is that the term "open source hardware" means something very specific and given where we are on the adoption curve, that tons of the stuff is out there and well known definitions exist, there is no reasonable excuse for bending that defition so far from its intended, and widely accepted, meaning.

     

    I also hear the point about the Broadcom SoC, however, if this were an open source design I could rip that out and replace it with another piece of silicon. Whether or not this would be economically viable, or the RP Foundation or Broadcom would be pleased, would be neither here nor there: with an open source hardware design I would be free to do as I please.

     

    Regards,

     

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Zaragon
    Zaragon over 14 years ago in reply to e14 Contributor

    I actually find all this discussion about open hardware and what is or isn't really funny. How many of these open source hardware are really as open as they expound. Those that use electronic component do they make available the actual die designs and lithograph plates or are they closed design proprietry designs? Afterall if you have the capabilities to make chips those would allow you to make your own. If not why is it OK to use closed source non CPU chips when it isn't alright to use a closed source CPU chip?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to Zaragon

    You raise a good point - almost all Open Source Hardware project I know of are only open down to some level of abstraction.  That tends to be the silicon.  There are efforts like OpenCores to even open up that aspect but I think that is quite a bit far off for many applications. 

     

    There was a good presentation on this topic at the Open Source Hardware Summit:

     

    http://www.openhardwaresummit.org/wp-content/uploads/2011/09/Open_Sourcing_the_IC-s.pdf

    [PDF]

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 14 years ago in reply to Zaragon

    You raise a good point - almost all Open Source Hardware project I know of are only open down to some level of abstraction.  That tends to be the silicon.  There are efforts like OpenCores to even open up that aspect but I think that is quite a bit far off for many applications. 

     

    There was a good presentation on this topic at the Open Source Hardware Summit:

     

    http://www.openhardwaresummit.org/wp-content/uploads/2011/09/Open_Sourcing_the_IC-s.pdf

    [PDF]

     

    Cheers,

    Drew