Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Not Open Source Hardware.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 708 subscribers
  • Views 3820 views
  • Users 0 members are here
  • raspberry_pi
Related

Not Open Source Hardware.

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

Firstly, I would like to make clear that I am a huge fan of the Raspberry Pi and I cannot wait to pick one (or three!) up for myself. However, can we just set the record straight: it is not open source hardware — the schematics and/or Gerber files etc. are not provided and made available under a suitably liberal licence, i.e. as per:

 

http://www.opensource.org/osd.html

 

It runs open source software, but then so can an Apple laptop and an IBM mainframe. Please cease referring to this as open source hardware, which is something quite different. For further clarity, see:

 

http://freedomdefined.org/OSHW#Open_Source_Hardware_.28OSHW.29_Definition_1.0

 

and:

 

http://wiki.openhardware.org/Project:Certified_Open_Hardware_License_Approval_Process

 

This is not to downplay the RP which is an incredible achievement, and having met David and Liz last year and discussed this with them I have a little insight into perhaps why it is, for now at least, a proprietary (closed) hardware design.

 

Regards,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Interesting thing about this device is that it isn't much different from cheap wifi routers, except routers do not have GPU, but have case, wall wart and wifi built in. Nobody gets too excited about cheap wifi routers these days image
    So what is so much different about Raspberry Pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I think this thread is hilarious. someone said open source hardware instead of open source.

    Having been up since 5 am and still not managing to order one, I think some should unregister their interest to spend some more time discussing this, and allow me to move up the queue.

     

    He He. Just injecting a bit of lightheartedness to lighten my foul mood at not getting an order in.... !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I think this thread is hilarious. someone said open source hardware instead of open source.

    Having been up since 5 am and still not managing to order one, I think some should unregister their interest to spend some more time discussing this, and allow me to move up the queue.

     

    He He. Just injecting a bit of lightheartedness to lighten my foul mood at not getting an order in.... !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    There has been a lot of interesting and useful discussion. And again, just to make clear, I think that the RP is incredibly worthwhile, a great achievement, and I'm not criticising the RP Foundation here for the approach that they have taken. Rather instead I'm calling out the error in referring to this as "open source hardware" — which it emphatically is not.

     

    Open source hardware means something very specific, as does open source software, and "open source" in and of itself is ambigous. I've heard quite a few times the RP being referred to as open source hardware, with comparisons being made to Arduino and BeagleBoard etc, and this is extremely misleading and akin to suggesting that MS Word is open source because you could write an open source novel using it.

     

    The open source hardware movement has seen exponential growth, is receiving a lot of interest, and with players such as Facebook and Ford Motor investing heavily, and coverage from the likes of Forbes and the Economist etc. The conflation of markedly proprietary hardware and open source hardware is most unhelpful, and does a disservice to those who take the leap of faith and publish hardware design artefacts under a liberal license.

     

    On of the matter of using non-open source components in a design — we mostly don't have much choice, and the generally accepted community norm would be open source schematics, BoM and Gerbers, and HDL source too if there is there is an FPGA in the design. If you produce a design with no schematics made available under a liberal license, it cannot be regarded as open source hardware. Simple.

     

    Finally, and just to make absolutely clear: I'm not downplaying the RP, and I'm not nit-picking — but to call the RP open source hardware is disingenous at best.