Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Not Open Source Hardware.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 708 subscribers
  • Views 3825 views
  • Users 0 members are here
  • raspberry_pi
Related

Not Open Source Hardware.

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

Firstly, I would like to make clear that I am a huge fan of the Raspberry Pi and I cannot wait to pick one (or three!) up for myself. However, can we just set the record straight: it is not open source hardware — the schematics and/or Gerber files etc. are not provided and made available under a suitably liberal licence, i.e. as per:

 

http://www.opensource.org/osd.html

 

It runs open source software, but then so can an Apple laptop and an IBM mainframe. Please cease referring to this as open source hardware, which is something quite different. For further clarity, see:

 

http://freedomdefined.org/OSHW#Open_Source_Hardware_.28OSHW.29_Definition_1.0

 

and:

 

http://wiki.openhardware.org/Project:Certified_Open_Hardware_License_Approval_Process

 

This is not to downplay the RP which is an incredible achievement, and having met David and Liz last year and discussed this with them I have a little insight into perhaps why it is, for now at least, a proprietary (closed) hardware design.

 

Regards,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I think one of the reasons to be a "Not Open Source Hardware", have to be with codecs licensing. They have "closed source libraries that give access to the GPU acceleration features."

     

    http://thedigitallifestyle.com/w/index.php/2012/01/31/raspberry-pi-detail-system-libraries-and-codecs-support/

     

    I think that the GPU can hardware decode more codecs than only MPEG4 and h.264, but they have to limit that whit the closed libraries, because the device would be more expensive only to pay royalties to patents holders of the additional codecs 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    I think one of the reasons to be a "Not Open Source Hardware", have to be with codecs licensing. They have "closed source libraries that give access to the GPU acceleration features."

     

    http://thedigitallifestyle.com/w/index.php/2012/01/31/raspberry-pi-detail-system-libraries-and-codecs-support/

     

    I think that the GPU can hardware decode more codecs than only MPEG4 and h.264, but they have to limit that whit the closed libraries, because the device would be more expensive only to pay royalties to patents holders of the additional codecs