Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can Raspberrypi boot initially from USB stick
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 710 subscribers
  • Views 3680 views
  • Users 0 members are here
  • raspberry_pi
Related

Can Raspberrypi boot initially from USB stick

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

As i usually install software via USB stick i wonder, will RaspberryPI also install when bootable USB stick is inserted into the USB slot?

 

E.g. can i bypass in this manner the creation of the bootable SD card.
And just have the install process of the image do the job for me, just like an average installation on a disk. In this case it will be a SD card.

 

Thanks for sharing.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Most modern BIOS chips allow / can be updated to set a USB port device as bootable.

    I can't see any reason why this should be any different.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    One very clear and obvious reason why this is different is because the Raspberry Pi's architecture does not have or need a BIOS chip at all.  There are *no* choices about the initial boot, no "BIOS settings" to be made or altered at all - the GPU powers up and has a very very small set of hardcoded instructions that say "Go initialise the SD card and look for the first FAT32 partition and look for a firmware file there".  That firmware then kickstarts the ARM processor, which loads a kernel from the SD card.  After that, the standard distributions will typically mount a root filesystem from the SD card as well, but it's possible to mount a root filesystem from some other USB device instead - no choice in the matter till this point though, and absolutely impossible to boot initially without an SD card with the right firmware files on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hmmmm interesting - BIOSlessness...............

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    Or, to put it another way, the RasPi BIOS is in the SD card.  You want to update the BIOS?  Just write new files to the SD card.  I think BIOS settings are in a file called "config.txt" on the SD card, but I'm not sure and haven't looked at details.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    Or, to put it another way, the RasPi BIOS is in the SD card.  You want to update the BIOS?  Just write new files to the SD card.  I think BIOS settings are in a file called "config.txt" on the SD card, but I'm not sure and haven't looked at details.