Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Not Linux, Not Windows, But...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 708 subscribers
  • Views 2888 views
  • Users 0 members are here
  • raspberry_pi
Related

Not Linux, Not Windows, But...

e14 Contributor
e14 Contributor over 14 years ago

I want to run DOS and ML on this thing. Will I have to build this environment myself? I'm not a Linux fan, and not interested in building yet another Windows machine-let!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    You could download FreeDOS source and build it yourself, piece-by-piece, for the ARM arch.

     

    http://sourceforge.net/scm/?type=svn&group_id=5109

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I am not sure getting FreeDOS would work, or even if it worked if it would be useful.

    It doesnt appear that FreeDOS has been ported to ARM architecture yet - I think because it doesnt have a hardware extraction layer it assumes it is running on x86, so porting to another CPU architecture is very hard.

    Even if you could get FreeDOS running on your pi, very few applications (or old games) would work as they would need recompiling to run run on ARM architecture.

     

    A better solution would be to run DOSbox on linux and run your old software that way.

     

    What I really want though is BBC emulator running so I can say to my kids - look this is what I had when I was young image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ricnev
    ricnev over 14 years ago in reply to e14 Contributor

    There is a story going round that one of the people involved in the Raspberry Pi Foundation is keen to see RISC OS ported to RasPi because in his youth he wanted a Risc PC, but couldn’t afford one. If RISC OS does become a viable OS on a RasPi, there are BBC B emulators which will run on it. I think there are also some BBC B emulators for Linux - perhaps these'll work with the distros RasPi will be using.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ricnev
    ricnev over 14 years ago in reply to e14 Contributor

    There is a story going round that one of the people involved in the Raspberry Pi Foundation is keen to see RISC OS ported to RasPi because in his youth he wanted a Risc PC, but couldn’t afford one. If RISC OS does become a viable OS on a RasPi, there are BBC B emulators which will run on it. I think there are also some BBC B emulators for Linux - perhaps these'll work with the distros RasPi will be using.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to ricnev

    I really wanted an archimedes when it came out. I wonder if RISC OS is ported if I will finally be able to play zarch.

     

    just thinking about this - as its based on an ARM chip, perhaps somebody could get android running on it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Cylon
    Cylon over 14 years ago in reply to e14 Contributor

    i suggest you start here.http://www.riscos.org.uk/

     

    There is a huge ammount of work already to port it to PI.

     

    Wont be long now.