Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum two questions: why USB2 instead of USB3 and will there be a multi-nic version at some point?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 710 subscribers
  • Views 2578 views
  • Users 0 members are here
Related

two questions: why USB2 instead of USB3 and will there be a multi-nic version at some point?

e14 Contributor
e14 Contributor over 14 years ago

Why is the PI using USB2 instead of USB3 at this point and is there any plan to come out with a multi-nic version of the card?  I can see this being used as a very nice little firewall if one could stack, say, 3 nics on the card.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    RasPi's BCM2835 only has a USB 2.0 port.  The Model B hooks this up to an SMSC LAN9512 2-port USB hub with Ethernet.  Given that the connection to the CPU is USB 2.0, there is really no point to hooking it up externally to anything faster.  If you want a high-performance firewall, you'll need something with built-in Ethernet ports.

     

    The raspberrypi.org site is still suspended due to high traffic of loyal Razzers seeing if it's back up yet.  However, you can get RasPi technical information at the Wiki: http://elinux.org/RaspberryPiBoard and http://elinux.org/Rpi_Hardware.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

     

    During the design of RPi we had to make lots of difficult decisions about what to put on and what to leave off.

     

    Once we had the basic functionality for running Linux and getting a display, pretty much everything else came down to space and/or meeting the cost target we had set.

     

    Although we had other ports that we could have probably added more Ethernet Functionality to it would have significantly added to the complexity of the design. The SMSC LAN9512 works brilliantly for us as it gives us the Ethernet and a second USB in a very cost effective way.

     

    The model A dispenses with this chip and we run the BCM2835 USB straight out.

     

    To get round this limitation what most people are planning is to use a 3-4 port USB Hub, wire one back to the Micro USB on the RPi to provide the power (we can do this as the data pins are not connected) and it then gives 3 spare ports for mouse, keyboard, memory stick etc.

     

    We have tried to give as many routes to expand the RPi as possible but have not compromised the baseline price points. So onboard Camera, Wifi, LCD drive and other good stuff got trimmed off the wish list fairly early on.

     

    We have also been asked quite a bit about Power over Ethernet but if you look at the demand trail it has mainly come from application ideas well away from our original goals.

    Let us know what you think, have we made a ‘wrong turn’ in our drive to Raspberry Pi Models A and B?

     

    Cheers – Pete

    Trustee and part of the Hardware Design Team.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

     

    During the design of RPi we had to make lots of difficult decisions about what to put on and what to leave off.

     

    Once we had the basic functionality for running Linux and getting a display, pretty much everything else came down to space and/or meeting the cost target we had set.

     

    Although we had other ports that we could have probably added more Ethernet Functionality to it would have significantly added to the complexity of the design. The SMSC LAN9512 works brilliantly for us as it gives us the Ethernet and a second USB in a very cost effective way.

     

    The model A dispenses with this chip and we run the BCM2835 USB straight out.

     

    To get round this limitation what most people are planning is to use a 3-4 port USB Hub, wire one back to the Micro USB on the RPi to provide the power (we can do this as the data pins are not connected) and it then gives 3 spare ports for mouse, keyboard, memory stick etc.

     

    We have tried to give as many routes to expand the RPi as possible but have not compromised the baseline price points. So onboard Camera, Wifi, LCD drive and other good stuff got trimmed off the wish list fairly early on.

     

    We have also been asked quite a bit about Power over Ethernet but if you look at the demand trail it has mainly come from application ideas well away from our original goals.

    Let us know what you think, have we made a ‘wrong turn’ in our drive to Raspberry Pi Models A and B?

     

    Cheers – Pete

    Trustee and part of the Hardware Design Team.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • baz4096
    baz4096 over 14 years ago in reply to e14 Contributor

    Hi Pete

     

    Thanks for the reply. I've got absolutely no problem with the hardware decisions you've made, especially considering you're primarily catering for the educational market! I'm sure as costs come down and you start getting more feedback from users you'll probably add new functionality into the next generation of RPi, however for the time being, I think you guys have done a fantastic job.

     

    I'm also looking forward to seeing the latest demo of RISC OS running on an RPi in Wakefield next month, now that would definitely rekindle some fond memories - I just hope I can ressurect my 120MB harddrive from my old Acorn A3010 and retrieve my first few years worth of programming!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hey Pete,

    Thanks for clearing that up, now I personally understand why you did what you did to cut down on the price. Are there any future plans though to create a more full-featured version of the RPi? For those kids who have learned the basics with the RPi, would there then be a more advanced version for the next step for them, and for the community that wants to use them and develop them more than they could with the RPi that is currently out? This would then challenge the kids farther and also stimulate the communities minds about possible developments to the RPi.