Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Further possible delays to the Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 706 subscribers
  • Views 1660 views
  • Users 0 members are here
  • raspberry_pi
Related

Further possible delays to the Pi

GreenYamo
GreenYamo over 14 years ago

Don't know if you are generally aware of this, but it looks like there could be further delays to the Pi according to a recent blog post:

 

http://www.raspberrypi.org/

 

Incorrect RJ-45 sockets sourced by the manufacturers....

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    It is quite normal for the manufacturer to perform only an electrical test. It is the responsibility of the integrator (in this case the RPi Foundation) to perform the protocol tests. There is nothing unusual in the acceptance tests of the RPi.

     

    The problem was compounded by the fact that the manufacturer seems to have used the correct jack for the trial production run, which did pass the protocol tests. The manufacturer then used the incorrect jack for the real production run. This is a rare event, but this is why there are so many tests to ensure that faulty devices do not shipped to customers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to e14 Contributor

    In my experience it is usual for the manufacturer to perform complete end of line testing which should be designed to ensure 100% functionality of the part. Any reasonable test would show up the difference between a jack with magnetics and one without.

    I doubt that the RPi Foundation going to 100% test the boards when they arrive in the UK so one is left wondering if they have any proper test plan at all.

     

    Michael Kellett

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 14 years ago in reply to e14 Contributor

    In my experience it is usual for the manufacturer to perform complete end of line testing which should be designed to ensure 100% functionality of the part. Any reasonable test would show up the difference between a jack with magnetics and one without.

    I doubt that the RPi Foundation going to 100% test the boards when they arrive in the UK so one is left wondering if they have any proper test plan at all.

     

    Michael Kellett