Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum A Blood Curdling Scream!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 708 subscribers
  • Views 2920 views
  • Users 0 members are here
  • raspberry_pi
Related

A Blood Curdling Scream!

jack.chaney56
jack.chaney56 over 10 years ago

Do not let this happen!

 

image

 

i saw the newest RPI weekly with the picture of the new weather station package, and noticed the warning label "Oracle". I understand they are a great group that is happy to provide support to the Raspberry Pi community, but believe me, it is never without a cost. Case in point, MySQL, used to be free and released under the open source agreement, but when Oracle purchased Sun, it decided to include MySQL in with the assets, and now, for extended capabilities, like re-selling an application using the core module, requires purchase of a license. MySQL was incorporated under the GPL, which doesn't change based on who is supporting it.

 

My comment for this discussion is to serve as a warning, beware of a wolf in sheep's clothing.

 

Jack

  • Sign in to reply
  • Cancel
Parents
  • jack.chaney56
    jack.chaney56 over 10 years ago

    Just realized... This is probably a bad day to be confronting the establishment.  For those that understand, just smile and wish me luck.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to jack.chaney56

    Jack, Although they have started offering licences for MYSQL, that is mostly optional. Nobody is forced to buy that licence. And there are very little cases where anybody would want to or need to  to buy that licence.

     

    MySQL :: Commercial License for OEMs, ISVs and VARs

     

    Although they worded it a bit cryptic trying to try to include a few more cases, you would only have to buy the licence if you took the open source MySQL sources, added a few extensions for your own use-case, and then are selling the combination, while you're unwilling to provide sources for the extension that you made.

     

    This case now requires a licence, which previously was either impossible or otherwise not publicly offered.

     

    When e.g. you'd build a Linux-based "appliance" which includes a MySQL database, and you inlcude a few closed-source applications, then you still are NOT required to purchase a licence. This is the case that they are obfuscating a bit. (of course they didn't mean to).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to rew

    I am afraid this is going to launch into a rather heavy discussion.  You pointed directly to the issue at hand. The line:

     

    "This case now requires a license, which previously was either impossible or otherwise not publicly offered."

     

    should say instead ...was not necessary.  The usage agreement of GPL (oh, by the way the "L" stands for license) is quite clear, which is a free use, (free like beer, not freedom), and if improvements are made, they are to be returned to the community.  That is the contract, and yes, it is a contract. If you do a quick search to get the history lesson, you will see that back when the GPL was being crafted, it was litigated and refined by a substantial number of lawyers at the corporate and private levels to make sure it was air tight.  To say that it requires a license is correct, but it has a license. To say that it was not offered is incorrect, because it was already in place (though not in the best interest of the company).

     

    Jack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to jack.chaney56

    What I mean with "this case" is: if you want to "improve" as you call it and THEN distribute your work along with the original GPL stuff, without providing source to your improvement. That is what the GPL disallows. As you say, the licence (GPL) allows a lot, but not that.


    If the person or entity holding the copyright does not offer dual licencing and you still want to do that, it is not allowed.

     

    The GPL says nothing about money. (Free as in beer). I can (and have) improve on GPL code, and sell it. GPL then requires me to provide the sources (if they ask) to anybody who got the binaries from me. GPL says nothing about putting it on the internet, or requiring my sale of the improved version to be "free". However, my first client is then (again according to the GPL) allowed to sell copies of MY improved code, or put it on the internet. This would kind of spoil my market. The GPL thus causes most GPL-ed programs to be "free-as-in-beer", because if you'd ask for even a small amount, the guy next door (and/or your first client) can do it for free.

     

    Also note that the GPL is perfectly fine with me improving a GPL-ed program in-house and then "not giving back". But as soon as I give or sell the improved version to someone else, I'm required to provide the sources to my changes to them. And they get the right to redistribute / resell / publish the whole thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to rew

    Is this actually "left copyrighted"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to rew

    Is this actually "left copyrighted"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to clem57

    Thanks Clem, and it was, yes "copyleft" is the term that I have heard.

     

    Jack