Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum WINE Support
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 704 subscribers
  • Views 2139 views
  • Users 0 members are here
  • dvr
  • security
  • wine
  • windows
Related

WINE Support

e14 Contributor
e14 Contributor over 14 years ago

[Forgive me for such a noob question.  I'm not well versed in Linux and have never tried to use WINE.  That said...]

 

Will the RPi support an installation of WINE; specifically WINE running ContaCam?

 

I am interested in running ContaCam (http://www.contaware.com), a Security Serveillance application with motion detection, DVR, integrated web server, supporting webcams, WDM and DV, and IP cameras.  It's feature set is exactly what I need and I am familiar with the application.  I know ContaCam will run in WINE, but I have no idea if WINE will run on RPi and even if it will then are the resources required by ContaCam available.  When looking at Windows Task Manager, I see that ContaCam is taking about 65,000 K in resources.

 

Thanks in advance,

Andrew

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    Interesting question.  I've seen a few folks asking if it will run Windows which it definately can not.  However, if their interest is to run a specific Windows app like you, then I could see how WINE could be a good solution.

     

    There is a developer VM that Russell Davis created which allows folks to get started building software for the Raspberry Pi on their x86 computers.  You might want to check it out and see if WINE is an available package for either of the existing RPi distros (the VM includes all 3).  If not, you can try to compile compile it in the VM.  Here's more info on the dev VM:

     

    http://www.element14.com/community/message/47127

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Thanks.  I was thinking of trying the VMs, but thought I'd ask first.  I've used VMs quite a few times, but never paid much attention to the RAM & CPU settings.  If I recall, they default to a percentage of the RAM that I have avaliable and utilize as much CPU as they can.  I guess I'll need to look and see if these VMs throttle these settings to something realistic for RPi (256mb/700mHz).

     

    Thanks again,

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Thanks.  I was thinking of trying the VMs, but thought I'd ask first.  I've used VMs quite a few times, but never paid much attention to the RAM & CPU settings.  If I recall, they default to a percentage of the RAM that I have avaliable and utilize as much CPU as they can.  I guess I'll need to look and see if these VMs throttle these settings to something realistic for RPi (256mb/700mHz).

     

    Thanks again,

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Actually, I just realized that I wasn't thinking about ARM versus x86.  I think a Windows x86 VM wouldn't run on an ARM device like the Pi (and memory would probably be an issue, too).

     

    I also suspect that a x86 Windows app wouldn't run on ARM with WINE either.  But one way to find out would be to use the developer VM to try to compile WINE for the Raspberry Pi.  (The point of the developer VM is that is has scratchbox setup which allows you to build [aka cross-compile] software for any of the 3 ARM Linux distros available for the Raspberry Pi.)

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    image  I guess it comes back around to my original question, "Will the RPi support an installation of WINE..."?  I can do the experimentation myself, but if someone already knows the answer then it will let me use the time to move on to other areas of the project.

     

    And if it turns out that ContaCam can't be run then I'm open to suggestions of a reasonably full featured application that will at the least detect motion (with sensitivity adjustments), capture still images of the triggering event, and capture video of the triggering event.

     

    Thanks again,

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 14 years ago in reply to e14 Contributor

    I vaguely recall a university project called CUCAM which might have the souce code available for cross compile.  Somewhere I think I have the bundle downloaded.