Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Would this work for a handheld DVR?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 708 subscribers
  • Views 1287 views
  • Users 0 members are here
  • help
  • raspberry_pi
  • touchscreen
  • video_compression
Related

Would this work for a handheld DVR?

e14 Contributor
e14 Contributor over 14 years ago

Hello All, I plan to develop a small handheld digital video recorder, and it looks like the Raspberry Pi might be just the piece of base-kit I've been looking for!

 

For the basic device, I need to connect an LCD touchscreen to it, which I would guess I can do via one of the USB ports, and a composite video (CVBS) input.  For future use, I'll need ADC and CAN-comms inputs, but that all looks fairly straight-forward, based on what I can see from the specs docs.

 

I was looking at the Beagleboard for this initially, but I hope to make small batch production runs with it for a business start-up.  The Beableboard people repeatedly say that it's not suitable for production runs, but don't say why unfortunately, so that's why I'm now pinning my hopes on the Raspberry Pi.

 

Can anyone out there help me out with these questions:...?

- From reading through the spec and some of the posts here, it looks like there is plenty of power to decompress a digital-video file and drive out a video stream to the HDMI or Video port, but what about the other way around - compressing a video input stream?  Is the MIPS of the ARM core and the available memory on the Raspberry Pi board enough to compress a video input stream (probably H.264), in readiness for storage to some kind of mass media (SD-Card, or possibly a USB SDD)?
- I see that there is something called a 'Camera Port' on-board, but can't find out much about it - is this suitable for composite video input, or is it for something else entirely?
- In case I can't connect a CVBS signal straight into the board, for a backup I've also been looking for a piece of hardware that I could use for digitising a CVBS input into a USB port, but the only one I've found that's even close to what I need costs a small fortune, and knocks my target price for six!  I want to get hold of somethig like those cheap bits of video=>PC conversion gadgets that are in abundance on eBay (etc), but that also allows integration into other systems.  Does anyone in the community know of such a thing for around £20?
- I want to use a touchscreen input to side-step the logistical complexity of having user-buttons read into the GPIO ports - is USB the only way I'm likely to be able to get a touchscreen input into the Raspberry Pi, or does anyone know of a device that would enable me to hook a touchscreen up to an interface that's already on the board?
- Lastly, is the Raspberry Pi suitable for what I want to do, or would I still be better off looking at the Beagleboard, or even Beaglebone?

 

The Raspberry Pi looks like a fantastic peice of equipment for this kind of thing - and it's British - and I'd love to be able to use it for my project, so any help or advice would be greatly appreciated.

 

Doug Ponsford.

  • Sign in to reply
  • Cancel
Parents
  • mahjongg
    mahjongg over 14 years ago

    Well, I agree with Michael Kellett, the RPI as is is unsuitable for what you want at the moment, but maybe its not because it lacks the hardware to do what you want, but more because there is no support at the moment for what you want to do with that hardware; let me explain.

     

    The RPi does have hardware (interfaces) for Video Input and LCD output, but there is no software support for them (yet), and the interfaces are very modern, and therefore may not be easy to interface to the kind of devices you want to use. It has these interfaces because the Broadcom SoC (chip) that is used is actually a chip meant for smartphones and tablets and such, and therefore naturally has these interfaces, (for smartphones and such) the RPF decided to bring them out to a connector for possible future use.

     

    For video input the RPI has a 15-pins connector on board for a CSI camera, this interface is meant for the type of camera's typically found in smartphones. It connects to such a camera module with a paper thin flexible foil (with metal traces on them). This interface thus provides a video input option, but perhaps not in a form that is directly useful to you. The foundation has announced they are working on a camera module for this interface.

    Its to be noted that this DSI camera "speaks" directly to the GPU, which can only be controlled through a software interface, so its hard to say what useful things you can do with the captured video, the (ARM) CPU is probably too slow to encode the video signal into any kind of video format, but the GPU might be able to, IF such a thing is supported by it, using the available software interfaces.

     

    Regarding an LCD, obviously you can hang a PAL (NTSC) or HDMI LCD screen on it using the RCA and HDMI connectors, but the SoC also has a DSI output connector (also a 15 pins connector of the same type as the DSI connector), which can be used to drive raw LCD panels. But for this interface too, hardly any documentation exists at the moment, nor does a driver. DSI is very powerful and can not only transfer video data to the panel, it also can control the LCD panel and read out a touch interface.

     

    So maybe sometime in the future something like you want will be possible, but not at the moment, and not unless you are very knowledgeable about these interfaces, and the software that is needed to make them work, and only then if you can coax the GPU to do what you want, which may be impossible without support from Broadcom.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bartonwood
    bartonwood over 14 years ago in reply to mahjongg

    Hi Martin

     

    I certainly agree with much of what you have said. I am an optimist at heart and when I first came across the RPi I thought that we might just have a chance of making things a little bit more positive with respect to opening-up some quite clever electronics applications via open-source strategies.

     

    I’m a retired engineer with an interest in aerial, digital still and video photography using actively stabilised, RC, fixed wing platforms. I wish to use the RPi (when I get mine?) with Aptina MT9D111 2MP and MT9P031I12STMH ESMT9P031I12STMH ES 5MP SOC camera modules (among others) to store the captured images onto SD card. These modules where designed for and are used in mobile phones and similar systems hence my particular interest in the RPi and its Broadcom SoC processor. The question I should like to ask of anybody who has an informed opinion on the subject is: Is there any support for such devices at present or in the pipeline for using digital camera sensors, board modules, SOC’s etc. especially for full HD (1080p@30fps H-264) video and, say, 5MP or 8MP still images? If so, where, when and how, can we get details of such work? The software for these tasks has been written many times, for many devices: it only needs someone with a little generosity (it doesn't have to be the latest, all-singing, all-dancing version) to release it into the public domain for the use of all hobbyists, students, educators, tinkerers etc. Maybe we need to pressure RPF into negotiating with Broadcom to give more support for this AOI especially in terms of legacy drivers and their hardware.

     

    An ever hopeful tinkerer, 

     

    John Barton Wood

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mahjongg
    mahjongg over 14 years ago in reply to bartonwood

    John,

     

    searching the forum on the original raspberry PI site might provide some answers, as well as a place to ask question, or ask for features.

    the site (if you do not know) is here: http://www.raspberrypi.org/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to bartonwood

    @John,

     

    I'd be interested to hear how you get on.

     

    Doug.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    It sounds like an interesting project, Douglas, and even if you decide to use some other ARM board, your experiences could be quite useful to the Pi community.  Please keep us in the loop periodically. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    It sounds like an interesting project, Douglas, and even if you decide to use some other ARM board, your experiences could be quite useful to the Pi community.  Please keep us in the loop periodically. image