Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi server clusters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 96 replies
  • Subscribers 710 subscribers
  • Views 15788 views
  • Users 0 members are here
Related

Raspberry Pi server clusters

morgaine
morgaine over 14 years ago

One of my current intentions is to play with server clustering once the Raspberry Pi is in volume production and the 1-per-person restrictions are lifted.  I have a long-term background in parallelism and concurrency --- my doctoral research was in the topic, and I lectured on it later as well, so it's quite dear to my heart.  The very low price of the board makes this feasible with a monetary outlay far below anything else, so I'm really looking forward to an Rpi clustering project.

 

I'm sure that I'm not the only one thinking about Rpi+clustering. image  If anyone here has this kind of application in mind, or just general interest in the subject, please keep in touch and post any interesting links you may find on the topic.  Once there are millions of the boards around, this could be a very popular area. image

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    Hooray,  objective measurements are starting to appear as more people receive their Pi boards:

     

    • http://candgsoc.host56.com/2012/04/quality-time-with-a-raspberry-pi/

     

    It's very important to match what the board can offer against the specific requirements of your application, otherwise it can lead to disappointment.  Also, it's crucial not to make a one-dimensional analysis when multiple factors come into play, as cand's article highlights --->  the Pi's Ethernet performance can approach the full bandwidth of the line, but only at a huge CPU cost.

     

    First indications then suggest that networked applications of Pi are likely to be most successful when the network use is occasional and when not much else has to be executed concurrently with the communications.

     

    This will need a lot more careful analysis so that we know exactly where the bottlenecks are.  Some of them are quite likely to be remedied by kernel config improvements or with better drivers, but one has to know the detailed cause of a problem before one can tackle it.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    The following is about HPC which isn't my focus, but interesting nevertheless.  From Slashdot today:

     

    "Phoronix constructed a low-cost, low-power 12-core ARM cluster running Ubuntu 12.04 LTS and made out of six PandaBoard ES OMAP4460 dual-core ARMv7 Cortex A9 chips. Their results show the ARM hardware is able to outperform Intel Atom and AMD Fusion processors in performance-per-Watt, except it sharply loses out to the latest-generation Intel Ivy Bridge processors."

     

    More at:  http://linux.slashdot.org/story/12/06/16/1510257/12-core-arm-cluster-beats-intel-atom-amd-fusion

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 14 years ago in reply to morgaine

    Probably not quite what you're thinking of but the Design Spark forum (the competition) has an article on someone using Pis to make a VAX cluster.

     

    Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to bodgy

    OMG, DECnet!  http://www.designspark.com/content/raspberry-pi-vax-cluster

     

    Thanks for the headsup, Colin. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    There is an interesting article benchmarking a 12-core ARMv7 cluster

    against some PC's.

     

    http://www.phoronix.com/scan.php?page=article&item=phoronix_effimass_cluster&num=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Yeah, saw that.  It's very underwhelming though.  I'm a bit surprised that ARM (the company) isn't working harder in that area and dedicating more research to multicore clustering.  A reference board from them bearing say 16 dual-core Cortex-A9 MPcore chips would really fan the flames wonderfully.

     

    Intel can still warrant its total complacency about server-side ARM because a modern Atom core is nearly an order of magnitude faster than the best ARM core, so it doesn't have to push very strongly.  Well ARM can't do anything about the speed difference yet, but because it has the power advantage over Atom it really ought to use that to promote high core counts in clusters and start closing the gap with sheer core numbers.  It's not doing that, and I'm not too sure why not.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    There must be better ARM chips in the pipeline. At least Dell & HP are said to have arm based servers in the works and I can't see them being the only ones. Better performance per watt for arm only goes so far. I can see it being a tough sell if you need 10x the number of servers to meet some performance point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    There must be better ARM chips in the pipeline. At least Dell & HP are said to have arm based servers in the works and I can't see them being the only ones. Better performance per watt for arm only goes so far. I can see it being a tough sell if you need 10x the number of servers to meet some performance point.