Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi - Hardware Flaws and Fixups?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 188 replies
  • Subscribers 717 subscribers
  • Views 22762 views
  • Users 0 members are here
  • flaws
  • hardware
  • single_board_computer
  • single_board_computers
  • raspberry_pi
  • Design
  • fixups
Related

Raspberry Pi - Hardware Flaws and Fixups?

e14 Contributor
e14 Contributor over 14 years ago

Several people have commented on the hardware design of the Raspberry Pi.  Some are buried in other topics so please post your comments here.  I'll try my best to answer questions about the design decisions we made.  The Raspberry Pi is not perfect, never will be.  I've always found that perfect designs have a habit of never getting built, engineers are always a bit guilty of that, but I had Eben phoning/emailing me every day wanting to know when it would be finished.  Also, one persons perfection is another persons nightmare.

 

e14 is the home for engineers so please contribute to make Raspberry Pi better.

 

Thanks

 

Pete

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Not  a flaw, but I'd like to know if in future it'll be possible to power more demanding usb2 peripherics from the onboard hub, having the right power source; I'm referring to a RPF blog entry where protections on power input were discussed.

    My interest would be the possibility of plugging a 2,5 harddrive, and have it powered directly by the RPi, without the use of an hub; right now this is not possible, since the spinup currents would fry the tracks, 500mA max if I remeber it right, where a spinup is >1A.

    Is this feasible? Sure it's more for non-educational users, but it'll be a nice plus.

     

    Unrelated question: I read that the usb and the lan share bw, is that true? If it is, can you give some details about how that is managed? Like usb attainable speed, lan attainable speed, both combined...

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    piovrauze wrote:

    Unrelated question: I read that the usb and the lan share bw, is that true? If it is, can you give some details about how that is managed? Like usb attainable speed, lan attainable speed, both combined...

    Thanks.

    The SOC chip is meant to be used  inside a phone. So whereas modern CPUs have high speed busses to connect to peripherals either on the motherboard or on expansion cards, that simply isn't going to happen for a chip inside a phone or tablet.

     

    So the SOC has... USB. The model B has an USB-ethernet dongle integrated on the board. And because there is just one USB port on the chip, there needs to be an USB hub on the board as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The BCM has a single USB2.0 connection to the SMSC9512 (take a look) that provides the 2 USB + Ethernet.  So yes from a simplistic hardware viewpoint you have 480Mbits/s to share between all three.  The SMSC looks like a hub for three devices so dynamic sharing will go on.

     

    From the design point of view this was seen to be more than adequate for the educational target (an yes I will keep harping back to that - sorry) and was a nice (low cost and smallish) solution.  I may still moan a bit about power consumption but welcome to mixed signal.  In a general setup where you have a keyboard and mouse - clearly not a problem.  I've seen some people wanting to put Drives up on the USB.  So if you were say streaming off the internet or a usb cam and recording on the fly you might run into limits that will cause you problems rather than just being sluggish.

     

    Before anyone bails in - I have not considered software/driver overhead, bit 'wastage' through protocol and other good stuff.  In reality this will need measurement in real applications to come to a firm conclusion.

     

    I'll have a hunt and see if I can dig up some more data (but my bandwidth is very limited over the weekend) .. you could cross post onto raspberrypi.org and a software guy may be able to enlighten us as to what we should really expect, if it's actually been measured yet.

     

    Pete

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks both of you for making it clear for me.

    I don't plan to push the usb/eth to the limits, maybe not even half of it combined, so it shouldn't be an issue.

     

    What about the power related question (more amperage on the usb port)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    PeteL,

     

       Thanks for the responses and educated answers.  I'm actually really liking this thread since we are discussing something other than ship dates.

     

        I agree with your statement on the intent for the RPi, I don't remember a home streaming media server being on the list.  ;)

     

        I do see though many users finding the limitations through experimentation.  The first 10k recipients hopefully will be filling these forums with data and stories so the rest can modify or tweak their plans.  I would also hope that we could affect future versions by providing documented "deficiencies".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Kevin - I agree, people will find limitations and probably some issues that will need a workaround.  I'm keen to get input on what people have found and what should or should not be included in future versions / revisions.

     

    I keep saying that the roadmap of activities do not extend beyond the educational release, but we all know it's fun to consider what would be possible in the future.image 

     

    Innovation - 1 part enabling technology, 1 part funding, 100 parts dreaming what if !  If we can get the kids thinking then I'll be a happy man rather that a grumpy 'ol engineer!

     

    Pete

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Generally, the best throughput you can get out of USB 2.0 Hi-speed is about 2/3 of the signalling rate, or about 320Mb/s, half-duplex. In HDD terms, that's about 40MB/s.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Perfect, I estimated the same numbers, so now they shuld be right.

    This is more than enough BW for my needs, and I just need the HW to test it live now... XD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

    The BCM2835 SoC wasn't developed for use inside a phone, at least not as a primary target.  Not many phones have an HDMI socket. image

     

    You could say that when I said "phone" I meant "a low power hand-held device". However:

     

    This is the sort of phone I was thinking about: http://www.phonearena.com/news/Samsung-Galaxy-S-II-supports-HDMI-out-after-all-and-can-have-live-TV-streamed-to-it_id17004

     

     

    The reason the BCM2835 is affordable is that they are powering smartphones. That makes the market large -> large volume and competitive market.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Pete, are you planing to post some schematics ?

    That would be nice for your educational objecitve.

    Is it against commercial agrement with your distributors ?


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    Roger Wolff wrote:

     

    Morgaine Dinova wrote:

    The BCM2835 SoC wasn't developed for use inside a phone, at least not as a primary target.  Not many phones have an HDMI socket. image

     

    You could say that when I said "phone" I meant "a low power hand-held device". However:

     

    This is the sort of phone I was thinking about: http://www.phonearena.com/news/Samsung-Galaxy-S-II-supports-HDMI-out-after-all-and-can-have-live-TV-streamed-to-it_id17004

     

     

    The reason the BCM2835 is affordable is that they are powering smartphones. That makes the market large -> large volume and competitive market.

    I'm glad you replied to that, since I was about to reply that my own phone, the HTC Evo ("4G") uses an HDMI out port, as do many other mobile phones today.  Don't even get me started on HDMI out via USB dongle.  Or Component vs HDMI vs SDI

     

    I believe most phones use a Cortex processor rather than an ARMv11 these days...

     

    But at any rate the low power requirement itself is your biggest clue to it's potential applications:  With today's huge wireless data use and monolithic screen sizes the GPU is rarely any phone's biggest energy hog.  From my experience with Roku boxes (which I find unwatchable) the Broadcom 2835 is an affordable and reliable chip as long as you aren't trying to push 720p through a 450kbps mp4 stream.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Note that this "hdmi through USB" is probably not proper use of the USB connector. They need have the USB connector anyway so they multiplex the HDMI signals onto that connector when you connect that special cable. USB isn't fast enough to handle most screens. (Full-HD is about 3Gbit/sec, just a tad over 480Mbps... )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Note that this "hdmi through USB" is probably not proper use of the USB connector. They need have the USB connector anyway so they multiplex the HDMI signals onto that connector when you connect that special cable. USB isn't fast enough to handle most screens. (Full-HD is about 3Gbit/sec, just a tad over 480Mbps... )