Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi - Hardware Flaws and Fixups?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 188 replies
  • Subscribers 717 subscribers
  • Views 22893 views
  • Users 0 members are here
  • flaws
  • hardware
  • single_board_computer
  • single_board_computers
  • raspberry_pi
  • Design
  • fixups
Related

Raspberry Pi - Hardware Flaws and Fixups?

e14 Contributor
e14 Contributor over 14 years ago

Several people have commented on the hardware design of the Raspberry Pi.  Some are buried in other topics so please post your comments here.  I'll try my best to answer questions about the design decisions we made.  The Raspberry Pi is not perfect, never will be.  I've always found that perfect designs have a habit of never getting built, engineers are always a bit guilty of that, but I had Eben phoning/emailing me every day wanting to know when it would be finished.  Also, one persons perfection is another persons nightmare.

 

e14 is the home for engineers so please contribute to make Raspberry Pi better.

 

Thanks

 

Pete

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 14 years ago

    Reviewing the rev 1.0 schematics and docs for the related parts, I found something that looks wrong.

     

    The SMSC LAN9512 has two VDD18CORE pins that are internally connected between them and to the internal core 1.8V voltage regulator, those pins need to be connected externally as well and to a couple of filter caps.

     

    The RasPi schematics shows those pins also connected to the +1V8 power line from RG1.

     

    That looks wrong, the SMSC VDD18CORE pins should not be connected to +1V8.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to jamodio

    I fully agree! with your "VDD18CORE" remark.

     

    Jamodio, have you found a "reset" pin on the 2835? The only thing I could find was "run". Would the CPU just pause when pulled low? I don't know.

     

    While investigating this, I found that "D10" is not marked "(B)" as it should. (even though it is involved with the USB powersupply for the model A, the other side is not connected on the model A, so the component is redundant on model A).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to rew

    Unfortunatelly there is not much doc available for the BCM2835.

     

    The electrical characteristics on the LAN9512 DS do not make any mention about those pins, then I'd infer that the only reason for their

    existance is for the external caps for the internal regulator like many other devices. So those pins are not intended to be an input from

    an external 1.8V source nor an output to become a 1.8V source.

     

    Besides injecting noise on the core voltage, it really depends in which direction current is flowing at any given time, so extra current

    draw from the internal regulator or additional current flowing through those pins will probably increase the chip temperature, and

    since those pins are not intended to be connected to anything active, the silicon probably has not much protection, so potentially

    you could damage the chip.

     

    I don't know what consequences it may have on the BCM chip.

     

    In summary, I don't believe it is something that will make the board blow up but MUST be corrected on future revisions, the way it is

    right now it is simple wrong.

     

    I'll see what happens if I pull down RUN.

     

    Right now I'm testing the Arch Linux distro, Debian seems to have another issue on the kernel related probably to the USB/ethernet

    driver.

     

    My .02

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to jamodio

    It's not connected to the BCM2835 1.8V regulator output: The BCM2835 doesn't have a 1.8V regulator.

     

    The 1.8V comes from the RG1 regulator. (Ah! This means we'd be able to run 1.2V SDRAM!), but as things are right now, it'd be a funny experiment to remove the NCP1117 altogether and see what happens. :-)

    When the 9512 has some "headroom" and/or the SDRAM interface doesn't use too much power on the 1.8V line, this would save a few components for the foundation/farnell/RS.

     

    I though that the 1.8V regulator was the smallest of the three, so that the "design power" of the regulator was probably the lowest. Not true: RG1 is the middle one. So Pete problably thought a noticable current would flow there....

     

    (The FT232BM had a 3.3V regulator on board, which could deliver 10mA of extra current. Useful, but quickly inadequate. The FT232RL has a 3.3V regulator with 50mA to spare! That's quite useful. You can easily power an AVR and a few leds from that!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to rew

    Yes afaik there is no internal regulators on the BCM2835.

     

    The LAN9512 pins are connected to the main 1.8V fed by RG1 wich feeds the BCM2835 1.8V, several clocks and PLL circuits, the USB module, etc.

    Those pins are not intended to be an OUTPUT just a connection point for the required filter caps.

     

    I've no clue what is the total current draw by the BMC2835 through those pins.

     

    I don't think it would be a good practice, even to try, sourcing the 1.8V from the LAN9512 pins. And for model A you will sill need the 1.8V regulator.

     

    The NCP1117 can provide up to 1A (obviously not in this application), it shows about 95F so there is some current flowing there.

     

    I guess Pete has the advantage of seeing all the BCM2835 documentation that is not available publically.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to jamodio

    jamodio wrote:

     

    Yes afaik there is no internal regulators on the BCM2835.

    not true... There is a switching regulator IN the BCM2835 that generates the 1.2V core power its own use!

     

    C16 and C17 next to the SOC are involved (input/output capacitor) and directly opposite on the bottom side of the PCB, L5.

     

    Suggestion for the future....

     

    You know those pins that power the SD interface voltage? The one that was left floating in the alpha batch in january? That should become jumperable to 1.2V or 1.8V. That opens up a few new RAM chips.

     

    In fact I think I have a 'pi that has a 1.2V RAM chip installed where this voltage is SUPPOSED to be 1.2V. Not 1.8V.... (On the other hand, the RAM chip that I have also needs 1.8V, and I don't know which is which..... In january I thought the missing connection was the one for the IO buffers on the chip, which I THINK are supposed to be 1.2V for my samsung K4P2G324ED. And from the schematics I cannot see what voltage would be present on SDRAM_VDD.) (*)

     

    Oh, in the box "PWR1" at the top of page 1 of the schematics, you see several "voltage regulator outputs" on the BCM2835.... :-)

     

    (*) On the other hand, the pins marked 1.8V are probably really 1.8V, and really power the SDRAM chips themselves. while the SDRAM_VDD might be the one that is the IO voltage for the SDRAM and be the 1.2V that the Samsung page mentions as the VDDQ, the IO voltage for the SDRAM chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to rew

    You are absolutely right, didn't look in detail at those pins !!

     

    I t would be nice if Broadcom at least releases the pinout documentation with a brief explanation of what each pin does.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to jamodio

    So no follow ups, additional comments about this issue ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to jamodio

    What issue are you referring to? The pinout datasheet? You say "it would be  nice... ", and I agree. But it is not going to happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to rew

    Perhaps ask them nicely for informally documented pinout information?

     

    At worst they'll either refuse or just ignore the request, but you never know.  We might be hugely and pleasantly surprised.  It's summer after all, and Broadcom might have some interns kicking around the lab looking for something simple to do. image

     

    In addition, there's another possible outcome lying somewhere  between the best and worst cases, which is that certain Broadcom employees who regularly post on the RPF forum will probably come out with elaborate rationales about why pinout information must be protected at all costs otherwise it will reveal the deepest secrets of the company to the competition.  That would be worth its weight in gold for sheer comedy, so please ask. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Maybe someone should ask Where's Pete?

    Last we heard, back in April he was going to release v1.1

    of the schematics "soon".    After seeing 100% of the

    foundation's paid staff (Myra) disappear without any

    announcement, I get nervous when key people like Pete,

    who was quite active on this forum, go off to fixup the schematic

    and don't return.  I think the Model A was also his baby,

    and has disappeared from radar.  And as we know, Seneca was

    going to fix the login and timezone problems in Fedora 14 back in

    March, and from what I can tell, Chris Tyler is off writing a book,

    and his student helpers haven't been heard from lately. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to rew

    I was actually referring to the LAN9512 VDDCORE pin connected to the +1V8 line.

     

    There is also somewhere else a question posted about thermal issues and the warning sheet shipped with the Rpis that says "should not be covered."

     

    I'm also trying to dig into a kernel panic issue when the network interface is under stress using the Debian distro, I'll be posting a msg on the forum.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 14 years ago in reply to rew

    I was actually referring to the LAN9512 VDDCORE pin connected to the +1V8 line.

     

    There is also somewhere else a question posted about thermal issues and the warning sheet shipped with the Rpis that says "should not be covered."

     

    I'm also trying to dig into a kernel panic issue when the network interface is under stress using the Debian distro, I'll be posting a msg on the forum.

     

    -J