Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi - Hardware Flaws and Fixups?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 188 replies
  • Subscribers 717 subscribers
  • Views 22744 views
  • Users 0 members are here
  • flaws
  • hardware
  • single_board_computer
  • single_board_computers
  • raspberry_pi
  • Design
  • fixups
Related

Raspberry Pi - Hardware Flaws and Fixups?

e14 Contributor
e14 Contributor over 14 years ago

Several people have commented on the hardware design of the Raspberry Pi.  Some are buried in other topics so please post your comments here.  I'll try my best to answer questions about the design decisions we made.  The Raspberry Pi is not perfect, never will be.  I've always found that perfect designs have a habit of never getting built, engineers are always a bit guilty of that, but I had Eben phoning/emailing me every day wanting to know when it would be finished.  Also, one persons perfection is another persons nightmare.

 

e14 is the home for engineers so please contribute to make Raspberry Pi better.

 

Thanks

 

Pete

  • Sign in to reply
  • Cancel
Parents
  • Montala
    Montala over 14 years ago

    I know it has probably been mentioned before, but would it be that difficult (or expensive) to increase the on board memory, which apparently is shared with the GPU anyway, up to 512 Mb.?

    This would enable certain Linux distros to run more 'smoothly' and should increase performance generally... shouldn't it?

    I am by no means a hardware 'expert', so if this a silly rerquest. then I will apologise now! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Montala
    Montala over 14 years ago

    I know it has probably been mentioned before, but would it be that difficult (or expensive) to increase the on board memory, which apparently is shared with the GPU anyway, up to 512 Mb.?

    This would enable certain Linux distros to run more 'smoothly' and should increase performance generally... shouldn't it?

    I am by no means a hardware 'expert', so if this a silly rerquest. then I will apologise now! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Montala

    It's a very reasonable question. The answer that's been given before was that the price of the 512M memory modules is much higher and it couldn't be done for the required price.  My guess is that if memory prices fall a future version could have more memory. I think the limit is1G because of the number of pins available.

     

    All this is unofficial but based on what's been said before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Chris/David

     

    I have said before that it was not in our roadmap - but I hesitate things can always be changed  - I don't want to be in the situation where I say there is no interest or call for something when it is clearly not true.  So a measurement is in order.  I'll kick off a poll soon.

     

    Our original (and still current) aim was to make the cheapest functional device to do the target educational job.  Given the tremendous support we have been given from so many different quarters we will re-evaluate it.  Price is an issue but interestingly bringing the model A up to 256Mb worked to increased volume of a single device and the price impact was minimal on A and positive on B.

     

    Being absolutely honest my (not the foundation) concern is that providing a 512Mb device will mean that application developers will be tempted (not unreasonably) to use it and then not be able to support the 256Mb educational device - we are almost setting ourselves up for potential incompatibility issues. It's a concern not a fact - I'm and engineer and perhaps I'm plain wrong - comments?

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    My opinion is that the Pi board created this magnificent niche purely as a result of its low price, so you're totally right to focus on cost in my estimation.  After all, there is no shortage of higher-priced boards, but they never created this degree of interest.  $25 is a sort of magic threshold.  (The $35 model B is actually riding the wave created by the model A's magic price.)

     

    Personally I'd not worry about RAM size incompatibility, for four reasons:

     

    • Educational use rarely requires large amounts of memory, and education is after all the primary target.
    • The Unix model works well with very little memory, and encourages the use of multiple small processes.
    • Darwin will ensure that large monolithic programs that don't run in 256MB are discouraged. :-)
    • Technical progress will inevitably mean that memory size will increase, so size variation is inescapable.

     

    In summary, I suggest to always provide as much memory as current technology allows whenever a new iteration of the board is being designed, but always respecting the existing cost constraint.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 14 years ago in reply to e14 Contributor

    Thanks for your interesting reply Pete.

     

    As it is so easy to do, what with all the 'hype' surrounding this device, I had forgotten for a moment its primary purpose which is, as you say, as an 'educational device'.

     

    So far as the 'home user', 'enthusiast' or 'geek' (call them what you will) is concerned... and I include myself in one of those categories, I am sure they would welcome the involvement of more application developers, and hopefully the appearance of some more dedicated OS's also.

     

    The idea of a cheap, but functional, 'mini Linux box' is very appealing, (especially when enclosed in a smart case!) although obviously ARM support is essential here, and of course the Foundation have their own pre-determined path to follow.

     

    It would however be a very attractive option I feel, and one which would probably increase sales also... although perhaps not all in the intended market.

     

    Definite food for thought... and for much further discussion I expect!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Montala

    I know about the textbook Turing Machine example, but this remarkable project:

    http://dmitry.co/index.php?p=./04.Thoughts/07.%20Linux%20on%208bit  really makes the point that it is only the memory size that limits what a computer can do. The CPU just limits how *fast* it can be done.

     

    That said, for me the most distinguishing feature of the RasPi is the price. If you really need more performance, at some point you're really better off with just using a bigger system, for somewhat more $$ of course.  But, not sure where that point is exactly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Pete,

      I think your concern about application developers taking advantage of 512MB and leaving

    users of the 256MB device in the cold, is misplaced.  Most applications aren't being written

    from scratch for the RPi, they are being rehosted from other linux systems.  So the application

    is going to be identical regardless of the memory available. 

     

    For most applications, the application's code will fit fine in 256MB.  It's the data that matters.

    For example, a web browser's code will fit in 256MB, but if you are browsing large pages, or if you

    have multiple tabs open, you will run out of memory.

     

    Both Debian and Fedora have stated recommendations/requirements for substantially more than 256MB, so the 256MB RPi is not compliant.  It's not much different than trying to reduce costs by using a smaller cpu heat sink than the cpu manufacturer recommends/requires.   You wouldn't want to do that because inevitably it will lead to increased support costs and user frustration.