Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi - Hardware Flaws and Fixups?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 188 replies
  • Subscribers 717 subscribers
  • Views 22729 views
  • Users 0 members are here
  • flaws
  • hardware
  • single_board_computer
  • single_board_computers
  • raspberry_pi
  • Design
  • fixups
Related

Raspberry Pi - Hardware Flaws and Fixups?

e14 Contributor
e14 Contributor over 14 years ago

Several people have commented on the hardware design of the Raspberry Pi.  Some are buried in other topics so please post your comments here.  I'll try my best to answer questions about the design decisions we made.  The Raspberry Pi is not perfect, never will be.  I've always found that perfect designs have a habit of never getting built, engineers are always a bit guilty of that, but I had Eben phoning/emailing me every day wanting to know when it would be finished.  Also, one persons perfection is another persons nightmare.

 

e14 is the home for engineers so please contribute to make Raspberry Pi better.

 

Thanks

 

Pete

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Not  a flaw, but I'd like to know if in future it'll be possible to power more demanding usb2 peripherics from the onboard hub, having the right power source; I'm referring to a RPF blog entry where protections on power input were discussed.

    My interest would be the possibility of plugging a 2,5 harddrive, and have it powered directly by the RPi, without the use of an hub; right now this is not possible, since the spinup currents would fry the tracks, 500mA max if I remeber it right, where a spinup is >1A.

    Is this feasible? Sure it's more for non-educational users, but it'll be a nice plus.

     

    Unrelated question: I read that the usb and the lan share bw, is that true? If it is, can you give some details about how that is managed? Like usb attainable speed, lan attainable speed, both combined...

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    piovrauze wrote:

     

    Not  a flaw, but I'd like to know if in future it'll be possible to power more demanding usb2 peripherics from the onboard hub, having the right power source; I'm referring to a RPF blog entry where protections on power input were discussed.

    My interest would be the possibility of plugging a 2,5 harddrive, and have it powered directly by the RPi, without the use of an hub; right now this is not possible, since the spinup currents would fry the tracks, 500mA max if I remeber it right, where a spinup is >1A.

    Is this feasible? Sure it's more for non-educational users, but it'll be a nice plus.

     

    I know you mention not using a hub, but consider this: A tiny 4-port USB hub with a 2A power supply (the norm) could power both the hard drive and the RPi (with a USB type-A to micro-B cable).  As long as the overcurrent monitor on the hub is ganged (most are, since it's cheaper), there would only be a problem with overcurrent if the total draw is more than 2A. And you'd have two extra USB ports to boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I understand the point, and I'll have to use a hub, still I find it more attractive to use less HW.

    Would it be possible to add the 5V power source directly on the onboard usb port, in parallel wit the board supply? (using the same power source)

    If I use only one of the 2 usb ports, I could do it without soldering.

    Is this feasible? what happens to the rest of the RPi, does this bypass the board overcurrent protection?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    PeteL has said that you can bridge the fuses. You'll be stuck with "just" the 700mA entry-fuse on the microUSB port. And as long as the total doesn't exceed that, you'll be fine.


    I won't be doing this mod before Farnell has RPI's in stock for "next day delivery".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    That's for sure! I won't be doing HW endangering stuff till there is a costant supply of RPi ready.

    This one will be kept clean of mods, and I'll use it for testing the sw and limits of the HW.

     

    @PeteL: I remember Arch distro "overclocks" the SoC to 800MHz, how does this affect power consumption, temperature and emissions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    There is a report of an expensive TV being zapped when connected

    to the RPi hdmi port.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=6&t=5632

     

    perhaps prudent to use only inexpensive monitors until more is known

    about this issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    You know, I'm beginning to have my doubts about the whole power philosophy in the Pi's design.  Not for the next minor board update(s), but for the next major board design, I think the entire question of power should be reopened from scratch.

     

    The concept of using cellphone chargers for power sounded like genius originally, but in practice it has turned out to have a very ugly underbelly.  These chargers are made for charging, not for delivering constant power to downstream USB peripherals, and they're made to such a rock-bottom price that a very high proportion of them has pretty dreadful electrical performance.  This has been a source of many problems for Pi users already, who commonly go through several chargers before finding a good one.

     

    It's no surprise really, with the benefit of 20/20 hindsight. image  Chargers bundled with cellphones are only expected to work with one specific load, their cellphone.

     

    The polyfuse issue has exacerbated this.  It's bad enough using a wonky charger as a power supply, but when you then kill off voltage regulation almost completely by putting such high-resistance polyfuses in the supply line then you're just asking for trouble.  For all intents and purposes, the Pi is supplying an unregulated USB supply.

     

    It's not quite a disaster just yet, but I'm pretty sure that it's possible to do far better than this and still remain within the price niche, particularly now that BOM costs have dropped hugely as a result of volume manufacturing.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    I've only had a little experience with polyfuses.  That was a product where part of the manufacturing process included tweaking the 5V power supplies to compensate for the voltage drop across the polyfuses.  Not a very nice way to manufacture products.  My suggestion (which was adopted) was to replace the polyfuses with automotive mini-fuses, which have very low resistance and are easily replaced.  Sure, self-resetting fuses sound wonderful and convenient, but we're seeing lots of problems with them in practice given the variability of power supply voltages, micro USB cables, and polyfuse characteristics.

     

    I agree with Morgaine that the increased volume suggests that choices made to save pence should be revisited.  Personally, I like the idea of a built-in switching power supply with 3.5 mm jack and a bridge rectifier on the input so that you can hook up any 6V to 12V wall wart without worrying about polarity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    I agree 100%.

     

    While I accepted it, I've got never convinced that using a charger and the USB connector for input power were the best approach.

     

    I asked Pete more than once if they ever considered using a power management IC instead LDOs, Eben at some time talked about it, but never got/saw a response.

     

    There are plenty of low cost/acceptable quality power supplies out there, and by the volumes/interest we are seeing with the Pi I'm sure the distributors can get a

    very good price and bundle as an optional a power supply.

     

    Get rid of the fuses, there are input voltage protection chips like the NCP349 used on the Beaglebone and USB power switches with protection can be used

    in replacement of the fuses.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    I agree 100%.

     

    While I accepted it, I've got never convinced that using a charger and the USB connector for input power were the best approach.

     

    I asked Pete more than once if they ever considered using a power management IC instead LDOs, Eben at some time talked about it, but never got/saw a response.

     

    There are plenty of low cost/acceptable quality power supplies out there, and by the volumes/interest we are seeing with the Pi I'm sure the distributors can get a

    very good price and bundle as an optional a power supply.

     

    Get rid of the fuses, there are input voltage protection chips like the NCP349 used on the Beaglebone and USB power switches with protection can be used

    in replacement of the fuses.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    Replacing polyfuses F1 and F2 by wires leading back to the power input point VIN is quite likely to become Raspberry Pi Hardware Hack #1. image

     

    Morgaine.