Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 710 subscribers
  • Views 27664 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 14 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    That's a terrific system you're building there, with M4 master, M0 supervisor, FPGA, and <= 6 M4 slaves! image

     

    I'm intending to play with ARM clusters as well, not just Rpi but also STM32F4 of which I have several.  FPGAs (or at least CPLDs) are quite likely to appear in there somewhere too, as coprocessors or implementing a communications matrix.

     

    It's also one of my strong interests (separate from clusters) to make gate-level programming more approachable by directly attaching either an FPGA or CPLD to Rpi, turning the ARM into a high-level networked peripheral for logic-based design, perhaps a bit like Xilinx's Zynq-7000 in some respects.

     

    As you pointed out, there are no networked debug tools for FPGA work (at least not in my price bracket) ... but we can make the next best thing ourselves with the help of an ARM board, and Rpi is a nice one if you can work within its I/O constraints.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to morgaine

    Hello Morgaine,

     

    I have great hopes for the Zynq - are you going to the Xilinx Xfest in May where there are a whole load of lectures about it ?

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to fustini

    The major FPGA manufacturers all offer very good tools for free and even better ones for money. All the tools are memory and disk hogs (1Gb free memory min but often need much more) and as soon as you do much they need a really fast computer. The RPi just isn't up to it.

    I don't know of any open source small footprint solution to do the whole job (design capture, simulation, synthesis, programming).

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to michaelkellett

    Ah ok, I was fearing that.  My memories of Quartus were that it brought the PCs in our lab to a crawl during synthesis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to fustini

    Besides requiring lots of RAM there is also the fact that these programs are compiled for intel CPUs and not for ARM.

     

    Even though the RPI cannot run the synthesis software, the RPI can function as a good intermediary to the hardware. I'm not writing off the RPI for this application just yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustini

    Good video, thanks Drew.

     

    As Michael says, the FPGA manufacturers provide powerful tools, but they're all closed source package deals and they try to create a captive audience for their products, which is the opposite of where we want to be.  As we try to extend the reach of open source software down into the hardware, it would be incongruous if we then had to use closed source software tools to develop the open hardware.  That's clearly not the way to go.

     

    As Drew's video mentioned, open source tools like Icarus Verilog, Verilator and Gtkwave provide a start towards getting us back into software control there, at least at the front end.  Until the day that we get a open FPGA fabbed, we'll probably have to keep relying on closed back-end synthesis tools from the closed manufacturers, but we should at least try to limit them to the back end, as OpenCores is doing.

     

    Of course a fabbed OpenRISC would be fully open hardware from a programmer's perspective, but if you need closed source tools in its creation and simulation then you don't have a completely open toolchain.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to morgaine

    I had  a quick re-scan of open source VHDL tools and they are so limited at the moment - I don't think there is anything like the critical mass to make a "GCC" for FPGA.

    as for open FPGA .... only if someone like Intel (with silicon fab and deep pockets and currently showing strange interest in FPGA startups) decides they want to take a swipe at Xilinx and Altera.

     

    On a more promising note, and possibly should be in a new thread, interestng article about I2C isolation, just need to find where to buy them !

     

    http://www.edn.com/article/521380-Optically_isolating_an_I2C_interface_Beware_of_nonlinear_propagation_delays.php?cid=Newsletter+-+EDN+on+Consumer+Electronics

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to michaelkellett

    Pity that we can't split off the posts where we started talking about ARM and FPGAs into a separate thread.  They clearly have nothing to do with the original poster's topic, lol.  But if we start a new thread now it'll lack the posts above, and will probably dry up immediately by Sod's Law. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    Pity #2 that both cost and real-estate constraints are unlikely to allow optoisolation and/or buffering of signals on the GPIO connector even in future redesigns.  So many poor little Raspberry Pi's are going to die in the name of education and experimentation.  I guess it's a worthy cause at least, they will be remembered. image

     

    PS. The article you linked is a real eye-opener, Michael.  The real world is so hugely different to the cosy theoretical model of a simple bus with pullups.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    Hi Morgaine - good point that this discussion merits a separate thread.  I can branch as admin, but what do you think would be the best point to do so?  Maybe http://www.element14.com/community/message/48868#48735?

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustiniadmin

    Oh, excellent Drew if you can do that, thanks!   We went seriously off the OP's topic  by several miles, lol, but hopefully it was still useful material for Rpi-related development and education.

     

    I think it was Michael's very interesting description of his cluster incorporating an FPGA --- http://www.element14.com/community/message/48733#48733 --- which greatly sparked my interest and the subsequent detour.  Perhaps that would be a good branching point?

     

    Morg.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    Thanks, let me know if the subject should be tweaked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    Thanks, let me know if the subject should be tweaked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 14 years ago in reply to fustiniadmin

    OK by me.....

     

    So an RPi FPGA board:

    First thoughts, must be cheap, must be hand solderable (no BGA), must use bits that can be bought retail.

     

    For £15 one at a time from Farnell you could have a Lattice  XP2  or a Xilinx Spartan 6 in 144 pin TQFP (there will be something Altera that is similar).

    The XP2 has on chip flash so you get instant boot up - the Xilinx part needs a separate boot flash rom.

    At this level you get about 5k LUTs, some on chip multipliers and a chunk of block RAM. The Spartan is more capable in raw performance.

    Of course you could go a bit cheaper and use a CPLD type part but then you don't get enough logic to be really exciting.

     

    I prefer the on chip flash (keeps it all simple) and sInce I use Lattice parts all the time the XP2 gets my vote !

     

    There needs to be  a way of using the standard FPGA tools (ie connector for JTAG) and a way of re-flashing the FPGA from the RPi.

     

    It'll need 3.3V and 1.2V regulators and some buffering bits and pieces so you would be looking at a solder it yourself cost of about £25.

     

    More thoughts any one ?

     

    Michael Kellett