Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 713 subscribers
  • Views 26470 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 14 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    There's a nice new write-up of Valent F(X) FPGA boards for RasPi and BeagleBone at Linux Gizmos: BeagleBone and Raspberry Pi gain FPGA add-ons.  Boards not yet available commercially, but they're considering a Kickstarter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Very interesting.  I had a good chuckle at "LOGI-BONE SLIM" and "LOGI-BONE PHAT". :-)

     

    Care to hazard a guess at pricing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Bugblat cost is also hidden by a $22 charge for shipping, so the real cost is close to $60 while you can get the breakout board with the largest XO2 chip for $26 directly from Lattice.

     

    I have been using the Lattice family since the GAL families in the 80's.

    I like the fact that they are instant on, and do not need to relaod the firmware at each power on like Xilinx and Altera. But they are limited in size, about 6500 LUTs.

    Teir larger FPGA family is the ECP3, but they all are large ball count BGA, so not for the average DIY dude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • guzunty
    guzunty over 12 years ago in reply to morgaine

    > The two devices aren't even remotely the same in capability nor price.

     

    Totally agree. However, the Guzunty is my baby and I am very sensitive to devices that might be perceived by some to be better. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Speaking of "cuddly CPLDs", I guess Morgaine never saw (or has forgotten) the old MMI PAL data books, which were filled with cartoon drawings of friendly, smiling "PALs" in standing-up DIP packages.

    I have in front of me Monolithic Memories' Programmable Logic Handbook of 1985 featuring a cuddly and smiling PAL sitting on a die on page 1-5, and on page 1-6 waving a rod at a very non-smiling PROM teaching it new tricks. imageimageimage

     

    Some things just can't be thrown away. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    Jean-Paul Louis wrote:

     

    I have been using the Lattice family since the GAL families in the 80's.

    I have Lattice's GAL Data Book from 1989 on the shelf here too, but it has no cuddly smiling chips. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Jean-Paul Louis wrote:

     

    I have been using the Lattice family since the GAL families in the 80's.

    I have Lattice's GAL Data Book from 1989 on the shelf here too, but it has no cuddly smiling chips. image

    The only advantage to companies' not giving away or selling data books any more is that you never have to throw away old data books to make room for new ones. image

     

    Pack rat?  Moi?

     

    Edit: Woo hoo!  This is my post number 1000 (decimal)!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Well I did throw away most of my PDP and VAX handbooks.  I hope Drew isn't listening. image

     

    Addendum:

    John Beetem wrote:

     

    Edit: Woo hoo!  This is my post number 1000 (decimal)!

    Congratulations! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Packrat? moi? naw. I just can't part with my 1975 RCA COSMOS Digital catalog.

    Who remembers Silicon on Saphire?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    an open source tool chain for FPGA design is frankly a ridiculous idea, all FPGA vendors release and support their own proprietry design software and trying to integrate all the features that they support into a single tool is, well the first question I would ask is why the hell would you even want to think about attempting it?

    The whole idea is typical of the open source software community as a whole, nerds with nothing better to do than bleat about linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    @FF

     

    The economics may be different but in principle the idea of FOSS support for FPGA design is not that different from the GCC concept. At the higher levels of abstraction the tools are (in both cases) hardware agnostic. Actual fitting and routing into an FPGA is very hardware specific (although I'm not sure that FPGA architectures are any more diverse than processors'). The usual way this is dealt with is by a vendor supported software component but completely independent designs are possible.

     

    The question as to why is perhaps less obvious - quite good FPGA tools are available free or very cheap but when you need serious tools it starts to cost a bit more.

    The VHDL/Verilog simulator that I use on a day to day basis costs more than £10k - you can get the same thing for free in a crippled  version (artificially slowed down). If there were an open source version it would run at full speed for everyone so that would fit nicely with the silicon vendors free router/fitter.

     

    The open source community has every right to crow/bleat/be-proud-of Linux - it is hugely successful and has done a lot to stimulate the efforts of others to make better stuff at better prices.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    If you have so little to do in your day job that you think rewritting huge amounts of code to no good effect is a good use of your time then maybe you should come and work for me and we'll get you doing real world designs which we have to sell to real customers using the code supplied by the likes of Xilinx and Altera.In my company we spend our time making money by selling designs which people use, rather than dicking about with open source crap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    If you have so little to do in your day job that you think rewritting huge amounts of code to no good effect is a good use of your time then maybe you should come and work for me and we'll get you doing real world designs which we have to sell to real customers using the code supplied by the likes of Xilinx and Altera.In my company we spend our time making money by selling designs which people use, rather than dicking about with open source crap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    I'll ignore the somewhat offensive tone and address the substance of your comment.

     

    At no time did I suggest that I would be investing my time in writing FOSS code for FPGA development. The most likely source for such funding would be one of the smaller silicon vendors and the reason that they might do it is that rather than pay Mentor\Aldec etc for the subsidised use of their tools they could fund FOSS and leverage the open source effort that this might attract.

     

    Your perspective of FPGA design is obviously limited by your Altera/Xilinx focus, I already sell designs which people use and I don't use Altera or Xilinx parts. As I explained before I use a paid-for simulation tool.

     

    I'll leave it to others to correct your rather weird generalised open source antipathy - I don't happen to use Linux but I do use some open source tools - and I find the range of quality to be not much different than paid-for but the cost is lower.

     

     

    MK