Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 682 subscribers
  • Views 21563 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 13 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • pjclarke
    pjclarke over 13 years ago

    Hi all,

     

    Thanks for pointing me at this Morgaine.

     

    I think there are a few point to consider here I want to throw in. However I want to be clear that I'm very pro getting schools, collages and Uni's more hands on and involved with things like Raspi and FPGA/CPLDs.

     

    First off from a education point of view we have to consider what you guys are talking about and the target audiance. As someone who has teached kids in electroincs clubs and takes part in school engineering contests (as a judge) I had written this blog on my first views of the Raspi in educations. This was followed up by a head of ICT who poested this on Deaign Spark too.

     

    My point is however that education is just not geared up for the Raspi and certanlly not for FPGAs. I ahve spoken to a teacher only yeasterday about this and she confirmed that they have no idea what they are doing. So throwing FPGAs at them will scary them off. The key point she picked up from my blog above is that unless a package is supplied to schools that is clear and simple to use then it will not get past the teachers desk. This sounds harsh, but its so true. Its take two years for the Arduino to apear in school contests.

     

    Moving on to haveing a CPLD or FPGA attached to a Raspi I think is a good idea. The Raspi is limit in GPIO and anything that can help expand this will be good. As a first off I would use somthing like a simple CPLD as a direct access to the GPIO as this will hold its configuration at power up, allow simple patcheing and basic logic circuits to be run from it.

     

    The XAPP058 is a great starting point for someone to generate a JTAP programmer for the Raspi. This can then use XSVF files to program either the CPLD or another FPGA if attached.

     

    At this basic level I think you could then start offering not only programming but some simple VHDL / Verilog to schools and collages. However as pointed out you can't run the tools on the Raspi so will HAVE to have another machine for this. You then have to ask if this is protical. What is the Raspi really doing in this project that you can't do with a PC or some of the specially designed education kits like ther terasic DE2. Find that answer and argue it and then you can push Raspi and FPGA tech togetter into schools. However in my view, use pre complied XSVF files to teach logic and basic electroincs via the Raspi.

     

    Moving up as I said you can then add larger FPGAs like the Spartan-3, good price point and enough flex for entry levels. However I think what your offering is a high end education kit or a really nice development kit.

     

    Anyway just some of my ideas tio throw in - truned intoa long answer so sorry about that but would be intrested to see anyones developments and hear your views too.

     

    Paul

    (@monpjc)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to pjclarke

    Hi Paul, nice to see you here. image

     

    I agree with everything you say about the problems in education.  I come from a very academic family, having been a university lecturer myself in EE and Computing before I went into industry, and half of my relatives being teachers in maths or science, so I've seen the difficulties personally both first-hand and second-hand.

     

    But all is not lost.  While the schools system as a whole is just not geared up for working with the Pi because of lack of curriculum, staffing, skills, time and money, and even less geared up for teaching programmable logic, the Pi is so inexpensive that official sanction and government-backed investment are in many cases not necessary.  I have little doubt that many teachers will be picking the Pi up personally and just "making it available" to their keener youngsters, even when there is no scheduled time for class-wide involvement, and in some cases even when it's beyond their personal area of competence.  You don't need a government curriculum nor well-equiped teaching labs to spark interest in technology.  Inquisitive minds will be drawn automatically to whatever is  available.

     

    I can't help but draw on personal experience of this.  At an age of 14 or 15 I was reading books on fine structure of stellar spectra and the stability of halide complexes.  My topics of interest were so far outside the school curriculum and the personal knowledge of my physics and chemistry teachers that my questions were more disruptive than helpful in class, yet the teachers all encouraged my inquiring deeper and deeper into what fascinated me.  What's more, labs and reagent cupboards were "made available" most definitely without official sanction (the school governers would have been horrified), and as a result lunch periods were a time of much fun and of very intensive personal learning and oiled the path towards a very technical career.  You just can't keep youngsters from learning if they want to. image

     

    The Pi is much safer than playing with chemicals, fortunately, but the same rules apply.  Teachers can easily encourage IT learning by making cheap computer systems available, curriculum or no curriculum, and the very low price of Raspberry Pi makes that possible.  It doesn't need to be taught class-wide at all, and it would in any case be the height of boredom for the majority,  The one or two natural geeks out of a class of a few dozen pupils is all that it takes to create a new generation of future engineers and scientists, and they will gravitate towards interesting technical things irresistibly if they are made available.

     

    On the specific issue of programmable logic, you might notice that earlier in the thread I was trying to bring CPLDs into the picture, not just FPGAs, and this was directly in response to the worry that the more complex a system is, the less valuable it is for education.  Even CPLDs are too complex for educating kids about the principles of programmable logic, with far too much "and magic happens here" being done by industrial-strength power tools.  Education is very different to vocational training, and exposing youngsters to proprietary tools with mind-boggling interfaces has deeply problematic issues of principle as well as hiding the mechanisms involved.

     

    Personally I think that even simpler programmable logic devices with basic open source tools would provide a better foundation for teaching the elements of this subject than any of the big name tools used for commercial work.  What's more, this approach would require nothing but the Pi itself, no additional powerful x86 PC to run the tools.  I know that all of us here are keen to use the most powerful devices and tools available, but that's because we are already experienced professionals, not pupils nor long-suffering school teachers.  There is a big disconnect occurring whenever someone suggests that programming a Spartan-3A might be featured in a school curriculum.  Yes it's possible, but it rather misses the point, and it adds major hurdles as well.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to pjclarke

    Hi Paul, nice to see you here. image

     

    I agree with everything you say about the problems in education.  I come from a very academic family, having been a university lecturer myself in EE and Computing before I went into industry, and half of my relatives being teachers in maths or science, so I've seen the difficulties personally both first-hand and second-hand.

     

    But all is not lost.  While the schools system as a whole is just not geared up for working with the Pi because of lack of curriculum, staffing, skills, time and money, and even less geared up for teaching programmable logic, the Pi is so inexpensive that official sanction and government-backed investment are in many cases not necessary.  I have little doubt that many teachers will be picking the Pi up personally and just "making it available" to their keener youngsters, even when there is no scheduled time for class-wide involvement, and in some cases even when it's beyond their personal area of competence.  You don't need a government curriculum nor well-equiped teaching labs to spark interest in technology.  Inquisitive minds will be drawn automatically to whatever is  available.

     

    I can't help but draw on personal experience of this.  At an age of 14 or 15 I was reading books on fine structure of stellar spectra and the stability of halide complexes.  My topics of interest were so far outside the school curriculum and the personal knowledge of my physics and chemistry teachers that my questions were more disruptive than helpful in class, yet the teachers all encouraged my inquiring deeper and deeper into what fascinated me.  What's more, labs and reagent cupboards were "made available" most definitely without official sanction (the school governers would have been horrified), and as a result lunch periods were a time of much fun and of very intensive personal learning and oiled the path towards a very technical career.  You just can't keep youngsters from learning if they want to. image

     

    The Pi is much safer than playing with chemicals, fortunately, but the same rules apply.  Teachers can easily encourage IT learning by making cheap computer systems available, curriculum or no curriculum, and the very low price of Raspberry Pi makes that possible.  It doesn't need to be taught class-wide at all, and it would in any case be the height of boredom for the majority,  The one or two natural geeks out of a class of a few dozen pupils is all that it takes to create a new generation of future engineers and scientists, and they will gravitate towards interesting technical things irresistibly if they are made available.

     

    On the specific issue of programmable logic, you might notice that earlier in the thread I was trying to bring CPLDs into the picture, not just FPGAs, and this was directly in response to the worry that the more complex a system is, the less valuable it is for education.  Even CPLDs are too complex for educating kids about the principles of programmable logic, with far too much "and magic happens here" being done by industrial-strength power tools.  Education is very different to vocational training, and exposing youngsters to proprietary tools with mind-boggling interfaces has deeply problematic issues of principle as well as hiding the mechanisms involved.

     

    Personally I think that even simpler programmable logic devices with basic open source tools would provide a better foundation for teaching the elements of this subject than any of the big name tools used for commercial work.  What's more, this approach would require nothing but the Pi itself, no additional powerful x86 PC to run the tools.  I know that all of us here are keen to use the most powerful devices and tools available, but that's because we are already experienced professionals, not pupils nor long-suffering school teachers.  There is a big disconnect occurring whenever someone suggests that programming a Spartan-3A might be featured in a school curriculum.  Yes it's possible, but it rather misses the point, and it adds major hurdles as well.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    I should also mention that while I was in academia, I experienced first-hand exactly the same thing as described repeatedly by Eben Upton of the Foundation, a very pronounced reduction in technical competency among our intake from UK schools over the years.  So many applicants lacked the elementary knowledge required to begin an EE/CSc degree that we had to offer remedial courses to bring them up to speed, or else we'd have 1st year intake consisting exclusively of extremely bright Chinese youngsters.

     

    It really was depressing.  A major change is required in school education or we're heading towards disaster as a country.  It's a technical world, and the real currency is technical skills, not dollars.  You can't avoid providing your future citizens with a technical education if you expect to remain relevant in the world.

     

    Morgaine.