Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 682 subscribers
  • Views 21368 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 13 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • pjclarke
    pjclarke over 13 years ago

    Hi all,

     

    Thanks for pointing me at this Morgaine.

     

    I think there are a few point to consider here I want to throw in. However I want to be clear that I'm very pro getting schools, collages and Uni's more hands on and involved with things like Raspi and FPGA/CPLDs.

     

    First off from a education point of view we have to consider what you guys are talking about and the target audiance. As someone who has teached kids in electroincs clubs and takes part in school engineering contests (as a judge) I had written this blog on my first views of the Raspi in educations. This was followed up by a head of ICT who poested this on Deaign Spark too.

     

    My point is however that education is just not geared up for the Raspi and certanlly not for FPGAs. I ahve spoken to a teacher only yeasterday about this and she confirmed that they have no idea what they are doing. So throwing FPGAs at them will scary them off. The key point she picked up from my blog above is that unless a package is supplied to schools that is clear and simple to use then it will not get past the teachers desk. This sounds harsh, but its so true. Its take two years for the Arduino to apear in school contests.

     

    Moving on to haveing a CPLD or FPGA attached to a Raspi I think is a good idea. The Raspi is limit in GPIO and anything that can help expand this will be good. As a first off I would use somthing like a simple CPLD as a direct access to the GPIO as this will hold its configuration at power up, allow simple patcheing and basic logic circuits to be run from it.

     

    The XAPP058 is a great starting point for someone to generate a JTAP programmer for the Raspi. This can then use XSVF files to program either the CPLD or another FPGA if attached.

     

    At this basic level I think you could then start offering not only programming but some simple VHDL / Verilog to schools and collages. However as pointed out you can't run the tools on the Raspi so will HAVE to have another machine for this. You then have to ask if this is protical. What is the Raspi really doing in this project that you can't do with a PC or some of the specially designed education kits like ther terasic DE2. Find that answer and argue it and then you can push Raspi and FPGA tech togetter into schools. However in my view, use pre complied XSVF files to teach logic and basic electroincs via the Raspi.

     

    Moving up as I said you can then add larger FPGAs like the Spartan-3, good price point and enough flex for entry levels. However I think what your offering is a high end education kit or a really nice development kit.

     

    Anyway just some of my ideas tio throw in - truned intoa long answer so sorry about that but would be intrested to see anyones developments and hear your views too.

     

    Paul

    (@monpjc)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to pjclarke

    "Logic!  Why don't they teach Logic at these schools?" asks the Professor in The Lion, the Witch, and the Wardrobe.  When I was a lad in USA schools, there was no instruction in Logic, and I imagine it's no different today and probably no different in the UK.  I had to learn Logic on my own.  My mother actually got me started by buying me a dice-based logic game called WFF 'n' Proof, probably because she didn't know what to get and the sales clerk said it would be "educational".  WFF 'n' Proof was pretty useless as a game since there wasn't anyone to play it with, but the instruction manual was a terrific introduction to symbolic logic and got me hooked on the idea of solving logic problems automatically.  The Madison, Wisconsin public library had a terrific collection of computer and electronics books, and before long I was making RTL circuits using schematics from the GE Transistor Handbook.  Then 7400 TTL showed up at an impressionable age and suddenly I could easily make really good logic circuits.  Bliss!  CPLDs and FPGAs brought it up to the next level, where you can do far more and not have to worry about the details of logic minimization and having to re-wire to fix errors.  Real chip design on the cheap, no masks, no minimum quantities, and no NRE.  Double Bliss!

     

    My point here is:  So what if it's impractical to teach logic design in elementary/high school classes?  The kids who will run with it will do so on their own if the tools are available and cheap and there is good documentation.  Kids who don't want to bother with logic -- or thinking in general -- aren't going to be sold no matter how good the curriculum is.  To quote Jean-Jacques Rousseau (Émile, from memory): "A child should not learn by Rote what he cannot understand.  He must learn by Experience what he can understand."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago in reply to pjclarke

    "Logic!  Why don't they teach Logic at these schools?" asks the Professor in The Lion, the Witch, and the Wardrobe.  When I was a lad in USA schools, there was no instruction in Logic, and I imagine it's no different today and probably no different in the UK.  I had to learn Logic on my own.  My mother actually got me started by buying me a dice-based logic game called WFF 'n' Proof, probably because she didn't know what to get and the sales clerk said it would be "educational".  WFF 'n' Proof was pretty useless as a game since there wasn't anyone to play it with, but the instruction manual was a terrific introduction to symbolic logic and got me hooked on the idea of solving logic problems automatically.  The Madison, Wisconsin public library had a terrific collection of computer and electronics books, and before long I was making RTL circuits using schematics from the GE Transistor Handbook.  Then 7400 TTL showed up at an impressionable age and suddenly I could easily make really good logic circuits.  Bliss!  CPLDs and FPGAs brought it up to the next level, where you can do far more and not have to worry about the details of logic minimization and having to re-wire to fix errors.  Real chip design on the cheap, no masks, no minimum quantities, and no NRE.  Double Bliss!

     

    My point here is:  So what if it's impractical to teach logic design in elementary/high school classes?  The kids who will run with it will do so on their own if the tools are available and cheap and there is good documentation.  Kids who don't want to bother with logic -- or thinking in general -- aren't going to be sold no matter how good the curriculum is.  To quote Jean-Jacques Rousseau (Émile, from memory): "A child should not learn by Rote what he cannot understand.  He must learn by Experience what he can understand."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    @John:  My answer:  Exposure. image

     

    Kids can't get enthused about things that they've never heard about.  A Pi sitting in the corner blinking its LEDs during science class is a very powerful attractor for youngsters with the right mental disposition.  And if you can work it into science experiments as a tool to turn things on and off, you're halfway towards giving future engineers a lifetime of enthralling fun that just happens to be very valuable to society as well.

     

    The process is self-selecting, but it needs a spark.  And in this new Pi era, sparks are cheap to provide. image

     

    None of this argues against your point that many kids will find out about technology on their own, which is very cool.  But not everyone will, and given the price of a Pi, providing additional exposure in schools has an astronomic benefit/cost ratio.

     

    Morgaine.