Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 682 subscribers
  • Views 21393 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 13 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • guzunty
    guzunty over 12 years ago

    Yes indeed.

     

    > So I don't see a lot of people using ready-made cores as a springboard to designing their own programmable logic.

     

    Well let's see what happens with the Guzunty Pi open hardware CPLD board. If even a few percent of the people who like the idea of ready made cores go on the learn to program their own cores from HDL, schematic or tables thats a Good Thing.

     

    Totally agreed on the remote tools idea. Xilinx used to have a web interface themselves did they not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to guzunty

    Derek Campbell wrote:

     

    Well let's see what happens with the Guzunty Pi open hardware CPLD board.

    Alex Eames posted a nice review of the Guzunty Pi at: http://raspi.tv/2013/guzunty-pi-open-source-cpld-board-for-the-raspberry-pi

     

    As I've said upstream, the XC9572XL-10TQ100CXC9572XL-10TQ100C is a terrific CPLD which I've used in a lot of work projects.  Very nice balance of resources.  Ah, if only Xilinx would publish the bit format so it could be programmed with FLOSS tools...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Alex Eames posted a nice review of the Guzunty Pi at: http://raspi.tv/2013/guzunty-pi-open-source-cpld-board-for-the-raspberry-pi

     

    As I've said upstream, the XC 9572 XL is a terrific CPLD which I've used in a lot of work projects.  Very nice balance of resources.

     

    Due to a high level of interest, Derek has now made Guzunty Pi boards and kits available world wide: https://github.com/Guzunty/Pi/wiki/Buy-a-Guzunty.  First programmable logic board I've seen that costs less than a RasPi image

     

    IMO Guzunty Pi would be a nice addition to element14's RasPi accessory assortment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • guzunty
    guzunty over 12 years ago in reply to johnbeetem

    Hi John,

     

    Thank you very much for the words of encouragement.

     

    Yes, there were a number of design goals I set myself:

     

    - Low cost.

      There seemed to me no point in doubling the cost of a Rasperry Pi with expensive add-ons. I wanted to create a 'Pocket money

      peripheral'. CPLDs are so much cheaper than FPGAs, it's a great way to dip your toe in the water before thinking about trading up

       to FPGA.

    - Easy to build.

      There's no better way to keep the cost down than to make it yourself. And the satisfaction of seeing your creation working comes

      absolutely free! I therefore wanted the board to be very easy to build. It is through hole soldering only, and the solder mask on the

      PCB makes it easier than building on stripboard. If you follow the instructions on GitHub carefully, you can build one of these for

      sure. At this time, I have no reports of any failed builds out in the field.

    - Downloadable cores.

      I think everyone will agree that learning to design your own core does require some investment of time. By offering ready made

      cores, you can start right away, knowing that there is more you can do with it later.

    - Educational.

      Aligns with the Raspberry Pi philosophy.  I think the Pi revolution is about more than learning to program software. Once you have

      a Guzunty running on your RPi, who could resist the temptation to learn HDL and begin to design cores yourself? Certainly not

      me :-)

     

    I must have done something right, because interest in the Guzunty CPLD add on for the RPi has been fantastic. I'm now able to

    offer a kit of parts anywhere in the world. See https://github.com/Guzunty/Pi/wiki. Just click on Pages > Buy a Guzunty

     

    best regards and thanks to everyone for the support,

     

    Derek

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to guzunty

    More information from Derek about his super little Guzunty CPLD board over in  this other thread.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to guzunty

    More information from Derek about his super little Guzunty CPLD board over in  this other thread.