Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 682 subscribers
  • Views 21560 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 13 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    Regarding inexpensive FPGA development boards, here's a new pair of boards for the Lattice iCE40 "Los Angeles" family: $39 for a small board with a 1280-cell + 64Kb FPGA and built-in USB programmer.   I hadn't heard of the iCE40 before -- it seems to be something Lattice got when it acquired SiliconBlue.  The iCE40 looks like a pretty clean and simple architecture, making it quite suitable for students.  As usual, you need a PC to run proprietary tools, but at least they say they run under GNU/Linux.  The USB programming interface is an AT90USB processor.  I don't know if they provide an open way to talk the the AT90USB or if you have to use Lattice tools (or reprogram the AT90USB).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    Thanks John, looks very interesting.

     

    OpenOCD has an entry for Lattice in their Debug Adapter Hardware section, pointing to Lattice's download cables -- http://www.latticesemi.com/lit/docs/devtools/UG48.pdf . I don't know if this relates in any way to these new ICE40 boards though.

     

    I looked around at my local Lattice stockist (Mouser) and found the ICE40 board listed for 27 pounds, but not in stock.  They have lots of ICE40 devices listed too, the smaller ones for under 3 quid in single units, but alas all non-stocked and on 14 week delivery.

     

    I see that my Mouser also has the Lattice XP2 Brevia Dev Kit in stock though,  for 34 pounds, which seems quite reasonable -- http://www.latticesemi.com/products/developmenthardware/developmentkits/xp2brevia2developmentkit.cfm .  Their CPLD ranges are of course even cheaper.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    More Lattice ICE40 links:

     

    • Lattice announcement - http://www.latticesemi.com/corporate/newscenter/productnews/2012/r120508announcesproductio.cfm
    • ICE40 Marketing page - http://www.latticesemi.com/products/cpld/ice40series.cfm?CFID=76612705&CFTOKEN=53568543&jsessionid=f0308cbc51f09d4ff973157115e4c7052644
    • iCEblink40-HX1K Evaluation Kit - http://www.latticesemi.com/products/developmenthardware/developmentkits/iceblink40hx1kevaluationk.cfm
    • Front/Back/Side images - http://www.latticesemi.com/images/img45631.jpg , http://www.latticesemi.com/images/img45633.jpg , http://www.latticesemi.com/images/img45635.jpg
    • Development resources - http://www.latticesemi.com/dynamic/index.cfm?fuseaction=view_documents&sloc=01-01-09-00-22
    • iCEcube2 Design Software - http://www.latticesemi.com/products/designsoftware/icecube2/index.cfm
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    More Lattice ICE40 links:

     

    • Lattice announcement - http://www.latticesemi.com/corporate/newscenter/productnews/2012/r120508announcesproductio.cfm
    • ICE40 Marketing page - http://www.latticesemi.com/products/cpld/ice40series.cfm?CFID=76612705&CFTOKEN=53568543&jsessionid=f0308cbc51f09d4ff973157115e4c7052644
    • iCEblink40-HX1K Evaluation Kit - http://www.latticesemi.com/products/developmenthardware/developmentkits/iceblink40hx1kevaluationk.cfm
    • Front/Back/Side images - http://www.latticesemi.com/images/img45631.jpg , http://www.latticesemi.com/images/img45633.jpg , http://www.latticesemi.com/images/img45635.jpg
    • Development resources - http://www.latticesemi.com/dynamic/index.cfm?fuseaction=view_documents&sloc=01-01-09-00-22
    • iCEcube2 Design Software - http://www.latticesemi.com/products/designsoftware/icecube2/index.cfm
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    While poking around Lattice goodies at Mouser, I just noticed that they also stock the Lattice MachXO2 range of "PLD" devices which Michael described earlier as an FPGA-CPLD crossover with added hardwired peripherals.  At 21 pounds for the breakout board, that certainly looks appealing.

     

    • Lattice LCMXO2-1200ZE-B-EVN - http://uk.mouser.com/ProductDetail/Lattice/LCMXO2-1200ZE-B-EVN/?qs=vI1DwPFGRq8Zkw8xAIBGGUlXAPoDVpLrLaAGRk6g8KM%3d
    • MachXO2-1200ZE Breakout Board Evaluation Kit - http://www.latticesemi.com/documents/EB68.pdf

     

    Farnell UK has a somewhat more expensive MachXO2 board in stock:

     

    • Lattice LCMXO2-1200ZE-P1-EVN - http://uk.farnell.com/lattice-semiconductor/lcmxo2-1200ze-p1-evn/dev-kit-programmer-machx02-pico/dp/2064276
    • MachXO2 Pico Development Kit - http://www.latticesemi.com/documents/EB61.pdf

     

    I haven't yet compared the two.

     

    PS.  Now I have.  The first (cheaper) unit is just a breakout board, hence better for embedding, whereas the second is a little development / evaluation kit with a few simple devices available on board for the PLD to poke, even a small LCD.  Both are very useful boards, horses for courses.

     

    General MachXO2 device information:

     

    • MachXO2  Family Data Sheet, 103 pages - http://www.latticesemi.com/documents/38834.pdf
    • MachXO2 Family Handbook, 436 pages - http://www.latticesemi.com/documents/HB1010.pdf
    • MachXO2 Overview Video -http://www.latticesemi.com/products/cpld/machxo2/overviewvideo.cfm?gclid=CL7c7PCk968CFcshtAodBX9VDw

     

    And intriguingly ...

     

    • "The WISHBONE Bus in the MachXO2 is compliant with the WISHBONE standard from OpenCores." -- http://www.latticesemi.com/documents/TN1205.pdf

     

    That rings the right bell for me. image