Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Webinar. What Webinar?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 711 subscribers
  • Views 3597 views
  • Users 0 members are here
Related

Webinar. What Webinar?

e14 Contributor
e14 Contributor over 14 years ago

Well I have to say the Webinar was a bit of a disaster for me. I registered to attend and got email acceptance on 23/3 and spent an hour trying to get in no joy so many pitfalls. Really fed up. Yes I tried different browsers. image

 

Sad me. No Pi no webinar no CE mark yet. Oh well sits back and waits some more.

 

One day my parts will come. image

  • Sign in to reply
  • Cancel
  • ubuntourist
    ubuntourist over 14 years ago in reply to e14 Contributor

    Q&A Session for Programming The Raspberry Pi

    Session number:  841475134
    Date:  Wednesday, April 04, 2012
    Starting time:  7:03 AM


    nuno alves6:30 AMQ:good morning!
    Mike Powell6:37 AMA:Hi everyone. Welcome - we're just setting everything up now...
    AB AB6:38 AMQ:Excuse me when is it starting
    Chris Sullivan6:39 AMA:Hi, the session will begin in 20 minutes.  Not long now!
    Jeffrey Tooker6:48 AMQ:Hello from California
    Mike Powell6:48 AMA:Welcome everyone - attendees joining very rapidly now!
    chris hillcox6:45 AMQ:i cant hear anything at the moment. how do I know if the audio works.
    Mike Powell6:52 AMA:Hi Chris - it'sll be quiet until around 2.58 pm BST
    David S7:03 AMQ:Hi Mike. Will this be recorded and made available?
    Mike Powell7:03 AMA:Hi David - yes it will be.
    Rosso Maltese6:59 AMQ:sorry, still no sound
    Mike Powell7:04 AMA:Have you used the computer audio or telephone option? Worst case we're recording this for you...
    chris hillcox6:48 AMQ:Is it ok if I record this on my dictaphone. I don't have my Pi yet so may want to listen again when I do get it.
    Mike Powell7:06 AMA:Hi Chris, this will be recorded for you anyway.
    Andrea Gatti6:47 AMQ:excuse me, what I have to do if I see the message error "You do not have the necessary audio  capability to join Audio Broadcasting"? Thanks a lot!
    Mike Powell7:07 AMA:Hi Andrea, try using the Audio option in WebEx and dial in using a telephone.
    Liam Fraser6:46 AMQ:Is this event being recorded for those who miss it?
    Mike Powell7:07 AMA:Hi Liam, yes it is.
    Timothy Giles7:08 AMQ:Is this the alpha , beta or final board in the image?
    Mike Powell7:09 AMA:Hi Tim, I can't verify, but I'd be surprised if it wasn't a final board. Eben is in a different location to me.
    AB AB7:09 AMQ:What type of HDMI port do you use to connect to a PC Monitor for a laptop.
    Mike Powell7:10 AMA:Hi AB, in my demos I used a standard HDMI-HDMI cable, then a HDMI-DVI connector for a DVI monitor.
    Keith Madderson7:10 AMQ:is the Raspberry Pi being supplied boxed, or is it just as a PCB as being shown here?
    Mike Powell7:11 AMA:Hi Keith, as shown.
    Evandro Junior7:11 AMQ:Dear Eben, I´ve received an email from element 14 saying that the pre-order for Raspbery PI was availble, however there was no option to select Brazil for the country of delivery on the form. Can it be shipped to Brazil?
    Mike Powell7:13 AMA:Hello Evandro, it can be shipped to Brasil. Please contact your local Newark office for help.
    Chris Prosser7:12 AMQ:Does the SD Card have to be 2GB?
    Mike Powell7:14 AMA:Hi Chris, 2GB is a good size. 2GB+ is what you need.
    Stéphane Zorio7:13 AMQ:Is the Raspberry PI work with 16Gb or 32Gb SD Card ?
    Mike Powell7:14 AMA:Hi Stephane, I haven't tested it. No reason why it shouldn't work.
    Andrea Benini7:12 AMQ:I guess dd-removable is some sort of port of linux dd command, is it right ? Because I don't use Win
    Mike Powell7:15 AMA:Hi Andrea, I don't know the dd project, but I'd assume so.
    Janar Plinkner7:13 AMQ:I presume the image can be installed to the SD card in linux with the command dd?
    Mike Powell7:16 AMA:Hi Janar, yes thats right.
    Chad LaFarge7:14 AMQ:Does the Debian distro used have UVC drivers (for driverless Webcams) included? I've also seen references to a Fedora and Ubuntu distro... same question. Many thanks.
    Mike Powell7:16 AMA:Hi Chad, I haven't tried looking for that yet. Let us know!
    Mark Redden7:14 AMQ:Can an SD card larger than 2GB be used?
    Mike Powell7:16 AMA:Hi Mark, mine was 4GB, so yes it can.
    Jamie Oliver7:14 AMQ:The presentation seems to be lagging, and taking ages to update between slides. Anything I can do to improve this?
    Mike Powell7:17 AMA:Hi Jamie, not sure - think it may be an issue at Eben's end. Sorry.
    Patrick Potter7:14 AMQ:Mike, what should we look for in an SD card?  Are there some cards we should avoid?
    Mike Powell7:18 AMA:Hello Patrick, please look at the bundled packages on element14.com for guidance.
    gerrit polder7:15 AMQ:is it posible to flash the sd card form linux or mac os x using standard dd tools?
    Mike Powell7:19 AMA:Hi Gerrit, yes for Linux. Don't know for Mac OS.
    Pavol Bujna7:15 AMQ:can I download this event later?
    Mike Powell7:19 AMA:Hi Pavol, yes the video will be available later on.
    Eric Lange7:15 AMQ:What will happen if you plug the unit into a PC instead of a mobile charger?
    Mike Powell7:20 AMA:Eric, everything will work fine.
    Jay Bhagat7:15 AMQ:will the clock be persistent?
    Mike Powell7:21 AMA:Hi Jay, no - there is no RTC on board. But if the board is connected to the internet via it's ethernet adaptor, the OS goes and find the time/date from a time server.
    Brian Schmiedlin7:17 AMQ:Will the clock keep time even though the unit is powered off?
    Mike Powell7:21 AMA:Hi Brian, no there is no RTC.
    Nik Butler7:18 AMQ:is there vi  as well ?
    Mike Powell7:21 AMA:Hi Nik, yes, vi is there.
    Lee Hardman7:19 AMQ:Hi Mike, is IDLE bundled with the standard image?
    Mike Powell7:22 AMA:Hi Lee, I don't know - I'd need to check.
    Matt Moss7:20 AMQ:Hi Mike, Is the Rasberry Pi's RCA Video output going to be PAL or NTSC format? Thanks!
    Mike Powell7:23 AMA:Hi Matt, both and is configurable in a text file.
    7:24 AMQ:when will Fedora be available?
    Jean-Francois Lagarde7:19 AMQ:Hello Mike, a little off topic, but when I ordered the Raspberry Pi on newark a few weeks ago, it said that it would be available for shipping mid-april. This morning I checked my order and it says mi-august. Everything has been delayed?
    Mike Powell7:24 AMA:Hi Jean-Francois, I'm surprised at that. Please speak to your local Newark office about this.
    martijn steegmans7:22 AMQ:Does the hdmi port support digital audio?
    Mike Powell7:26 AMA:Hi Martijn - yes it does.
    Frank Buss7:22 AMQ:is it possible to start something more comfortable like KDE or Gnome on it?
    Mike Powell7:27 AMA:Hi Frank - yes, liight versions exist to give a very impressive desktop environment.
    John Ennis7:23 AMQ:Is it possible to ssh into the Pi?
    Mike Powell7:27 AMA:hi John - yes it is. In the Debian distro, the SSH server starts automatically at boot.
    mark goldie7:24 AMQ:does the Pi board come with some kind of BIOS control? Also, on connecting the LAn cable, how would one control DHCP registration ?
    Mike Powell7:28 AMA:Hi Mark, there is no BIOS, but there is a configuration text file to set up the basics of the board.
    Jean-Francois Lagarde7:22 AMQ:I understand that the board automatically connects to a time server and the internet via dhcp? if we need static ip, I guess we need to modify the sources or is there a way to configure the settings of the Pi?
    Mike Powell7:29 AMA:Hi Jean-Francois, you can modify the network settings easily as you would any computer.
    Andrea Benini7:25 AMQ:Is there an I2C bus in the GPIO connector available for external peripherals ? I've made a really easy RTC circuit on I2C bus and I'd like to connect it to the PI. I can supply an RTC if the linux image is able to read it from I2C
    Mike Powell7:31 AMA:Hi Andrea - yes there is.
    Herbert Keks7:30 AMQ:Will it be possible to run http://www.tvdr.de/ or xbmc on the Raspberry? This would be the killer app in my eyes. But I'm not sure about the video hw acceleration.
    Mike Powell7:34 AMA:xbmc has been shown to work. The onboard GPU supports high resolution, full motion video.
    gary Paterson7:31 AMQ:Hi Mike, what is the default version of python and is python 3 available?
    Mike Powell7:34 AMA:Hi gary, I don't know the answer to that sorry.
    robert jones7:35 AMQ:will Class B (residential) FCC/EC compliance be required?
    s2. henry7:32 AMQ:hi,  what power supply do we need ? (voltage, current, physical size ?)
    Mike Powell7:36 AMA:A 'regular' phone charger with microUSB plug will work.
    7:36 AMQ:does Farnell have a rep at the factory?  If so, can they take a picture showing how many units have been built?
    7:37 AMQ:how many pallets of units were shipped back to China when the ethernet jack problem was found?
    rohan kumar7:38 AMQ:Is the Pi overclockable?
    Mike Powell7:39 AMA:Hi Rohan, yes it can be via the configuration script.
    Charlie Godwin-Brown7:39 AMQ:Can you get a desktop for your RPi?
    Mike Powell7:39 AMA:Yes, the Debian distro contains a GUI that you start with sudo startx.
    bryce foster7:44 AMQ:If the raspberry pi is put in an enclosed project box will we have to worry about the ARM processor over heating?
    Mike Powell7:42 AMA:Hello Bryce, in my opinion you don't need to worry. The whole board only consumes 2-3W.
    abi nathan7:49 AMQ:what is the maximum amperage the pi can handle at 5v? Thanx
    Mike Powell7:44 AMA:Hi Abi, the Pi draws the current it requires from the USB power source. This is typically 500mA-750mA depending on what the GPU is doing.
    Stéphane Zorio7:42 AMQ:Is a Apache server include in the Debian Distribution ?
    Mike Powell7:45 AMA:Hi Stephane, I don't know, but you can use a apt-get install command to install it as long as you are on the internet.
    Stefan Fischer7:42 AMQ:is the gpio pin description available?
    Mike Powell7:46 AMA:Hi Stefan - look at element14, the pin assignment is there.
    Richard Blundell7:43 AMQ:I'm hoping to add a 2nd network adaptor to my Pi (when it comes) and use it as a logger/filter on my home broadband.  Will this work and can you give me any pointers where to look to set this up (I only had a little Linux use some years ago)?
    Mike Powell7:47 AMA:I don't see why this shouldnt work using IP Tables in Linux for example.
    Andrea Gatti7:43 AMQ:Hi, I'm a beginner so I want to know if there is any manual or guide online for learning to use and programm the raspberry pi?
    Mike Powell7:48 AMA:Hi Andrea - look at the various forums and guides that will grow on element14 as time goes by.
    John Morris7:44 AMQ:Can I hook the RPi up to a laptop screen?
    Mike Powell7:50 AMA:Hi John, not directly. Only to HDMI TV, DVI monitor or older style  TV. Command line via an SSH terminal is possible using an external laptop.
    Alessandro Ancillotti7:45 AMQ:Will RaspberryPI able to run a webserver like lighttpd?
    Mike Powell7:52 AMA:Hi Allesandro, yes I have run mini_httpd on it.
    AB AB7:50 AMQ:can you use a triple usb adapter.
    Mike Powell7:53 AMA:Yes, hubs are supported.
    Chad Gray7:53 AMQ:I am not a linux guy, but would we have to compile software like Apache/Tomcat/MySQL for the RPI?  Any examples of doing this?
    Mike Powell7:54 AMA:Yes, you can compile any programme from source, but it doesn't mean the programme will run acceptably.
    Andrew Gates7:54 AMQ:I missed the beginning of the presentation, is it going to be posted on the Raspberry Pi website?
    Mike Powell7:55 AMA:Hi Andrew, it will be on element14.
    Jean BRUDER7:55 AMQ:Hi all, sorry to be late ... Is is possible to download this webinar if it has been recorded ?
    Mike Powell7:55 AMA:Hello Jean, it will be available on element14 soon. Don't worry.
    Patrick Daubinger7:56 AMQ:are you planing to open the pcb schematics?
    Mike Powell7:56 AMA:Hi patrick, they will be opened later this year.
    adam ricket7:57 AMQ:are there any plans for a distributor in australia?
    Mike Powell7:58 AMA:It is element14.

     

    Message was edited by: Kevin Cole

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to ubuntourist

    I joined the webinar in plenty of time (almost half an hour in advance) but the webinar software seems distinctly flaky.  It complained I didn't have audio (untrue), and refused to show me anything other than a list of the speakers.  I tried dialling in to the 0800 number given, but although that got me audio it wasn't a lot of use without the pictures.

     

    Altogether a pretty naff software solution.  Please don't use it again.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    "

    It would appear that maybe the webinar only worked with windows???Oh, the irony..

    "

     

    Maybe, maybe not.. it didn't work in windows firefox 11 for me - logging in made an attempt to install a corrupted plugin or some from premierfarnell.webex.com or some such and iexplorer kept crashing at the same point.

     

    It was bad timing for me anyway so I gave in in the hope of it being on youtube tomorrow image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 14 years ago in reply to e14 Contributor

    Why do you say that the 'plugin' was corrupted?

    A lot of people (myself included) downloaded and ran it witout any problems?

    I am sorry, but I do consider the software to be flaky either!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi everyone! I uploaded a temporary recording of the Webinar until e14 puts their better and official copy up.

     

    http://www.youtube.com/watch?v=woSUVNovI70

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 14 years ago in reply to e14 Contributor

    Thank you for uploading that, as I found it interesting to go back to check out some of the 'slides' again.

     

    Hopefully these will be made available for individual downloading by Element 14 in due course.

     

    I guess that when the dtae of this 'webinar' was first decided, it was anticipated that the first batch would have already been shipped, and that some people would already have received one, which has not unfortunately been the case.

     

    Let's hope that it will be not be too long now though before things start moving again.

     

    A very interesting webinar, nevertheless, and thanks must be given to Element 14 for hosting it, and obviously to Eben for his presentation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 14 years ago in reply to e14 Contributor

    Unfortunately I didn't make it to the live showing (2 a.m my time), however I'm suprised about the reports of Webex failing. Webex are owned by Cisco and I have used it in another life for demonstrating medical pathology slides (2TB images) to researchers amd medical staff world wide - it always performed OK apart from the one hospital that was still on dial up and a weird exchange system.

     

    What is confusing if Webex someone hasn't used Webex before is that it isn't always apparent which page you should be looking at and how if you've clicked on the list of participants by mistake how to get back to the actual event.

     

    I have both Firefox and 11.0 and IE9 installed, and Webex does seem to work better with IE with those versions. There is also a Webex Player that some events require which can be downloaded and installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to bodgy

    Although it's generalizing, all proprietary systems are doomed to be flakey, non-portable, and permanently giving people headaches.

     

    Webex is a good example of this.  And, given Cisco's litigation-based "business plan" for Webex, it's not going to get any better in the future.  I would tend to recommend to Element 14 that they stick to open standards, even if it means a reduction in bullet points.  At least open standards reduce the headaches at the same time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to bodgy

    I have both Firefox and 11.0 and IE9 installed, and Webex does seem to work better with IE with those versions.

     

    I think you may have put your finger on it there.  It looks like this is an application which is thoroughly tested for Windows, but whilst it provides token Linux support it's a bit touch-and-go whether it works or not.

     

    I was using Debian Squeeze with Firefox.  I checked the hardware and software requirements in advance.  It said I would need Flash and the test for Flash worked fine.  (I use the official version.)  When I came to join the webinar however, it seemed to download a Java application instead.  This ran but refused to show the webinar.

     

    It would be good if there were a way to test in advance whether the software is working.  It's really annoying to find out only once the thing has started that the software doesn't work, then spend half the time of the event hunting through the rather sketchy help to see if you can find anything.

     

    I did find one knowledge-base article which said that the software wouldn't work on Windows 7 unless you had something plugged into your microphone port (huh, what?!)  I tried plugging a microphone in and restarting in case the same bug affects the Linux version but that didn't help.

     

    Thank you to the person who put a copy on Youtube.  It was a gently informative talk.  Pity about the technology failure.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for that video link. Most kind.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>