Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Faulty board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 278 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Faulty board

e14 Contributor
e14 Contributor over 14 years ago

Ive also sent this to Liz but you guys might be better placed to answer,

 

Got my Pi yesterday and not had much luck, every seems to boot ok but after a while (depending what is plugged in) USB lose power closely followed by Ethernet (about 15 second delay but happens everytime the USB drops) but the OS continues to run

 

I thought this was going to be the Power Supply based on the forums however starting to think its not, ive tried the following chargers

 

Official HTC 1000mah (using official HTC USB lead as well as trying a official Samsung one as well)

2x Official Blackberry 700mah (lasts the longest on this one)

From Powered Belkin USB Hub (not sure of ratings on this one)

 

My mouse and Keyboard are both 5v 100mah rated and have tried the above chargers with the Keyboard/Mouse directly plugged in and via Hub. For all of the chargers the voltage from GPIO headers never drop below 4.76v (using the Blackberry charger never drops below 4.84v)

 

Theres no set point where it will drop though without ethernet it lasts longer, but seems to drop quicker when the CPU gets used (and still drops even when idle after a while). However last night (talking after 6hrs of testing and trying to get it to work) it did seem to become more stable (still wouldnt accept ethernet though) its been mentioned on the forum it could be a faulty Polyfuse.

 

Full Forum Thread if you want to have a read is at http://www.raspberrypi.org/forum/troubleshooting/usb-bus-seems-to-be-shutting-down-after-30seconds

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 14 years ago

    Given all the symptoms listed here and at raspberrypi.org, I'd suspect either too much resistance in the USB cable (though you have tested two cables) or the polyfuse F3 (bad component or bad solder joint) or perhaps micro USB connector S1.  You have reported voltages at the GPIO +5V pin.  You could also check voltages at S1 pin 1, though probing is tricky.  If S1 pin 1 is steady near +5V during your failure modes, I'd suspect F3.  If the voltage at S1 pin 1 is dropping during your failure modes, it's probably a poor cable, a defective S1, or a bad S1 solder joint.

       Another thing to try is shorting out F3 with a wire jumper.  If this makes the problem go away, I'd suspect F3 is bad or poorly soldered.  A bad solder joint may conduct but add resistance.

       JMO/YMMV: These opinions are offered without warranty.