Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi and Windows 8
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 712 subscribers
  • Views 2889 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi and Windows 8

e14 Contributor
e14 Contributor over 14 years ago

Will the up coming Windows 8 ARM port run on the Pi?

 

kindly,

J

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    I don't believe so.  Every reference I've seen to Windows in the RaspberryPi.org FAQ and forums have stated no.  And I sure hope not as any Windows 8 ARM device must be locked down by manufacturer to only run Windows:

     

    http://www.xda-developers.com/feature/microsoft-confirms-lockdown-of-arm-devices-running-windows-8/

     

    "On an ARM system, it is forbidden to enable Custom Mode. Only Standard Mode may be enable.

    Disabling Secure [Boot] MUST NOT be possible on ARM systems."

     

    What this means for XDA Developers, and the development community as a whole, is that unless a security exploit with UEFI is found, no ARM device with Windows 8 will ever run anything other than Windows 8 and Metro UI.

     

    The Raspberry Pi is able to meet its magical price because it leverages decades of open source software.  I hope that folks enticed by the low price of the Pi will get to become familiar with, and come to appreciate, Linux and the open source software ecosystem.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Drew,

      Would this lockdown prevent a device manufacturer from selling a version of their

    device without WIndows 8, for use with Linux?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Drew,

      Would this lockdown prevent a device manufacturer from selling a version of their

    device without WIndows 8, for use with Linux?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    No I don't think so.  I think what it means if a manufacturer wants to make an ARM device that Microsoft will allow Windows 8 to run, then it has to be locked down so that it will only boot Windows 8.  Thankfully, the Foundation has designed the Pi for Linux so this isn't really a concern.  And given that, it will never be certified by Microsoft to run Windows 8. 

     

    I suppose the only theoretical way to get Windows 8 ARM to run would be to install some modified version on the Pi (which I presume would violate Microsoft's licensing).  Regardless, as you pointed out, the memory is limited and, in an ironic twist, the powerful proprietary GPU capabilities are only being made available for Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to fustini

    will the Raspberry PI run earlier versions of windows? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 14 years ago in reply to cullimore

    I'm not sure if dosbox will run on an ARM, but if it did, you might be able to run windows 3.1 in it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cullimore

    Darren,

     

       Why would you want to?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    > Why would you want to?

     

    Maybe so that Windows 8 for ARM viruses, malware and spyware can run on it? image

     

    Joking aside, when there are millions of Raspberry Pi in the world, you can be certain that the sociopaths and organized crime will be attracted to Pi as yet another infection vector.  My guess is that netfilter and iptables will become an important Rpi topic in just a matter of months, if not before.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to bodgy

    Bodgy, Someone has run windows 3.11 in Dosbox on the Rpi forum: http://www.raspberrypi.org/forum/general-discussion/chips-challenge-windows-3-1?value=chips%20challenge&type=1&include=3&search=1

     

    I'm too busy with Quake at the moment to experiment :-)