Raspberry Pi Forum USB and LAN ports not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 678 subscribers
  • Views 5907 views
  • Users 0 members are here
Related

USB and LAN ports not working

Former Member
Former Member over 13 years ago

I received my Raspberry Pi today, but unfortunately neither the USB ports or the LAN port appear to be working.

 

I have tried numerous low power USB devices like keyboards mice etc. but can't get any life out of them, although I am able to charge my phone from the ports. Same results using two different 2A adapters to power the Pi and with a powered USB hub.Tried connecting the LAN port but the light on the router indicating a device is attached did not come on.

 

I've tried Debian, Arch and Fedora from RaspberrPi.org and also tried the kernel update which I believe is to address a different issue with USB. At this stage I'm fairly sure there is a fault (LAN is connected through USB I believe?). I'll wait and see if anyone else reports similar problems, otherwise I think I'll have to return it.

 

Does anyone have any suggestions or has had a similar experience with theirs?

 

Thanks

Mark

  • Sign in to reply
  • Cancel
Parents
  • bodgy
    bodgy over 13 years ago

    Just one final thought before you go to the bother of either begging, buying or stealing (did i say that?) a multimeter or sending it back to E-14, have you double checked your SD Card image isn't corrupt?

     

    Do you have a different keyboard you could try?  The reason I mentioned in my first post specifically conecting a keyboard into the lower port is because when I tried my USB keyboard in a hub it didn't work, nor did it in the top USB connector, it only works in the lower one.  I had no problem with a wireless keyboard plugged into my powered hub though.

     

    Just had a further thought!

     

    If you are using a powered hub try connecting both the USB data lead (from the hub) AND the 5v fly lead connected into both USB ports and see if that makes any difference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bodgy
    bodgy over 13 years ago

    Just one final thought before you go to the bother of either begging, buying or stealing (did i say that?) a multimeter or sending it back to E-14, have you double checked your SD Card image isn't corrupt?

     

    Do you have a different keyboard you could try?  The reason I mentioned in my first post specifically conecting a keyboard into the lower port is because when I tried my USB keyboard in a hub it didn't work, nor did it in the top USB connector, it only works in the lower one.  I had no problem with a wireless keyboard plugged into my powered hub though.

     

    Just had a further thought!

     

    If you are using a powered hub try connecting both the USB data lead (from the hub) AND the 5v fly lead connected into both USB ports and see if that makes any difference.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.