Raspberry Pi Forum USB and LAN ports not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 678 subscribers
  • Views 5925 views
  • Users 0 members are here
Related

USB and LAN ports not working

Former Member
Former Member over 13 years ago

I received my Raspberry Pi today, but unfortunately neither the USB ports or the LAN port appear to be working.

 

I have tried numerous low power USB devices like keyboards mice etc. but can't get any life out of them, although I am able to charge my phone from the ports. Same results using two different 2A adapters to power the Pi and with a powered USB hub.Tried connecting the LAN port but the light on the router indicating a device is attached did not come on.

 

I've tried Debian, Arch and Fedora from RaspberrPi.org and also tried the kernel update which I believe is to address a different issue with USB. At this stage I'm fairly sure there is a fault (LAN is connected through USB I believe?). I'll wait and see if anyone else reports similar problems, otherwise I think I'll have to return it.

 

Does anyone have any suggestions or has had a similar experience with theirs?

 

Thanks

Mark

  • Sign in to reply
  • Cancel
Parents
  • malcolm51
    malcolm51 over 13 years ago

    cheapest multimeters are probably from cpc (part of farnell group) but when you add P&P its probably cheaper, and a lot less frustrating, to get one from maplin or the like if you have one near you..... me, I;m lucky as cpc is my local store (preston, lancs)

     

    as for cables.......... NEVER trust that they're ok (they usually are)... I always remember a delivery of 100 screened audio cables.. they buzzed like hell and turned out to be standard (unscreened) cables.

    on complaining, they checked stock and found out they had several thousand like it...... its not common but it does happen.

     

    I agree with the general comments.... check all voltages first.... the board is designed for learning about systems... you ought to be able to take multimeter readings.. BUT more importantly... It OUGHT to work FIRST time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to malcolm51

    I really like coder27's suggestion that a  multimeter would make an interesting addition to an RPi bundle.  Or alternatively, if not bundled then a very cheap multimeter could at least be listed on the RPi accessories page.

     

    This isn't really in answer to Mark's RPi not booting of course, since booting should be verified on every single unit at the factory and must be expected to work, along with most other testable functionality.  It's more to do with the fact that I consider a multimeter to be a highly valuable educational instrument, and given that the Pi is a bare board and not cased, to some extent every Pi purchaser is "messing with hardware".  Even if the only thing that they are doing is to plug in connectors, the Pi has exposed power and signal lines and there's no getting away from that.

     

    I know that I'm soapboxing this subject a bit, but I really feel that anyone buying an uncased Pi should do themselves an educational favour and buy a multimeter too if they don't have one already. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to malcolm51

    I really like coder27's suggestion that a  multimeter would make an interesting addition to an RPi bundle.  Or alternatively, if not bundled then a very cheap multimeter could at least be listed on the RPi accessories page.

     

    This isn't really in answer to Mark's RPi not booting of course, since booting should be verified on every single unit at the factory and must be expected to work, along with most other testable functionality.  It's more to do with the fact that I consider a multimeter to be a highly valuable educational instrument, and given that the Pi is a bare board and not cased, to some extent every Pi purchaser is "messing with hardware".  Even if the only thing that they are doing is to plug in connectors, the Pi has exposed power and signal lines and there's no getting away from that.

     

    I know that I'm soapboxing this subject a bit, but I really feel that anyone buying an uncased Pi should do themselves an educational favour and buy a multimeter too if they don't have one already. image

     

    Morgaine.