Raspberry Pi Forum USB and LAN ports not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 678 subscribers
  • Views 5913 views
  • Users 0 members are here
Related

USB and LAN ports not working

Former Member
Former Member over 13 years ago

I received my Raspberry Pi today, but unfortunately neither the USB ports or the LAN port appear to be working.

 

I have tried numerous low power USB devices like keyboards mice etc. but can't get any life out of them, although I am able to charge my phone from the ports. Same results using two different 2A adapters to power the Pi and with a powered USB hub.Tried connecting the LAN port but the light on the router indicating a device is attached did not come on.

 

I've tried Debian, Arch and Fedora from RaspberrPi.org and also tried the kernel update which I believe is to address a different issue with USB. At this stage I'm fairly sure there is a fault (LAN is connected through USB I believe?). I'll wait and see if anyone else reports similar problems, otherwise I think I'll have to return it.

 

Does anyone have any suggestions or has had a similar experience with theirs?

 

Thanks

Mark

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    Ok so I bought a multimeter today and have now tested 7 different power sources and all were within the tolerated range throughout booting. Only one came close to the lower limit, weighing in at 4.79 Volts, and the rest were between 4.85V and 5.09V.

     

    Having a USB keyboard attached to the lower port made no difference to the readings.

     

    All were tested with the same cable. If I get sufficiently bored later I'll try all the cables I can find to try and identify any poor performers.

     

    I'm fairly sure my SD card and images are ok because I've tried two different cards and 4 images - all with the same results. Indeed, as I type this, XBMC is staring at me from the Pi, taunting me!

     

    I appreciate the help and ideas you have all offered, but I must have reached a stage where you won't begrudge me sending it back for replacement now, right? image

     

    I'll probably spend the evening prodding various things with my new multimeter so at least something good has come of this!

     

    Thanks everyone!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    7 different power sources, wow. I think you have comprehensively ruled out a power issue! At this point my guess is a broken trace, cold solder joint, damaged part or other hardware issue somewhere in the vicinity of the LAN9512 Eth/USB chip (IC3) which prevents it from seeing your devices. Supposedly all devices get a functional test at the factory. If so, this would have to be something that happened in shipping; hairline fractures, cold solder etc. can behave that way, and be very difficult to see by visual inspection.  Anyway I'd agree; sounds like it should be returned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    7 different power sources, wow. I think you have comprehensively ruled out a power issue! At this point my guess is a broken trace, cold solder joint, damaged part or other hardware issue somewhere in the vicinity of the LAN9512 Eth/USB chip (IC3) which prevents it from seeing your devices. Supposedly all devices get a functional test at the factory. If so, this would have to be something that happened in shipping; hairline fractures, cold solder etc. can behave that way, and be very difficult to see by visual inspection.  Anyway I'd agree; sounds like it should be returned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to Former Member

    'Sure hope that the boards which had their RJ45 replaced manually went back into full test.  Manual rework is quite likely to have a higher fault rate than the robotic production line.

     

    And it's not just the networking that needs to be tested after the correction, because rework can damage other parts that were fine before.