I received my Raspberry Pi today, but unfortunately neither the USB ports or the LAN port appear to be working.
I have tried numerous low power USB devices like keyboards mice etc. but can't get any life out of them, although I am able to charge my phone from the ports. Same results using two different 2A adapters to power the Pi and with a powered USB hub.Tried connecting the LAN port but the light on the router indicating a device is attached did not come on.
I've tried Debian, Arch and Fedora from RaspberrPi.org and also tried the kernel update which I believe is to address a different issue with USB. At this stage I'm fairly sure there is a fault (LAN is connected through USB I believe?). I'll wait and see if anyone else reports similar problems, otherwise I think I'll have to return it.
Does anyone have any suggestions or has had a similar experience with theirs?
Thanks
Mark