Raspberry Pi Forum USB and LAN ports not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 678 subscribers
  • Views 5910 views
  • Users 0 members are here
Related

USB and LAN ports not working

Former Member
Former Member over 13 years ago

I received my Raspberry Pi today, but unfortunately neither the USB ports or the LAN port appear to be working.

 

I have tried numerous low power USB devices like keyboards mice etc. but can't get any life out of them, although I am able to charge my phone from the ports. Same results using two different 2A adapters to power the Pi and with a powered USB hub.Tried connecting the LAN port but the light on the router indicating a device is attached did not come on.

 

I've tried Debian, Arch and Fedora from RaspberrPi.org and also tried the kernel update which I believe is to address a different issue with USB. At this stage I'm fairly sure there is a fault (LAN is connected through USB I believe?). I'll wait and see if anyone else reports similar problems, otherwise I think I'll have to return it.

 

Does anyone have any suggestions or has had a similar experience with theirs?

 

Thanks

Mark

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    In this thread:

     

    http://www.raspberrypi.org/forum/troubleshooting/my-pi-has-a-faulty-usb-port

     

    there is confirmation that Farnell has units reserved for replacing fautly units,

    and that they will not only replace the unit promptly but will arrange for the

    faulty unit to be picked up.   On the other hand, a customer from RS reportedly

    had to pay to have his unit returned, although reportedly the return shipping costs

    are reimbursable.

     

    There seems to be mounting evidence that the USB ports are not adequately

    tested before delivery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago

    In this thread:

     

    http://www.raspberrypi.org/forum/troubleshooting/my-pi-has-a-faulty-usb-port

     

    there is confirmation that Farnell has units reserved for replacing fautly units,

    and that they will not only replace the unit promptly but will arrange for the

    faulty unit to be picked up.   On the other hand, a customer from RS reportedly

    had to pay to have his unit returned, although reportedly the return shipping costs

    are reimbursable.

     

    There seems to be mounting evidence that the USB ports are not adequately

    tested before delivery.