Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Battery-powered Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 708 subscribers
  • Views 5119 views
  • Users 0 members are here
  • help
  • power-supply
  • raspberry_pi
Related

Battery-powered Pi?

mgt6910
mgt6910 over 14 years ago

I would like to use my Pi on a robotic platform, for which an onboard power supply will be

necessary. I  have a rechargeable 6-volt battery. How can I regulate this down to 5V ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    What are the RPi current requirements? How much current can it draw at 100%CPU?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The numbers I've seen from someone actually measuring current draw was 550 mA, but the official spec is 700 mA. I think this may not include power drawn by USB devices connected to the Pi's two USB ports.  The Pi has three linear regulators on board (check RG1, RG2, RG3 on the schematic), so you can guess it wasn't designed for the highest efficiency. The CPU core voltage is generated by a switcher integrated on the SoC, though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The numbers I've seen from someone actually measuring current draw was 550 mA, but the official spec is 700 mA. I think this may not include power drawn by USB devices connected to the Pi's two USB ports.  The Pi has three linear regulators on board (check RG1, RG2, RG3 on the schematic), so you can guess it wasn't designed for the highest efficiency. The CPU core voltage is generated by a switcher integrated on the SoC, though.