Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Version of RPi with VGA output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 707 subscribers
  • Views 1293 views
  • Users 0 members are here
  • vga
Related

Version of RPi with VGA output

e14 Contributor
e14 Contributor over 14 years ago

I'd really like a version of the Pi with VGA output.  I would be willing to pay more for it.  I understand this would not be trivial to do but I only have monitors with VGA inputs.  Even though the FAQ describes VGA as "end of life" it is still ubiquitous.  The alternative for me would be to buy a new monitor or an astronomically expensive adaptor box.  For a low price board this rather seems to defeat one of the objectives of the Pi completely.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    MarkW,

       My understanding is that the chipset on the RPi doesn't support VGA. Adding ports or components that aren't supported natively by the chipset would normally mean a redesign and would increase the costs.

       I think a composite to VGA adapter would be a cheaper option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    MarkW,

       My understanding is that the chipset on the RPi doesn't support VGA. Adding ports or components that aren't supported natively by the chipset would normally mean a redesign and would increase the costs.

       I think a composite to VGA adapter would be a cheaper option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I realize that adding such support would increase the costs hence my comment in the original post "I would be willing to pay more".  I believe I read that adding such support would double the cost of the Pi, but that would be considerably cheaper than buying an adaptor or new monitor. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    The common desire to use a single board layout common to multiple versions of a product really only makes sense when volumes are low.  When volumes are high, the reduced costs that can be obtained by tailoring PCBs to the exact functionality required become the more important factor since it makes the product more profitable.

     

    In the case of Pi, the overall numbers are already pretty big even when selling merely to enthusiasts, and truly astronomic if the plans to get Pi into education come to fruition worldwide.  That means that making special versions of the boards becomes very worthwhile to consider.

     

    I have no doubt at all that there are sufficient numbers of people who would be interested in a non-HDMI board to warrant creating non-HDMI board releases.  For a start, composite video is really quite incongruous in 2012 as a computer display for the developed world, so drop the on-board composite circruitry and connector and make a pure HDMI release.  However, composite video is considered highly important even today in the underdeveloped world, so making a version featuring composite but no HDMI would make sense and would allow prices to drop even further.

     

    The same applies to the proposal here that VGA should be provided.  I expect that there are still so many VGA displays in the world that this would be a very popular option.  Drop composite and HDMI for a VGA model.

     

    And finally, and most important of all, a very significant proportion of Pi users have server applications in mind and do not need display electronics at all.  Just serial console and ssh is quite enough for this segment of Pi users.  There definitely should be a low-cost version of Pi released with Ethernet but without graphics output hardware.

     

    The latter version should of course be called Model N, standard nomenclature in the industry. image

     

    The cost saving in each of these categories could be substantial.  High volume really changes the game.

     

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    Following the above suggested theme:

     

    • Model A - Legacy name, aka. Model CH
    • Model B - Legacy name, aka. Model CHN

    ----

    • Model C - Composite video only
    • Model H - HDMI output only
    • Model N - Networking only, no graphics output
    • Model V - VGA  output only

     

    image

     

    Morgaine.