Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Lost my place in line due to Elements incompetence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 709 subscribers
  • Views 2361 views
  • Users 0 members are here
  • raspberry_pi
Related

Lost my place in line due to Elements incompetence

e14 Contributor
e14 Contributor over 14 years ago

I am going to give my story mostly because I am angry...

I placed an order for a Pi on March 1.  In the time since my credit card had to be canceled due to illicit activity.  Apparently Element has no way to change this information and the only solution they have for me is to cancel my original order and place a new order.  This obviously makes me lose my place in line.

The moral of this story is don’t let anyone hack your credit card until they ship your Pi otherwise you lose your place in line. My Pi was supposed to ship tomorrow now it says November.  This is unbelievably disappointing.

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    Your story raises a related issue.

     

    Credit cards are issued with expiry dates no more than 3-4 years in the future --- let's call it 5 years to be generous, which makes the average remaining life of a given credit card 2.5 years.  The bulk of initial Pi orders will be filled by the end of June we have been informed, which is 4 months from the launch date on 29th February.

     

    4 months is 13.333...% of 2.5 years, which means that up to 13% of all credit cards used for preordering Pi will have expired during the wait for preorders.

     

    If Element 14 has no way to change your credit card number without you losing your place in the queue, then this will also apply to up to 13% of credit card orders owing to card expiry during the interval.

     

    If this is true, there are going to be a lot of unhappy customers.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    According to this Element 14 discussion, if your credit card expires Newark will contact you and give you a chance to update your information.  I hope this works, as I am in this situation.  Given that I never got the e-mail to tell me about updated ship dates, I'm a tad dubious that I'll get the credit card e-mail.  It's really silly that you can't update credit card information at newark.com.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    @John: That "change card number when our attempt to charge fails" approach ought to cover m m's problem too then.

     

    This brings to mind what I wrote recently about my career experience with dev teams in industry ... let's just say, the situation is somewhat less than perfect. image

     

    I should temper that though with my equally common observation that very clever and insightful tech teams often cannot implement sensible and (to them) obvious designs because the requirements imposed by management lie somewhere in the range between not sensible to downright surreal.  Dilbert's PHB is alive and well in industry.

     

    I guess we'll never know whether it's a failure of developers or of management.  Ultimately though, it doesn't matter.  It's a company as a whole that suffers when things go wrong, so everyone is to blame.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    My only question is why they the distribution is so slow, i mean a lot of poeples want a pi but cannot buy one, they can make millions of tablets in month, but pi barelly 10k... i mean everyone want one, make production go faster and sell more, i ordered mine  monday, i hhope to not wait 5-6 months its ridiculous, i will receive mine when a new PI will be available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    @Sylvain:  Yes, that is odd, isn't it.

     

    It's not like any of the components is rare or anything (with the possible exception of the Broadcom SoC), so why not ramp up production by a lot more?  After all, demand is utterly guaranteed so there is zero risk associated with the manufacturing investment, particularly given the educational goals of the Foundation which take the numbers into astronomical territory.

     

    And to make matters even more ridiculous, if they manufactured in greater quantities then their BOM costs would drop still further and so they would make even more profit!  What is there not to like?

     

    It's very curious.

     

    I see only two possibilities that have any chance of explaining it:

     

    1. RS+Farnell are frightened or cautious of high volume manufacturing, because traditionally they have been only distributors, and although they do engage in bespoke manufacturing, it has always been on relatively small scales to satisfy the low volume demand from engineers.
    2. Broadcom does not have sufficient manufacturing capacity for the SoC to allow high volume production.

     

    Any other possible reasons?

     

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I think they need to balance demand and inventory. They want to get them in peoples hands quickly, but if they ramp up production too much, they may find themselves stuck with tons of units they can't sell. If the RPi turns out to be a dud or a newer model comes out, look for people to quickly abandon the current model. I'm sure people would continue to buy the old model, but they'd have to be sold at a loss just to clear inventory. These aren't exactly iPhones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I think they need to balance demand and inventory. They want to get them in peoples hands quickly, but if they ramp up production too much, they may find themselves stuck with tons of units they can't sell. If the RPi turns out to be a dud or a newer model comes out, look for people to quickly abandon the current model. I'm sure people would continue to buy the old model, but they'd have to be sold at a loss just to clear inventory. These aren't exactly iPhones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Steve Jacobs wrote:

     

    if they ramp up production too much, they may find themselves stuck with tons of units they can't sell. If the RPi turns out to be a dud or a newer model comes out, look for people to quickly abandon the current model.

     

    Hahaha, good joke. image

     

    Also, you're forgetting that they have a monopoly.  Nobody can come out with a newer model to make their old one obsolete, other than they themselves.  Therefore they would not do so until current stocks are dwindling.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    @Morgaine

    Or something like this could come out: http://www.reghardware.com/2012/05/22/chip_maker_via_outs_49_dollar_raspberry_pi_alike/ and people would lose interest in the RPi. I just think they don't want to open the flood gates if they'd get stuck with a bunch of product they can't sell.