Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Accessories and Power Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 707 subscribers
  • Views 2398 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi Accessories and Power Questions

e14 Contributor
e14 Contributor over 14 years ago

Just got my order confirmation today and UPS shipping says it will be here on Thursday. Leaves me only two days to get everything I need so I'm looking to buy everything as soon as possible. However Im concerned about the power these things can handle and what kind of power supply to use. I read something about 700 mA but I'm not as tech savvy in electronics as some people. I have extra micro USB chargers for my Droid 2 phone as well as the ones all of my family has. Are these capable of the 700 mA needed? Or do I need a larger/smaller power supply in order to properly run the RPi without having shortages or overloading the board? I haven't checked but my TV might even have a USB port would that be good enough?

 

Which leads me to my next question about the accessories. I plan on adding a wireless USB mouse/keyboard combo as well as USB wifi dongle, and maybe a portable external hard drive but at bare minimum an 8 gb flash drive. Definitely going to buy a USB hub to accomodate the need for more USB ports but I don't want to overload the RPi and break the thing.

 

Any help would be greatly appreciated and feel free to post links to some of the accessories you got for your RPi. Interested to see what kind of mouse/keyboard combos and wireless adapters you guys went with.

  • Sign in to reply
  • Cancel
Parents
  • bodgy
    bodgy over 14 years ago

    Most charger power packs state the current capacity either on a silver label near the power point plugs or by the DC power lead. Sometimes it is just imprinted in the plastic case itself so hard to see, but if it is there, it will normally have a symbol showing th epolarity of the CD connector and for example 5v @ 1A.

     

     

    Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to bodgy

    Thanks for the replies many of my concerns have been put to rest. You guys are mainly in the UK (I'm in the US) but I'm assuming the power ratings are all the same. Only thing I have a question about now is I have an HTC charger that works for all Droid phones and it gives the power rating on the back..

     

    Input: 100-240V ~ 200 mA 50-60Hz

    Output: 5V--1A

     

    Does the input have to be 700 mA or just the output has to be 5V -- 1A? Hopefully the one I have works. If not theres another one lying around somewhere that I gotta go find to check if that will work.

     

    I'm definitely going to get a powered USB hub though so I can plug in the stuff I want without coming across any power issues. Will post the parts I decide to go with when I make the orders.

     

    Edit: Found three more (family has a bunch of battery chargers with USB ports), two are rated at 5V- 800MA and the third is just a non battery charging Verizon Wireless one with these specs

     

    Input: 100V-240V ~ 0.2A 50/60Hz

    Output: 5.0V - 1000mA

     

    Going over the 700 mA isn't a bad thing right? The Pi will only take what it needs I'm assuming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to bodgy

    Thanks for the replies many of my concerns have been put to rest. You guys are mainly in the UK (I'm in the US) but I'm assuming the power ratings are all the same. Only thing I have a question about now is I have an HTC charger that works for all Droid phones and it gives the power rating on the back..

     

    Input: 100-240V ~ 200 mA 50-60Hz

    Output: 5V--1A

     

    Does the input have to be 700 mA or just the output has to be 5V -- 1A? Hopefully the one I have works. If not theres another one lying around somewhere that I gotta go find to check if that will work.

     

    I'm definitely going to get a powered USB hub though so I can plug in the stuff I want without coming across any power issues. Will post the parts I decide to go with when I make the orders.

     

    Edit: Found three more (family has a bunch of battery chargers with USB ports), two are rated at 5V- 800MA and the third is just a non battery charging Verizon Wireless one with these specs

     

    Input: 100V-240V ~ 0.2A 50/60Hz

    Output: 5.0V - 1000mA

     

    Going over the 700 mA isn't a bad thing right? The Pi will only take what it needs I'm assuming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Its the output that needs to be above 700mA at 5v so that is fine.

    I use the HTC adapter rated at 1000mA 5V and its giving me no problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Sounds good thank you for the quick replies.

     

    Ordered these things...

     

    http://www.newegg.com/Product/Product.aspx?Item=N82E16823219009

     

    http://www.ebay.com/itm/802-11n-802-11g-802-11b-USB-Mini-Wireless-Adapter-WiFi-Network-WLAN-card-150Mbps-/400297035447?pt=US_USB_Wi_Fi_Adapters_Dongles&hash=item5d339006b7#ht_2153wt_1325

     

    http://www.newegg.com/Product/Product.aspx?Item=N82E16820208293

     

     

    Thinking about this but do I really need a powered one if I'm only going to be plugging in one nano USB adapater wireless keyboard/mouse, 8 gb flash drive, and the nano wifi adapter to connect to my network?

     

    http://www.newegg.com/Product/Product.aspx?Item=N82E16817111976

     

    Seems like I'm just wasting money if I buy that when I can just get a USB powered one for cheap. My current external hard drive has the power adapter so I'm not really worried about overloading it that way unless I get a new portable drive later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    These are the accessories I am using and any issues I am having with them:

     

    Keyboard/Mouse - occasionally I have to uplug the dongle and re-insert it for the mouse to work properly

     

    HDMI Cable - Had to add the line 'config_hdmi_boost=5' to 'config.txt' to give clear picture as its a longish lead

     

    HDMI - DVI Adapter - No Issues

     

    Wifi Adapter - Have got the drivers installed but cannot make it connect to router yet, simply hangs waiting to connect.

     

    Havent tried it with external USB hard drive as yet but dont think there would be any issues there.

    I would ALWAYS go for a powered USB hub on the Raspberry Pi as the devices you are likely to plug into it will more than

    likely overload the PSU you are using, so using a powered hub would remove this issue.

     

    Message was edited by: Mr P from his Ras-Pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Got it set up..sorta. I'm having an issue trying to login, I'm using the recommended Debian Squeeze with username: pi and password: raspberry but it won't accept any input for the password. I can put in the username "pi" but it won't let me type anything in the password section. I tried looking around the forums for the problem but I can't seem to find this answer unless it's adding a line to the command, which idk how to do anyway so if that's the case can anyone help me out here? Thanks.

     

    Edit : Nvm password is invisible...

     

    Got it running and all was browsing the internet for a while...kinda slow in my opinion. Even though it was connected with ethernet rather than USB dongle. I think I'd attribute the slowness to the SD card I was using which is an old old card, most likely with slow transfer rates compared to the SD cards nowadays. Waiting til I get the rest of my parts including new SD card but not bad for playing with it for only a couple hours.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Mr P have you gotten the wireless adapter working yet? What steps did you take to get the drivers installed? I figure we have very similar wireless adapters so the methods should be the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Andrew,

     

    i followed the instructions in this post, i have the RTL8188 chipset on my wireless thingy but unfortunately i cannot make it work yet..........

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=6256

     

    hope you have more success than me image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pjc123
    pjc123 over 14 years ago in reply to e14 Contributor

    To Andrew Morey:

     

    I am also in the US and was looking at the same hub you purchased when I came across this thread; the hub has good reviews and is cheap. Does it work properly with the raspberry Pi, in particular with the wifi and keyboard/mouse both attached to the hub, because that is my plan as well? That combination seems to be a problem for a lot of people.

     

    My other parts are different. I have a Microsoft Desktop 3000 wireless setup that someone gave me last year. I have a TP-Link TL-WN722N wifi adapter (really like it) and plan on ordering a Medialink MWN-USB150N adapter as well; I plan on testing each with the pi (Although the TL-WN722N) is already listed on the wiki as a working model and the Medialink appears to have the same chipset as another tested wifi device. One wifi dongel will go on my desktop and the other one on the pi. I am also leaning towards a Transcend card as well, maybe a class 8gb or 16gb class10 as I see others have successfully used these.

     

    My pi arrived yesterday, but I will probably wait until I get a case before I hook it up. My years of working as an engineer with electronics in production lines just won't allow me to lay the circuit board on a table.  I am thinking about the modmypi case which I really like, but I would not see it until the end of June.

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to pjc123

    I never actually purchased it, I thought about it but in my original post I mentioned that I was thinking about buying that USB hub. But I figured I was using a single USB to power the wireless keyboard and mouse, and the other onboard USB from the Pi would be used for the Wifi dongle. I know that there may be a limitation to the Pi's power especially when trying to connect the USB wifi adapter over a distance. But the USB hub may come at a later date when I've got the Pi working and demand more from it.

     

    Mr P I'm sad to see you've given up on the RTL8188 based adapter, I haven't gotten around to working on it yet I've been busy the past few days. Glad your other adapter works nicely though. How are the internet speeds over wireless?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I've had no ends of problems with Realtek based wifi adapters. Every time i get the realtekfirmware loaded I get continuous series of NYET/NACK/ACK (or something like it) debug message that cripple the Pi. This only happens when the firmware is loaded.

     

    I've ordered a Netgear wna1100 from eBay as the wiki says it works and it doesn't use Realtek.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Andrew, I havent actually done any speetests as such but it seems very useable, obviously the heavier the page content the less the pi likes to load it quickly.

    also I havent totally given up on the realtek adapter, just needed to get some wireless working as the RPI is sat in a room far away from the router.

     

    All in All for a board and OS thats still being developed I am more than happy with its performance so far.