Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum soldering crystal oscillators
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 708 subscribers
  • Views 2649 views
  • Users 0 members are here
Related

soldering crystal oscillators

e14 Contributor
e14 Contributor over 14 years ago

Several people have found that problems with usb and ethernet

were related to the 25MHz crystal oscillator.  Perhaps this part

isn't always soldered correctly. One important recommendation is

that you "stand on the board while soldering".

 

http://cfm.citizen.co.jp/english/product/cvo_manual.html

see paragraph 1.II.2.

  • Sign in to reply
  • Cancel
Parents
  • YT2095
    YT2095 over 14 years ago

    although I`m not quite familiar with ethernet, I have done a little work with USB, and that likes divisons or multiples of 12Mhz, that are taken care of on chip by either a divider or PLL.

    25MHz seems a strange number to start with (as opposed to a 24MHz for instance), could that be causing the problems?

    or can someone tell me how the 12MHz is derived for the USB please.

     

    Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to YT2095

    YT2095 wrote:

     

    although I`m not quite familiar with ethernet, I have done a little work with USB, and that likes divisons or multiples of 12Mhz, that are taken care of on chip by either a divider or PLL.

    25MHz seems a strange number to start with (as opposed to a 24MHz for instance), could that be causing the problems?

    or can someone tell me how the 12MHz is derived for the USB please.

    25 MHz is what the LAN9512 data sheet specifies for the XI/XO pins.  They probably quadruple this internally to 100 MHz for 100 Mb/s Ethernet.  For USB 2.0 you need 480 Mb/s so they probably need 480 MHz internally.  They probably have a 480 MHz PLL oscillator divided by 96 to get a 5 MHz feedback signal.  This is locked to the 25 MHz crystal reference divided by 5.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Apparently the timebase for 100 Mbps ethernet is actually 125 MHz.

    With 100BASE-TX hardware, the raw bits (4 bits wide clocked at 25 MHz at the MII) go through 4B5B binary encoding to generate a series of 0 and 1 symbols clocked at 125 MHz symbol rate. 

    -from http://en.wikipedia.org/wiki/Fast_Ethernet

    See also: http://www.designspark.com/content/raspberry-pi-waveforms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago in reply to johnbeetem

    Thanks, although I am somewhat confused about your assertion of USB2.0 needing 480 MHz to work?

    I use the PIC 18F4550 with full USB 2.0 capabilities, and that requires 12MHz to run, made by a 20 MHZ crystal, divided by 5, and then taken up to 48MHz for the CPU clock and 12MHz for the USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • YT2095
    YT2095 over 14 years ago in reply to johnbeetem

    Thanks, although I am somewhat confused about your assertion of USB2.0 needing 480 MHz to work?

    I use the PIC 18F4550 with full USB 2.0 capabilities, and that requires 12MHz to run, made by a 20 MHZ crystal, divided by 5, and then taken up to 48MHz for the CPU clock and 12MHz for the USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 14 years ago in reply to YT2095

    YT2095 . wrote:

     

    Thanks, although I am somewhat confused about your assertion of USB2.0 needing 480 MHz to work?

    The LAN9512 supports high-speed USB 2.0, which is 480 Mb/s.  It also supports full speed (12 Mb/s) and low speed (1.5 Mb/s).