Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using an iMac as a display for RaspberryPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 766 views
  • Users 0 members are here
  • display
  • mac
Related

Using an iMac as a display for RaspberryPi

e14 Contributor
e14 Contributor over 14 years ago

I'm starting completely new with RaspberryPi, and I want to use my iMac 10,1 (Intel Core 2 Duo, OS 10.6.8) as a monitor.

I'm using a HDMI cable from the RaspberryPi through two converters into the MiniDisplay Port at the back of the Mac, but I can't see any way of getting the Mac to display the input from the RaspberryPi.

Any ideas on how to do this?

I've tested the RaspberryPi using a TV as a display (it won't log on, that's another issue, but it will boot), so the board is working.

But I can't use the TV for playing with the RaspberryPi since other people want to watch the TV!  I only have the iMac or a Mac Powerbook to use for displays.

So I really need to get it working with the Mac - any ideas?

  • Sign in to reply
  • Cancel
Parents
  • GreenYamo
    GreenYamo over 14 years ago

    Hi there,

     

    I was going to suggest that you post in the RasPi forums, but I can see you have already done that (http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=7378&p=90881&hilit=imac+display#p90881)

     

    Dom is probably the best person to engage on this question, as I believe he is the Broadcom HDMI expert.

     

    I was also going to suggest playing about with the config.txt file, but I can see he has already done that.

     

    Think all I can say is Good luck :-)

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • GreenYamo
    GreenYamo over 14 years ago

    Hi there,

     

    I was going to suggest that you post in the RasPi forums, but I can see you have already done that (http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=7378&p=90881&hilit=imac+display#p90881)

     

    Dom is probably the best person to engage on this question, as I believe he is the Broadcom HDMI expert.

     

    I was also going to suggest playing about with the config.txt file, but I can see he has already done that.

     

    Think all I can say is Good luck :-)

     

    Steve