Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Multi-orders being enabled?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 707 subscribers
  • Views 1631 views
  • Users 0 members are here
  • raspberry_pi
Related

Multi-orders being enabled?

morgaine
morgaine over 14 years ago

One of the interesting snippets of information that we learned from the Maker Faire video that Drew linked here -- http://www.youtube.com/watch?v=WIf4Fk2252A  -- is that Eben expects Element 14 to enable multi-orders for Raspberry Pi on its website this week (he mentions it at around 14:00 minutes into the video).

 

Was that possibility mentioned anywhere else, such as in Element 14 emails or by Jenny on the RPF blog?

 

His comments also made me wonder whether the two partners will continue to be symmetrical in that respect, because he specifically asked the person in the audience who raised the question which distributor they were signed up with.  I can't quite make out the final word in Eben's comment "I can't speak for <someone>", but perhaps that was related too.

 

Anyway, it was a very interesting answer that Eben gave.

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Morgaine,

      Eben says he can't speak for Allied, which is the RS partner in the US.

     

    It's funny he says he hopes Element14 will be able to ship multiple orders

    soon.  In fact, there is already at least one report of Element14 shipping

    two units to the same customer, user SN:

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=23&t=6400

     

    and quite a few reports of people receiving one each from Element14 & RS.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    In the same video, at about 17:35, Eben talks about PCB-level

    changes being made to achieve FCC Class B certification.

    He says it's pretty important not to ship millions into schools

    without such certification.  I would expect he similarly wouldn't

    want to ramp production for multiple-unit orders before Class B

    was obtained.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Had we heard of Pi needing PCB-level changes for FCC Class B certification before this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

    > Had we heard of Pi needing PCB-level changes for FCC Class B certification before this?

     

    liz on April 10, 2012 at 7:04 pm

    said in page 3 of the comments to this article:

    http://www.raspberrypi.org/archives/978

     

    "Happily, we’ve found it doesn’t need a shielded enclosure to reach Class B,

    although it will require a (very minimal) redesign."

     

    JamesH on April 10, 2012 at 9:49 pm said:

     

    "I don’t know yet, but I had assumed that meant a PCB redesign.

    There isn’t much else that could be redesigned – it doesn’t come

    with a power lead for example!"

     

    As far as I know, Eben's video is the first official confirmation that

    the "redesign" Liz mentions involves a PCB change.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Interesting.  Well now's the time to make changes, as early as possible, and certainly before an educational release.  I just cannot understand all the secrecy though.  They have a serious problem in that area.

     

    And while they're at it redesigning the PCB, the polyfuses need to be revisited, at the very least their trip currents raised so that their highly detrimental effect on voltage regulation is reduced.  Far better though would be to take the input to F1 and F2 from upstream of F3 so that they are no longer interdependent.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to morgaine

    I don't know if it is related, but having got a second Pi it seems a lot more stable than the first.

     

    The first one I got (from the missing 8,000 (tm)) won't re-boot if it has been used for a while, I need to pull power for around 10 minutes or so before it is happy.

     

    Second Pi from RS, with *exactly* the same things plugged into it will re-boot quite happily after pulling the power for 20-30 seconds or so.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to GreenYamo

    Steve,

      There is a related thread here:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=6957

     

    including someone who says they have removed the monitor and

    all usb devices, so that rules out quite a bit.  They suggest

    possibly related to the SD card. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    That's what I thought originally (SD Card) but with my second Pi I am using everything the same, including the SD card so the only change is the Pi itself.

     

    I'm thinking of using it as my 'interfacing' Pi, so when I (inevitably) blow it up accidentally, it will have given it's life for a noble cause.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    That's what I thought originally (SD Card) but with my second Pi I am using everything the same, including the SD card so the only change is the Pi itself.

     

    I'm thinking of using it as my 'interfacing' Pi, so when I (inevitably) blow it up accidentally, it will have given it's life for a noble cause.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to GreenYamo

    Steve,

      It would be interesting to find out if element14 considers this normal behavior,

    or if they consider it grounds for a replacement.

     

    Similarly, I'd be interested to find out if they consider SoC and/or lan chips that

    are hot to the touch normal behavior.  I believe Liz and Gert have said the chips

    are supposed to be "warm", about body temperature, but not so hot that you

    can't touch them for more than about 5 seconds as some have reported.

     

    I'd also be interested to find out what the normal resistance is supposed to be

    for the polyfuses.  I believe it has been said that they should be in the milliOhms,

    but several people have reported 5, 6, and 7 Ohms for F1 and F2.