Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can GPIO pins generate interrupts?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 708 subscribers
  • Views 7308 views
  • Users 0 members are here
  • raspberry_pi
Related

Can GPIO pins generate interrupts?

jrychter
jrychter over 14 years ago

I looked at the example code for doing I/O using the GPIO pins, but — I need to be able to count impulses (between 0.01 and 250Hz), which isn't really doable with GPIO polling on a multitasking OS.

 

Are the GPIO pins capable of generating interrupts?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Yes they can generate interrupts, and just yesterday some example code was posted. Note, I do not know whether 250 Hz pulses (4 msec interval) will always be reliable, depending on what other operations the R-Pi is doing (SD card I/O, USB and Ethernet, etc.) although you may be able to change interrupt priority if needed.

     

    Support for GPIO-driven interrupts

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=44&t=7509

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jrychter
    jrychter over 14 years ago in reply to e14 Contributor

    Thanks for the link!

     

    I thought about it some more, and then remembered that this is Linux, where you deal with interrupts in kernel space, possibly creating an interface to user-space.

     

    I think for the moment it is actually simpler for me to use a MSP430-based Launchpad board to do the counting and interface it via SPI to the Raspberry.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to jrychter

    I was doing some experiments last night with a 555 timer set for around 1500 Hz connected to a GPIO on the pi, and a modification of the irq demo program linked from this page:

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=44&t=7509

     

    I used gettimeofday to time the interval between interrupts, and was getting numbers quite close (within 1% probably) of the frequency based on what I was reading from the frequency counter on my multimeter also attached to that input. CPU utilization was around 6-7%.

     

    --bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to rdolson

    That's a very interesting experiment. The question then is: Why are you getting a 1% difference?

     

    Is the crystal on the RPI inaccurate? Are you missing interrupts? Is the multimeter inaccurate?

     

    If you are just measuring the interval to be about 700 microseconds, and then doing 1/interval and getting 1500+/- 15 each time, you're not missing interrupts. If you count interrupts for a long enough period, maybe 1 day of wallclock or ntp-synced time, then you should be able to calibrate the crystal of the raspberry pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to rew

    The inter-interrupt times wandered around a central value (that wander is what I was estimating as 1%). This was a very sloppy experiment so I don't have any stored data to look back on. My assumption is that there's variation in the latency between the low-level GPIO interrupt and the time at which the userland code is able to take action, since the linux scheduler is involved (and there's a context switch required etc).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rdolson
    rdolson over 13 years ago in reply to rew

    The inter-interrupt times wandered around a central value (that wander is what I was estimating as 1%). This was a very sloppy experiment so I don't have any stored data to look back on. My assumption is that there's variation in the latency between the low-level GPIO interrupt and the time at which the userland code is able to take action, since the linux scheduler is involved (and there's a context switch required etc).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rdolson

    Hi,

     

    Sorry to "break in" to this discussion but I've been trying to get the "gpio-irq-demo" program to work with no success, and it appears that you've got it (or some version of it) working just fine :-).

     

    i fetched the code from here: http://dev.mrkva.eu/rpi/gpio-irq-demo.c

     

    The poll() call always just times out - the program doesn't detect the rising or falling signal edge.  Its probably something silly or obvious, but I've spent a few hours and no luck - can you help?

     

    I'm running on the latest apt-get updated Raspbian Wheezy kernel on a Rev 2 Pi which i understand includes the kernel patch for interrupt support (right?).  I'm using GPIO pin 17 (aka WiringPi pin 0) and have verified that i can read it using the "gpio" utility.  e.g.

     

    $ gpio mode 0 in

    $ gpio read 0 # returns the correct 0 or 1 if pin is at ground or Vcc

     

    # now pull the pin to ground

     

    $ gpio edge 0 rising

     

    $ ./gpio-irq-demo 17 # program is using the BCM pin numbers...

    value is 0

    timeout

    timeout

     

    # but when i pull the pin up to Vcc, i don't get the "interrupt, value is: " message

     

    Any idea what is wrong?

     

    thanks for your help!

     

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to e14 Contributor

    Hm, not offhand. However I did do the pin configuration directly using the /sys/class/gpio interface, not through wiring. Something like

     

    echo 17 > /sys/class/gpio/export

    echo rising > /sys/class/gpio/gpio17/edge

     

    I forget if I had to set the pin direction as well, but I suspect it defaults to in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rdolson

    hmmm.  i was getting "permission denied" (even with sudo) trying to use the "echo" commands with /sys/class/gpio so opted for the gpio route.  I think I saw some discussions somewhere about how to work around this, but can you let me know what you did?

     

    It would also be really appreciated if you could send me your interrupt code - I'm new to this site, not sure how that is done...

     

    thx

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to e14 Contributor

    You do need to run the commands as root ("sudo bash" will get you a root shell). My code is sitting on my pi which is powered off on my workbench - will put a copy up when I have it online next.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rdolson

    Eueka!  "sudo bash" did the trick - thanks.  Next step is to use threads so my main program can continue to run.  I will have to handle multiple inputs - I need to count pulses coming in on several GPIO pins.  I think i saw some example code (wfi.c) that does this, but I couldn't get it to work - probably for the same reason that I couldn't get gpio-irq-demo.c to work.  Good news is that the frequency i need to handle is really low - not more than a few pulses per second.

     

    If you have any example code that you think might help, let me know...

     

    My application, by the way, is an aquarium control system - I will be building sensors that will allow me to count CO2 bubbles (for a CO2 injector) and water drips (for a Nitrate filter), read Ph and ORP sensors, and control some valves to maintain specific levels.

     

    Thanks again for your assistance. 

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to e14 Contributor

    This sounds like a classic event driven application (you have events coming in triggered by interrupts from your bubble/drip sensors, and presumably from one or more timers that drive periodic checks and maintenance that will turn valves on and off).

     

    If I was writing this software for myself I'd probably not write it in C but rather use something like perl and the timer / event libraries that are available for it. I'm sure there are such event libraries for any of the scripting languages. The advantage of doing it with one of these languages is that the volume of code will be much smaller and the logic will be easier to represent. With the rates you are talking about performance will not be a problem at all.

     

    --bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rdolson

    Hi Bob,

     

    you are almost certainly correct, but being an old C programmer with minimal Perl expertise, I'm just more comfortable with that language. Something about an old dog and new tricks?

     

    Meanwhile, I've made good progress in C - i am able to read a temperature sensor (varistor) via an adc on the I2C bus, handle a pulse counter using edge-triggered interrupts and poll(), read an ORP probe via the Pi's serial port, and turn off/on some relays.  Next step is to start using threads to take the pulse counter out of the main program loop, put the whole thing together, and actually hook it up to the tank...

     

    regards

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to e14 Contributor

    Very cool ... if you're an old C hand I retract my suggestion :-)

     

    Being a conservative sort I'd still bag the threads and make the application event driven though, since you can set up timers to be triggered and hang the whole program around a loop around the poll() call.

     

    -bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rdolson

    Not sure I'm following your suggestion... My idea is to create a thread that does the poll(), ie is event-driven and wakes up with activity on the pin to increment a counter.  Thus the main program thread can handle the main control loop.

     

    the gpio input is set up for edge-triggered interrupts.

     

    Once i finish it (in a few days i hope, and assuming it actually works :-)) should I post my code here so you can review and clarify/make suggestions?

     

    Thx

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdolson
    rdolson over 13 years ago in reply to e14 Contributor

    What would your main program be doing while waiting for events from the thread? If it's only acting on external events, or on timeouts ("if no bubbles in 3 minutes do something"), you don't need a separate thread and the associated synchonization - you can use the poll mechanism to set up the timeouts.

     

    I'd be happy to take a look at the code.