Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Start up problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 633 views
  • Users 0 members are here
Related

Start up problem

e14 Contributor
e14 Contributor over 14 years ago

Just started - or trying to - with RPi B version.  Followed up the getting started and connected an HDMI cable to a TV (tested AOK from a working HDMI source), New USB keyboard - tested on another PC and is AoK, and a suitable micro USB mains power source - in one case a Sony EP800 +5V 850mA charger and a Kindle charger of the same rated capacity (this one is on the OK list.).  No video.  Red LED for power but NO Green LED status LED.  +4.94V DC across TP1 and TP2.

 

8GB SDHC ScanDisk card in the card slot ready for formatting.  Doesn't alter the conditions whether card in place or not.  Is my RPi faulty or am I missing something?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Thank you for your quick and comprehensive reply.  In the RPi "Getting Started Guide", Page 4, para 1.3 it does state that the RPi requires an SD card preloaded with a version of the Linux OS.  Then it immediately states that you can create your own preloaded card using a suitable SD or SDHC card and on pages 6 to 13 describes very clearly how to do this once a serial connection is established to the RPi.

    I didn't see the green LED flash, so really didn't twig that there was no inbuilt message(s) in the boot code.  I was leaning to the view that you have outlined in your reply but very nice to get it confirmed.  The really useful bit is the link to the RPi_Easy_SD_Card_Setup which nicely solves the problem.  Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Thank you for your quick and comprehensive reply.  In the RPi "Getting Started Guide", Page 4, para 1.3 it does state that the RPi requires an SD card preloaded with a version of the Linux OS.  Then it immediately states that you can create your own preloaded card using a suitable SD or SDHC card and on pages 6 to 13 describes very clearly how to do this once a serial connection is established to the RPi.

    I didn't see the green LED flash, so really didn't twig that there was no inbuilt message(s) in the boot code.  I was leaning to the view that you have outlined in your reply but very nice to get it confirmed.  The really useful bit is the link to the RPi_Easy_SD_Card_Setup which nicely solves the problem.  Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Adrian, With a bit of trickery, making an SD card on the rpi itself should be possible. I don't expect wiki-pages to mention that option yet. The thing is: You need  a working raspberry pi for that to get started. So there is a chicken and egg problem....

     

    (And you can mark the thread as "answered", which will probably make John happier, as you'll be awarding him some points for answering your question).