Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Debugging an ARM chip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 682 views
  • Users 0 members are here
  • raspberry_pi
Related

Debugging an ARM chip

e14 Contributor
e14 Contributor over 14 years ago

Matt Saunders from ARM is running a free webinar session on debugging @ http://www.element14.com/community/events/3363?ICID=webinar_featured

 

It's a Cortex M4, not the ARM11 on the Pi but should still be interesting

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    Cortex-M4 is arguably the most powerful microcontroller core in existence today (as opposed to applications processors), and yet it costs very little.  For example, the STM32F4-Discovery board --- http://www.st.com/internet/evalboard/product/252419.jsp is based on a Cortex-M4 and is available from Farnell UK for under 10 pounds -- http://uk.farnell.com/stmicroelectronics/stm32f4discovery/board-eval-stm32f4-discovery/dp/2009276

     

    Raspberry Pi is rather poorly endowed with hardware interfaces, but the STM32F4 is positively brimming with them, as well as having the usual features of a 32-bit ARM and DSP instructions and a hardware floating point unit which takes it far beyond Arduino territory.

     

    As a result, it's really hard to beat the combination of Raspberry Pi doing high-level work and an STM32F4-Discovery board doing low-level realtime work, interfaced together through SPI, I2C, or just plain USB.

     

    So, to anyone interested in hardware interfacing, I strongly recommend attending Matt Saunders' webinar!

     

    Debugging is important even if it's your first day with ARM. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago

    Cortex-M4 is arguably the most powerful microcontroller core in existence today (as opposed to applications processors), and yet it costs very little.  For example, the STM32F4-Discovery board --- http://www.st.com/internet/evalboard/product/252419.jsp is based on a Cortex-M4 and is available from Farnell UK for under 10 pounds -- http://uk.farnell.com/stmicroelectronics/stm32f4discovery/board-eval-stm32f4-discovery/dp/2009276

     

    Raspberry Pi is rather poorly endowed with hardware interfaces, but the STM32F4 is positively brimming with them, as well as having the usual features of a 32-bit ARM and DSP instructions and a hardware floating point unit which takes it far beyond Arduino territory.

     

    As a result, it's really hard to beat the combination of Raspberry Pi doing high-level work and an STM32F4-Discovery board doing low-level realtime work, interfaced together through SPI, I2C, or just plain USB.

     

    So, to anyone interested in hardware interfacing, I strongly recommend attending Matt Saunders' webinar!

     

    Debugging is important even if it's your first day with ARM. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    But I thought the ARM chips were already debugged :-)

     

    Oh, they mean "Debugging an ARM-based Design".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    Hehe.

     

    Pity that the webinar is going to be based on the  MCBSTM32F400 board and ULINK-ME debugger, which together cost over 200 quid --- http://uk.farnell.com/arm/mcbstm32f400ume/starter-kit-cortex-m4-stm32f407ig/dp/2100029?in_merch=New%20Products

     

    There's no need for that kind of expenditure.  The STM32F4-Discovery board has its own ST-LinkV2 debug adapter built in (there are actually two microcontrollers on the board, one running the debugger), which you can use either to debug the onboard STM32F4 or to debug an external STM board.