Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Trouble getting started
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 707 subscribers
  • Views 1428 views
  • Users 0 members are here
Related

Trouble getting started

madmac88
madmac88 over 14 years ago

Hi all,

 

I have followed the Official Getting Started Guide and could not get my RPi to work. Here's what I did:

  • Verified checksum for the Debian for ARM image
  • Used dd to write the Debian for ARM image to 2GB Panasonic SD (class 4) card
  • Connected keyboard, mouse, display via HDMI, Ethernet cable
  • Inserted SD card
  • Connected USB cable to computer main USB port (not hub)
  • Following the instructions, I could only see the red LED lit, but did not see the green LED at all. I saw some posts said that the green LED was supposed to flash quickly, but I never saw it. There was no power to the keyboard or the mouse and nothing showing up on the display.

 

Any suggestion would be greatly appreciated. Does anybody know how I can verify the image being written correctly? Meanwhile I will try another SD card.

 

Thanks!

 

Bob

  • Sign in to reply
  • Cancel
Parents
  • madmac88
    madmac88 over 14 years ago

    Never mind. I re-imaged and everything A-OK!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to madmac88

    Bob,

       Did you do anything differently when you re-imaged that would explain

    why it worked the second time?  Maybe a different SD card?  or a different

    card reader?   Quite a few people have reported similar symptoms, and

    it would be nice to know what to suggest to them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to madmac88

    Bob,

       Did you do anything differently when you re-imaged that would explain

    why it worked the second time?  Maybe a different SD card?  or a different

    card reader?   Quite a few people have reported similar symptoms, and

    it would be nice to know what to suggest to them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • madmac88
    madmac88 over 14 years ago in reply to e14 Contributor

    I was in Mac OS when I dd it the first time. When I re-imaged, I did from Windows 7 with Win32DiskImager. I did have to run Win32DiskImager as admin to get it to work, though, which was not mentioned in the instructions I have read.

     

    After reviewing the http://elinux.org/RPi_Easy_SD_Card_Setup page, I realized the error of my way. I dd it to the wrong raw device. I will have to play with it again tonight.

     

    So that brings me back to my question of how do you verify that you have written the image correctly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to madmac88

    "So that brings me back to my question of how do you verify that you have written the image correctly?"

     

    Good question.  I think you can view the SD card on a PC to see if you have the right number of

    partitions and that they are about the right size.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Shouldn't any decent operating system auto-mount at least the FAT partition?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    My Mac remounts the SD card after "dd"ing the image to it, but I get mixed results as to if the image works. My Pi will boot up to the point of finding the USB keyboard and mouse, but then will not start the Linux init (i.e. it doesn't seem to be seeing anything from the Linux partition of the SD card). Burning it again may or may not solve the problem, and I've installed several images, some of which work.

     

    I'm not sure what can or would make it work more consistently. I wish it would....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Does it say something like "cannot start init", or does it just hang?

     

    In principle, the system should "stop" when it encounters an error situation. The last message would be the error message for the situation. However with modern, bigger systems, sometimes an error at one level becomes a warning at another. For example, the "start the network" script may fail: "no network connected". Which is fine if the raspberry pi is just booting intended to be used standalone. On the other hand, when the root-filesystem is on NFS, that becomes fatal.

     

    So in practise, some more messages may scroll by before the situation runs out of hand and the system cannot continue. So: "cannot start init" may mean just that. The /sbin/init program is missing or corrupt. On the other hand, there might be filesystem corruption mentioned before that, so then THAT would need to be investigated.

     

    The fastest way for the experts to have a look at your log is if you can post a picture of your screen when it stops booting.

     

    How long does the copying of the image to your SD card take?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • madmac88
    madmac88 over 14 years ago in reply to e14 Contributor

    Finally got around to redo the image in Mac OS. I'm a little rusty in Linux and didn't realize that Mac OS is a bit different. I suppose there's a way to calculate the checksum of files and directories, but that's for another day.

     

    Everything went well and here's a quick capture of the volume info, just in case anyone is interested:

     

    [/Downloads/debian6-19-04-2012] root# diskutil info /dev/disk2s1

       Device Identifier:        disk2s1

       Device Node:              /dev/disk2s1

       Part of Whole:            disk2

       Device / Media Name:      Untitled 1

     

       Volume Name:              NO NAME

       Escaped with Unicode:     NO%FF%FE%20%00NAME

     

       Mounted:                  Yes

       Mount Point:              /Volumes/NO NAME

       Escaped with Unicode:     /Volumes/NO%FF%FE%20%00NAME

     

       File System Personality:  MS-DOS FAT32

       Type (Bundle):            msdos

       Name (User Visible):      MS-DOS (FAT32)

     

       Partition Type:           Windows_FAT_32

       OS Can Be Installed:      No

       Media Type:               Generic

       Protocol:                 Secure Digital

       SMART Status:             Not Supported

     

       Total Size:               78.6 MB (78643200 Bytes) (exactly 153600 512-Byte-Blocks)

       Volume Free Space:        48.5 MB (48478208 Bytes) (exactly 94684 512-Byte-Blocks)

       Device Block Size:        512 Bytes

     

       Read-Only Media:          No

       Read-Only Volume:         No

       Ejectable:                Yes

     

       Whole:                    No

       Internal:                 Yes

     

    [/Downloads/debian6-19-04-2012] root# diskutil info /dev/disk2s2

       Device Identifier:        disk2s2

       Device Node:              /dev/disk2s2

       Part of Whole:            disk2

       Device / Media Name:      Untitled 2

     

       Volume Name:              Not applicable (no file system)

     

       Mounted:                  Not applicable (no file system)

     

       File System:              None

     

       Partition Type:           Linux

       OS Can Be Installed:      No

       Media Type:               Generic

       Protocol:                 Secure Digital

       SMART Status:             Not Supported

     

       Total Size:               1.7 GB (1667235840 Bytes) (exactly 3256320 512-Byte-Blocks)

       Volume Free Space:        Not applicable (no file system)

       Device Block Size:        512 Bytes

     

       Read-Only Media:          No

       Read-Only Volume:         Not applicable (no file system)

       Ejectable:                Yes

     

       Whole:                    No

       Internal:                 Yes

     

    [/Downloads/debian6-19-04-2012] root# diskutil info /dev/disk2s3

       Device Identifier:        disk2s3

       Device Node:              /dev/disk2s3

       Part of Whole:            disk2

       Device / Media Name:      Untitled 3

     

       Volume Name:              Not applicable (no file system)

     

       Mounted:                  Not applicable (no file system)

     

       File System:              None

     

       Partition Type:           Linux_Swap

       OS Can Be Installed:      No

       Media Type:               Generic

       Protocol:                 Secure Digital

       SMART Status:             Not Supported

     

       Total Size:               200.3 MB (200278016 Bytes) (exactly 391168 512-Byte-Blocks)

       Volume Free Space:        Not applicable (no file system)

       Device Block Size:        512 Bytes

     

       Read-Only Media:          No

       Read-Only Volume:         Not applicable (no file system)

       Ejectable:                Yes

     

       Whole:                    No

       Internal:                 Yes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • madmac88
    madmac88 over 14 years ago in reply to rew

    You are absolutely correct. That should have been the first warning sign from my first attempt - the SD card does not show up formatted at all! I think it will help some folks out there if there's some notes about simple checks for imaging results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • madmac88
    madmac88 over 14 years ago in reply to e14 Contributor

    Are all the SD cards the same make/capacity? There's a list of compatible cards here: http://elinux.org/RPi_VerifiedPeripherals#SD_cards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    It doesn't produce any error message at all; It just never starts the init after recognizing the usb devices.