Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum no sound from hdmi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 708 subscribers
  • Views 1212 views
  • Users 0 members are here
  • raspberry_pi
Related

no sound from hdmi

cullimore
cullimore over 14 years ago

hi there

 

i cant get sound from my pi though hdmi. how do i enable it??

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    In /boot you have to create a file named config.txt with the following line

    hdmi_drive=2

     

    Before startx you have to run

    sudo modprobe snd_bcm2835

     

    Then it should run.

     

    Found the last tip in http://www.themagpi.com/ ,which is a good read and might become even better ;o)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to e14 Contributor

    thanks, i`ll try that tomorrow.

     

    funny u say that, i was about to read the mag pi, just downloaded

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    If you add a line with "snd_bcm2835" to the  /etc/modules file (which by default contains only "vchiq"), the sound module will get autoloaded on startup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to morgaine

    Thanks all,

     

    What is the name of the file in ect/modules that I am adding?? And what is the full path of etc/modules. I can't find it. Sorry (red faced )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cullimore

    Darren,

      The full path is /etc/modules

    That is, it's the file modules in directory /etc

    note that there is a slash before etc, and that it's etc

    not ect.  It stands for the latin etcetera.

    And you need to use sudo to edit it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to cullimore

    Great, typed in that command before the startx and now it works. Now to find out to do it so it boots with that command each time.

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to cullimore

    When I go to save modules it says permission denied. How do I get it to save with permission? Seem to be having a lot of trouble with this as I am trying to setup a wi fi dongle and it won't let me drop a file in to a directory.

    Do I need to be an administrator ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cullimore

    Darren,

      you get administrator privileges by typing sudo

    before any command that would otherwise fail for

    lack of privileges.  sudo stands for either switch user

    and do, or super user and do, depending on who you ask.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago

    Read my posts on: http://www.element14.com/community/thread/18205?tstart=0 This fixed my problem and might fix yours.

     

    All fixed (audio + resolution)

    Instuctions for others who may be experiencing the same issue with a TV and the Raspberry Pi:

    1. Install a fresh image (optional)

    2. start-up the Raspberry Pi and let it set itself up (normal set-up) - only on first boot

    3. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_drive=2 " [exactly as it is here]

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    4. Restart using the command: " sudo shutdown -r now "

     

    That gets the Raspberry Pi to register the TV as a HDMI device. You now have sound! For different resolution:

    5. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_group=1 " [exactly as it is here]

    Press Enter

    Type : "hdmi_mode=x " where x = corresponding number of resolution mode. See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=5851

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    6. Restart using the command: " sudo shutdown -r now "

     

    Now you have desired resolution and Sound!!!

     

    Happy Raspberry Pi...ing