Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum lxmusic will not play
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 707 subscribers
  • Views 1310 views
  • Users 0 members are here
  • raspberry_pi
Related

lxmusic will not play

jeffbiss
jeffbiss over 14 years ago

Alright, lxmusic is provided on the RPi Debian distro and will not play even after trying sudo apt-get install xmms2-plugin-all, to load codecs I assume, and sudo modprobe snd_bcm2835 prior to entering startx. Can someone provide a nice how-to get it to actually play when the play icon is clicked? It adds mp3 files to the "playlist", but then, well, nothing. I assume that there's something incredibly obvious, or not, that I'm just not getting to not get audio from the audio jack or to get lxmusic to indicate that its playing, such as the play icon changing to the pause icon.

 

Thanks in advance and sorry for my stupidity. I found a few pages that deal with this issue but none solved the no-play problem.

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    Here are a few possible things to check.  You've already loaded the snd_bmc2835 sound module using "modprobe", but better check that it's actually present using "lsmod".  There should be a few sound-related modules showing in the lsmod output (7 on my Pi).

     

    By the way, you might as well add the module name "snd_bmc2835" onto the end of the /etc/modules file too, using your favourite editor.  This will load the module automatically on boot and save you having to modprobe it manually.

     

    If all seems well there, try a clean start or restart of the ALSA system:

     

    • /etc/init.d/alsa-utils start            --- Start ALSA for the first time
    • /etc/init.d/alsa-utils restart         --- Restart the ALSA system

     

    If everything still looks good, then try a simple commandline player, for example mpg123 or my preferred one, moc.  If they're not in the default image (MOC is not) then you'll have to install one with apt-get, eg. "sudo apt-get install moc".  Invoke either of them directly on your .mp3 or .ogg files, for example "mocp foo.mp3".

     

    If there is still no sound then perhaps you're listening to the wrong output, for example the audio might be coming out over HDMI while you're listening on the analogue output, or vice versa.  You can switch between them using amixer:

     

    • amixer cset numid=3 1               --- This routes audio out the analogue port
    • amixer cset numid=3 2               --- This routes audio out the HDMI port

     

    Usually that's all you need to obtain sound, although some find that they also need "hdmi_drive=2" in their /boot/config.txt file if they want audio on HDMI, or "hdmi_drive=1" if their HDMI lead is plugged into a DVI-D input through an adapter.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jeffbiss
    jeffbiss over 14 years ago in reply to morgaine

    Morgaine,

     

    Thanks for that information but it appears that ALSA is not installed. I looked in /etc/init.d and alsa-utils is not there, so now to install ALSA.

     

    Then, and only then will I be able to use your information .

     

    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jeffbiss

    Easy to fix:

     

    • sudo apt-get install alsa-utils

     

    I'm surprised it's not installed on your system already though.  I have no record of installing it here explicitly, although perhaps it got installed implicitly as a dependency for something else I installed.

     

    That said, the alsa-utils package definitely has problems on Pi, for example alsamixer doesn't work, and nor does speaker-test, unfortunately.  But amixer does work and is used to switch audio output as I described.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to jeffbiss

    Easy to fix:

     

    • sudo apt-get install alsa-utils

     

    I'm surprised it's not installed on your system already though.  I have no record of installing it here explicitly, although perhaps it got installed implicitly as a dependency for something else I installed.

     

    That said, the alsa-utils package definitely has problems on Pi, for example alsamixer doesn't work, and nor does speaker-test, unfortunately.  But amixer does work and is used to switch audio output as I described.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jeffbiss
    jeffbiss over 14 years ago in reply to morgaine

    From reading the RPi posts about lxmusic, I thought that ALSA was part of the Debian distro, but seeing that it's not there, I must be wrong. I'll try to put together a how-to for the community when I get through this. thanks for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jeffbiss
    jeffbiss over 14 years ago in reply to jeffbiss

    Morgaine,

     

    Done! Again, thanks for your help.

     

    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine, I don't think it is the Pi. Alsamixer and speaker-test both work on my Pi (Arch Arm). I had added the cset numid=3 1 to my /etc/rc.local so that my sound would always work properly at bootup (my monitor is HDMI but doesn't have built in speakers so I use the speaker out to connect to some cheap Logitech speakers).