Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Mini USB Keyboard issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 730 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Mini USB Keyboard issue

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've taken delivery of a Raspberry Pi and have been through the boot sequence with it and can log on to it as root.

 

I was offered various options (I guess, by the Debian BIOS) when I initially started it up, one of which was to choose the type of keyboard that would be used with it.

 

I bought one of these specifically for that:

 

http://uk.farnell.com/jsp/search/productdetail.jsp?sku=1826378&CMP=i-bf9f-00001000

 

 

Part Num.           Qty. ordered Product description  Mnfr Part #

1826378  1 HK2007 KEYBOARD, MINI USB    HK2007

 

 

and I think, from memory, I chose 'A4TECH21' from the dropdown list of available keyboard types in the startup sequence.

 

When I log in and try to type at the command line the 'w', 's' and 'x' characters don't work. I don't know if it's the device itself is the issue or my choice of keyboard in the startup.

 

I plugged it in to a laptop and the result was the same (the keys above still didn't work). Should I send the keyboard back, or can I choose the keyboard again as part of the startup sequence, if so, how can I do that?

 

Any help much appreciated,

 

Thanks in advance

Pat

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    If the keys don't work when connected to the laptop, then the choice of keyboard layout within the OS on the Pi is not relevant. If I were you, I'd return it as faulty.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    If the keys don't work when connected to the laptop, then the choice of keyboard layout within the OS on the Pi is not relevant. If I were you, I'd return it as faulty.