Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36593 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi guys

     

    As promised, I have now finished testing and it toke alot more work then i had expected but here is a blog post with all the details

     

    http://www.tooms.dk/Tblog/Showblog1.asp?BlogID=201208292042561198

     

    So now the hunt for a LDO replacement

     

     

    Hope you like it.

     

    Thomas

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thomas Johansen wrote:

     

    Hi guys

     

    As promised, I have now finished testing and it toke alot more work then i had expected but here is a blog post with all the details

     

    http://www.tooms.dk/Tblog/Showblog1.asp?BlogID=201208292042561198

     

    So now the hunt for a LDO replacement

     

     

    Hope you like it.

     

    Thomas

     

     

    Hi

     

    just to say that i have now posted a follow up blog post to this with the new version 2 board

     

    http://www.tooms.dk/Tblog/Showblog1.asp?BlogID=201209222223022628

     

     

    Tooms

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    After reading so much fanboism about the Pi, we finally get one about the usb chargers.

     

    The Pi only works reliable between 4.85 and 5.25V. Even the foundation won't deny that.

    A cheap usb charger will provide a voltage of 5V usually with a tolerance of 10%

    If the Pi can't cope with these specifications, it's a bad design to use them.

    Look in the Forums if you don't believe that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    You claim I have heard about people blowing up their pi or TV. I have not.

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=7650

    http://www.raspberrypi.org/phpBB3/viewtopic.php?t=5632&p=91242

     

    There have been many similar reports, but it's easy to miss things due to the poor signal to noise ratio in the RPF forums.

     

    In my case, the quality of the usb charger was never a question. The 0.5v drop across the crappy micro usb cable was the real problem. For that reason alone I agree with jamodio that the idea was a bad one.

     

    Note that they didn't make any effort to promote better cables or better power supplies. It seemed much more like "everyone has a micro usb charger and it'll work with any old crappy charger and cable you have lying at the back of the cupboard". It's the combination of a cost constrained design with the flippant attitude that makes it a bad idea.

    Hindsight is always 20-20, but in hindsight it's difficult to argue that it was anything other than the wrong choice, even when it's understandable why the choice was made.

     

    Thing is that a crap charger and even worse cable probably works just fine as a phone charger simply down to them spending a few pennies extra on a decent power system... The same would likely be true for the Pi...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    Pete is a conservative designer. He likes the safety measures like fuses, decoupling caps, protection diodes etc etc.

     

    In this case, the fuses caused a lot of trouble. If you like to blame something else, fine. I'm going to do other things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to rew

    Removing the polyfuses does not change a poor power design which was modified to cut costs from the original design on the Alpha board.

     

    I respect your opinion and if you want to stick to it fine, your opinion, feel free to do other things.

     

    I'm not judging Pete as a designer, I'm judging the final product.

     

    It is not exactly the same thing but you can watch this video to see how poorly some of these power adapters are designed/made.

     

    http://www.youtube.com/watch?v=T88ej64aXUM&feature=player_embedded

     

    BTW I didn't search for the video, it was posted while long ago on the Rpi forum.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    selsinork wrote:

    In my case, the quality of the usb charger was never a question. The 0.5v drop across the crappy micro usb cable was the real problem. For that reason alone I agree with jamodio that the idea was a bad one.

     

    Note that they didn't make any effort to promote better cables or better power supplies. It seemed much more like "everyone has a micro usb charger and it'll work with any old crappy charger and cable you have lying at the back of the cupboard". It's the combination of a cost constrained design with the flippant attitude that makes it a bad idea.

    Hindsight is always 20-20, but in hindsight it's difficult to argue that it was anything other than the wrong choice, even when it's understandable why the choice was made.

     

    Thing is that a crap charger and even worse cable probably works just fine as a phone charger simply down to them spending a few pennies extra on a decent power system... The same would likely be true for the Pi...

    My opinion is that the RasPi's power design "seemed like a good idea at the time", and given the official USB specs for power supplies and (possibly) cables there was every reason to believe it would work.  The same is mostly true for polyfuses as well.  However, the reality is that a lot of imported USB devices and cables and polyfuses do not meet specs, and it is usually impossible to tell when you order the devices.  The Micro USB cable is a prime example: you have no idea what wire gauge the cable uses for power and ground when you order it. That cable should certainly be included -- I don't remember how many times I've advised people here and at the RasPi forum that when multiple power supplies fail to produce enough RasPi voltage, check the Micro USB cable.

     

    My own favorite example of cables not meeting specs is cheap HDMI cables that don't connect the individual ground pins.  Instead they rely on a foil shield connected to the connector shells on both ends.  This works fine in most HDMI applications, but if your application needs the ground pins you're in trouble.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to jamodio

    Ok, agreed, that's one crappy USB powersupply that won't power a 'pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Tooms wrote:

     

    Now i just need to build an 1.8V and 2.5V board and then do testing with the RPI board.

    personally I'd not bother with the 2.5v one, going by the schematics it's only used for the composite video and doesn't look like it'll ever have significant current requirements, so an LDO will be fine.

     

    yes your right, there is no point in the 2.5V

     

     

    Tooms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    However, the reality is

    image  there's a universal truth in there somewhere that reality never meets the spec.

     

    I wonder how much of the conservative engineers outlook of working out what's required, doubling it and then adding a bit of extra margin is because he knows that somewhere there's a beancounter who'll force a reduction for 'cost' reasons and to hell with the spec.

     

    The Pi being quite up front about everything being to meet the $25 price point probably suffers in that there was never any margin for the beancounter to cut...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    Ok, agreed, that's one crappy USB powersupply that won't power a 'pi.

    That case design is quite common for UK plugtop supplies for cheap electronic stuff. I have had several just like it, most of which died fairly quickly. Not hard to see why.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    Guys. Just FYI, my raspberry pi boots just fine on 3.7V.

    While slowly turning the voltage down, it crashed somewhere between 3.7 and 3.5V. That's when the "link" leds went off. It didn't come back up when I slowly turned the voltage back to the "last known working"  voltage of 3.7 and it DID come back up when I powercycled it from there.

     

    My 3.3V has dropped down to 2.7V. So the dropout of the LM1117 RG2, is about 1V. That's not very impressive for an LDO.

     

    So, if you want to keep your 'pi running, you have to keep your 5V above 3.7V. This is "actual device measurements". For "nominal operation" (e.g. to have the 3.3V within spec), you need about 4.3V, to have some margin, good engineering practise would set the  require met at "at least 4.5V" at the input.

     

    But notice that you have to go almost a whole volt below that before the 'pi stops working. That's proper engineering.

     

    The things that eat away at this margin are:

    * crappy powersupplies that don't deliver 5V at 400mA.

    * crappy powercables.

    * the polyfuse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 13 years ago in reply to e14 Contributor

    Guys. Just FYI, my raspberry pi boots just fine on 3.7V.

    While slowly turning the voltage down, it crashed somewhere between 3.7 and 3.5V. That's when the "link" leds went off. It didn't come back up when I slowly turned the voltage back to the "last known working"  voltage of 3.7 and it DID come back up when I powercycled it from there.

     

    My 3.3V has dropped down to 2.7V. So the dropout of the LM1117 RG2, is about 1V. That's not very impressive for an LDO.

     

    So, if you want to keep your 'pi running, you have to keep your 5V above 3.7V. This is "actual device measurements". For "nominal operation" (e.g. to have the 3.3V within spec), you need about 4.3V, to have some margin, good engineering practise would set the  require met at "at least 4.5V" at the input.

     

    But notice that you have to go almost a whole volt below that before the 'pi stops working. That's proper engineering.

     

    The things that eat away at this margin are:

    * crappy powersupplies that don't deliver 5V at 400mA.

    * crappy powercables.

    * the polyfuse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 13 years ago in reply to rew

    Roger Wolff wrote:

     

    Guys. Just FYI, my raspberry pi boots just fine on 3.7V.

    My RasPi system works down to 4.65V.  Below that my DVI-D monitor (connected through an HDMI Switcher) starts to misbehave.  I guess your peripherals are a lot more tolerant of low 5V than mine image   LM1117 dropout is indeed about 1V according to its spec sheet.

     

    Most 3.3V parts allow 5% - 10% tolerance, so I wouldn't let it go too low.  The previous low voltage I've heard of was 4.2V, which reduces 3.3V to 3.2V.  Below 3.3V you'll start losing Ethernet drive, but if you're only driving a 2m cable instead of 50m you'll be fine.  I would think you'd want to have at least 4.3V so RG2 is producing a precisely regulated 3.3V instead of propagating any misbehavior on the 5V0 net.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Proper engineering would require you to do the test at both end's of the Pi temperature range.

    It would also require to repeat the CE testing at the lower voltage, as it will likely make it more sensitive to radiation.

    I really don't see what the test is supposed to prove?

     

    The second test was usefull to prove that it isn't representative for all Pi's.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    My test shows the raspberry is pretty tolerant of "low voltage" at the input. The only peripherals that I had connected during my test was the ethernet. I'm not pretending you should run your raspberry at 3.7V. I'm not working on qualifying the 'pi for that. It's just that when people say that the raspberry doesn't work if your power supply delivers only 4.5V I get worked up. It simply isn't true. The raspberry pi itself works just fine downto 3.7V. All sorts of peripherals, even ones that should conform to the USB spec and therefore work downto 4.2V, drop out way earlier.

     

    I left my 'pi running at 3.7V and it's still running with an uptime of over 16 hours now.

     

    If you blame the wrong component when troubleshooting, the acutal cause of the problem won't be fixed.

     

    So, the raspberry pi works down to 3.7V on it's 5V line. This means you have to provide 3.9V at the USB connector for the raspberry to function. Given that lots of peripherals need more than that (and are also behind the polyfuse) the requirements for the powersupply and cable increase.

     

    I have tested a 500mA USB powersupply from china. It doesn't achieve its spec. But nobody claimed 500mA USB powersupplies would work.