Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36366 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    Wow. image  That's worrying.

     

    PS. It would be nice if you could include the images here directly, thumbnails at least.  Picasa is somewhat annoying because of its multiple required Javascript sources, and Google is developing quite a habit of turning off free services anyway ... as well as becoming evil. :-P

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago

    Wow. image  That's worrying.

     

    PS. It would be nice if you could include the images here directly, thumbnails at least.  Picasa is somewhat annoying because of its multiple required Javascript sources, and Google is developing quite a habit of turning off free services anyway ... as well as becoming evil. :-P

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Wow. image  That's worrying.

    Well yeah.. but I think we've suspected what's going on since jamodio pointed out the error on the schematics.

    PS. It would be nice if you could include the images here directly, thumbnails at least.  Picasa is somewhat annoying because of its multiple required Javascript sources, and Google is developing quite a habit of turning off free services anyway ... as well as becoming evil. :-P

    My reason for using an external host for the pictures is fairly simple. Most forums I try to upload to seem to have ridiculous limits, like max size of 10k and a .JPG will upload but not a .jpg or .patch rendering the facility rather pointless. I also dislike the forums where you have to register and login to see the images, or where the column width is enforced and the image gets cropped. Finally I'm usually going to share these things with several different groups of people and a central point makes it easier.  I accept you may not agree with my reasons, but they are what they are.

     

    So, if you can suggest someplace that meets the following: 1. not javascript encrusted, 2. not part of the evil empire, 3. free, 4. reasonably permanent,  I'd be more than happy to use it instead.

     

    Just trying it here, not too bad with a 2MB size limit, but still scales down the image with the associated loss of detail.  So I'll at least try uploading stuff here too.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So, if you can suggest someplace that meets the following: 1. not javascript encrusted, 2. not part of the evil empire, 3. free, 4. reasonably permanent,  I'd be more than happy to use it instead.

     

    Just trying it here, not too bad with a 2MB size limit, but still scales down the image with the associated loss of detail.

     

    Thanks. image

     

    Aye, it's a problem indeed.  I think I'm going to use this "ARM revolution" to detach myself as much as possible from the various evil empires by hosting resources of various kinds myself on cheap and low-power ARMs, and removing them from the 3rd party sites.  It'll kill several birds with one stone.  It even makes sense in colos, because you can run a whole pile of ARMs within the typical least-cost rack power allocation.

     

    Back to running my own servers like in the early days before we succumbed to the dark side. image

     

    Morgaine.