Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36382 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    When my other Pis arrive I might be tempted to break out the soldering iron. In the mean time, I'm doing a bit of reading.

     

    Looking at figure 2.2 of the 9512 datasheet (http://www.smsc.com/media/Downloads_Public/Data_Sheets/9512.pdf) would it be possible to cut the 3.3V input to the internal core regulator and have the core logic powered by an external (more efficient) 1.8V source? I'm not sure if this chip will run that way or how oversimplified this diagram is but it might be easier and more power efficient than trying to cut the link to the external 1.8V plane.

     

    I'm guessing those VDD33IO pins do more than just feed into internal regulators though, or the chip would just run off 1.8V to start with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    When my other Pis arrive I might be tempted to break out the soldering iron. In the mean time, I'm doing a bit of reading.

     

    Looking at figure 2.2 of the 9512 datasheet (http://www.smsc.com/media/Downloads_Public/Data_Sheets/9512.pdf) would it be possible to cut the 3.3V input to the internal core regulator and have the core logic powered by an external (more efficient) 1.8V source? I'm not sure if this chip will run that way or how oversimplified this diagram is but it might be easier and more power efficient than trying to cut the link to the external 1.8V plane.

     

    I'm guessing those VDD33IO pins do more than just feed into internal regulators though, or the chip would just run off 1.8V to start with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I'm guessing those VDD33IO pins do more than just feed into internal regulators though, or the chip would just run off 1.8V to start with.

    Yeah, you'd have to assume they're used for 3.3v IO pins back towards the SoC at the very least. Not really clear if the internal regulator is from a single pin, or from many, or which one. So not clear if it's easier or not.

    It's looking more like we need someone with a model A or who is prepared to pull the LAN9512 of the board to be able to measuer the RG1 current that way.  While I'm probably prepared to try that, I'm not there just yet image