Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36473 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • electron2
    electron2 over 14 years ago

    As shown in Troy Mackay's post on Jul 28 it seems to me that we could mod our PI's to work more as the chips were designed.

     

    I think that this could make the PI more stable, from the looks of it.

     

    I am not a designer Just an old tech, but I think we need to find a way to FIX what we now know is an error in the board.

     

    So could someone do some practical testing to see if there is something that can be done to easly fix the current board, rather than wait for RPI foundation to fix it by waiting for a board redesign?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to electron2

    i will love to try out the hack Troy mackay has done also and then test again with that fix on the board, but i have looked into this and i most say it is very well done by Troy as i think it is to small for me todo and i done have an microscope as need for this.

     

    so yes if some one can findout where to make an cut to split the LAN9512 1v8 from the lod 1v8 then i will try this also.

     

     

    Tooms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    jamodio wrote:

     

    What really concerns me (after all I'AM a "concern troll") is that this type of situation serves as a learning experience so we don't repeat the same errors or wrong processes, but I doubt that if there is ever a new revision or version of this board, we'll have the opportunity to review it before the hype-pi 2.0 starts.

     

    +1.

     

    Feedback on issues is part of the engineering process.  That's alien to Liz's hype & fandom process.

     

    PeteL wrote:

     

    As always - comments welcome.

     

    +1

     

    I've been trying to quantify one particular area of faulty operation, RF mice on self-powered USB hubs .  With dozens of tested (device X hub) combinations, and all 8 of the data points for RF mice showing complete failure on Pi, it's a very black-and-white test bench for USB functionality.  I happen to have a hot-running LAN9512, so I may be able to provide relevant testing if the 1.8v issues are thought to couple to USB operation.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    J

     

     

    Connecting the two 1V8’s is a sub optimal piece of design (you can look that up in the engineering translation dictionary - starts with a 'c' ends in ‘up’), and I didn't think that was of debate.

     

     

    The design did go through extensive review within the 'inner circle' of supporters who 'know' and have worked with the chips before especially the BCM. Both prototypes and pre-prototypes had this same connection and that of course made it more difficult. I also suspect, had there not been some reason to go and look, it would have never been identified. Just for the record, your technical input is appreciated, but rather than just implying - you could have just asked? Maybe you did earlier and I missed it.

     

     

    We tried to do the best job possible with the limited support and resources that the early phase project had. (We were going to make 5000-10,000 beta boards max). None of the early stress testing revealed the issue and only a small population (sub 0.01%) are reported to run unbearably hot (although more may, just not flagged up because it does not concern their owner - they are just having fun with it). Of the returns I have for analysis, I have still have not found a real ‘steamer’. These could be in part due to poor underfill or even a short/defect elsewhere on top of what we are asking the chip to do.

     

    There is an implication in posts that this is responsible for something else to do with USB but to date no info is forthcoming? (Stop press - just seen that other thread - will go and look later).

     

    It doesn't matter if you spend £1 or $10M things slip through, and there have been some very high profile events in that $10M category in all walks of engineering!

     

     

    I remember saying at the outset that Pi would never be perfect - just doesn't happen in engineering there is always something to be optimised, improved. What we do need to do is measure, evaluate, garner input and decide what, if anything, needs to be done. And I do appreciate the work done by people on this thread already.

     

     

    Pete

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Question is - were the Rubycon's real !

     

    P

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Pete,

    You wrote:

    "There is an implication in posts that this is responsible for something else to do with USB but to date no info is forthcoming? (Stop press - just seen that other thread - will go and look later)."

     

    I'm quite sure that there is no established connection at this point

    between this 1.8v power issue and any USB or other functional problems.

    Users with hot lan chips have been having USB problems, but so have

    users with cooler lan chips, so the USB problems could very well be due to

    other causes.

     

    SMSC has said "don't do that", but they haven't said what will happen

    if you do.  We've seen pretty convincing evidence that the lan chip

    will get hot, but don't know if it will malfunction, or cause a malfunction

    on the other devices connected to 1.8v, or whether its expected lifetime

    will be shortened.

     

    you wrote:

    "only a small population (sub 0.01%) are reported to run unbearably hot (although more may, just not flagged up because it does not concern their owner - they are just having fun with it). "

     

    I'm not sure what you are basing your statistics on.  Is it the return rate?

    I suspect that the rate is higher than 0.01%.  If the rate was that low,

    then certainly there would be no hesitation to announce that due to a

    design defect, a very small number of boards have chips that run blisteringly

    hot, and any user who is unlucky enough to have gotten one is welcome

    to exchange it.

     

    you wrote:

    "We tried to do the best job possible with the limited support and resources that the early phase project had."

     

    I don't think anyone would deny that you did a fantastic job with the limited

    resources you had.  But I think jamodio's point is that releasing schematics

    prior to production would not have cost anything, and could have resulted

    in great savings by uncovering such errors before mass production.

     

    I am not a hardware guy, but I am quite surprised to see that hardware

    schematics aren't clear about the direction of power flow.  It is a bit

    ironic that the beta board had a string of decoupling capacitors that

    should have been connected to 1.8v, but wasn't, and the production

    board has a similar string of decoupling capacitors that shouldn't have

    been connected to 1.8v, but was.  But there is nothing in the schematics

    to show which pins on the ICs have power going in, and which have

    power coming out.  So it is very difficult to check the schematics to

    find these kinds of errors, where components are either not connected

    to any source of power, or are connected to more than one source.

     

    At this point we are completely in the dark about what hardware revisions

    are contemplated, other than Eben's mention of some unspecified pcb

    change for FCC/CE residential compliance.  Hopefully that will change.

     

    Eben said he wanted to fix the FCC/CE issue prior to the educational

    release.  Since the 2012/2013 school year is about to start, the timing

    seems really odd not to have fixed that by now.  The timing also seems

    really odd not to have published the user's manual by now.  Amazon is

    showing a projected date of 16 October.  So are you aiming for the

    2013/2014 school year?  If so, I'm quite sure you will need 512MB ram

    to be competitive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    First of all thanks for being here and for following up. I really appreciate the work you have done and I truly believe that some of the mishaps from the RPF are not your own making.

     

    Connecting the two 1V8’s is a sub optimal piece of design (you can look that up in the engineering translation dictionary - starts with a 'c' ends in ‘up’), and I didn't think that was of debate.

     

    Well, you may call it "sub optimal design" but it is actually an error, and in my dictionary it starts with 'f' and ends in 'up' ;-)

     

     

    The design did go through extensive review within the 'inner circle' of supporters who 'know' and have worked with the chips before especially the BCM. Both prototypes and pre-prototypes had this same connection and that of course made it more difficult. I also suspect, had there not been some reason to go and look, it would have never been identified. Just for the record, your technical input is appreciated, but rather than just implying - you could have just asked? Maybe you did earlier and I missed it.

     

    Obviously the process didn't work, and as you clearly know in the previous prototype it was reported that various power connections were missing, kind of a surprise since part of the 'inner circle' was apparently involved in the design of the BCM SoC chip. Perhaps the 'inner circle' has a very small radius and some of the supporters actually "don't know." Not just me but many other asked while before the boards went to production for schematics/gerbers and the only we obtained was a crop showing a psu section. I reported the problem as soon as the schematics were made public, and it didn't took too much know how, just reading the SMSC datasheet to figure what each pin was used for, something that we don't even have for the SoC part.

     

    And about asking, I asked what else is on "the list", no response yet.

     

      We tried to do the best job possible with the limited support and resources that the early phase project had. (We were going to make 5000-10,000 beta boards max). None of the early stress testing revealed the issue and only a small population (sub 0.01%) are reported to run unbearably hot (although more may, just not flagged up because it does not concern their owner - they are just having fun with it). Of the returns I have for analysis, I have still have not found a real ‘steamer’. These could be in part due to poor underfill or even a short/defect elsewhere on top of what we are asking the chip to do.

     

    The foundation should have put they arrogance away and ask for help and additional support, there has been a large group of people willing all the time to cooperate, and they are still out there but the RPF attitude has been always "what we did is perfect and we know everything." I'll not trust any number, percentages or analysis derived from them given that there are no public numbers about how many boards have been manufactured, how many have failed, how many have been sold. how many have been shipped, how many have been returned, etc, and there is no formal or reasonable system to track complains/failures/fixes.

     

    There is an implication in posts that this is responsible for something else to do with USB but to date no info is forthcoming? (Stop press - just seen that other thread - will go and look later).

     

    I'm not sure if there is a direct connection with several of the problems reported with USB. Certainly the entire power architecture does not help, but there are some hardware/firmware issues related to USB where things are not working as expected and somebody is now reading the Verilog files for that piece of silicon on the SoC discovering some limitations and other stuff hidden behind the obscurity of the drivers.

     

    I know that everybody have tried to do their best, but recognition for a successful endeavour comes from producing positive results and not from the effort put to get them.

     

    My .02

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

     

    So I guess it is not worth me publishing here what I know and what I can measure?image image

     

    I do take issue with your final comment - it has been a success so far - with some measure of "success failure" thrown in.

     

    I've been talking to users who just have one or two and are over the moon with them (faults issues and all) and they tell me that they have already learnt so much.

     

    My overall positive view may yet be proved wrong, but as I said right at the outset it isn’t perfect, never will be - we just have to remember why we are clearing the swamp!

     

    Off to watch the Olympics image on TV image

     

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I am not a hardware guy, but I am quite surprised to see that hardware

    schematics aren't clear about the direction of power flow.

    In many years of working in the subcontract hardware assembly business I've seen hundreds of schematics from all sorts of companies, from the biggest names to tiny one man outfits and I've rarely seen anything indicating power direction.

    This sort of thing wouldn't have been a problem in years gone by as it was rare for IC's to have internal regulators and often power was supplied from an off board supply so it was obvious.

    Things change, technology gets more complex, leaving room for ambiguity and errors to creep in.

     

    IME Petes schematics are pretty good, they lack some things you'd normally find on much larger schematics like a cross reference of refdes and signals to page and location, but for four pages most of that stuff isn't really necessary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    lol.. nope.. it's like one of those russian dolls you keep removing another layer until you get to the 0201 smt cap somewhere inside image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    So I guess it is not worth me publishing here what I know and what I can measure?image image

     

    I'd certainly appreciate anything you're willing to share Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    PeteL wrote:

     

     

     

    I remember saying at the outset that Pi would never be perfect - just doesn't happen in engineering there is always something to be optimised, improved.

    There is a story about a craftsman who made beaten copper doors for the Tsar of Russia's throne room.  He would take a large sheet of copper and beat it over and over with a hammer, creating beautiful swirling patterns.  Someone asked him "how do you know when you're done?"  He answered: "It's never done.  I just keep hitting it until they take it away from me."

     

    Engineering is like that -- especially software engineering.

     

    Thank you for being open to suggestions, Pete!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    PeteL wrote:

     

     

     

    I remember saying at the outset that Pi would never be perfect - just doesn't happen in engineering there is always something to be optimised, improved.

    There is a story about a craftsman who made beaten copper doors for the Tsar of Russia's throne room.  He would take a large sheet of copper and beat it over and over with a hammer, creating beautiful swirling patterns.  Someone asked him "how do you know when you're done?"  He answered: "It's never done.  I just keep hitting it until they take it away from me."

     

    Engineering is like that -- especially software engineering.

     

    Thank you for being open to suggestions, Pete!